Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development petalinux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 364 subscribers
  • Views 1373 views
  • Users 0 members are here
Related

petalinux

yangtuzi
yangtuzi over 9 years ago

I want to make image by petalinux.

I do step fallow ug1144

1.source /home/petalinux/settings.sh

2.echo $PETALINUX

3.petalinux-create --type project --template zynq --name test

4.petalinux-config --get-hw-description=/home/design_1_wrapper_hw_platform_0

5.petalinux-build

then ERROR appears:

ERROR:OE-core's config sanity checker detected a potential misconfiguration.Either fix the cause of this error or at your own risk disable the checker(see sanity.conf).Following is the list of potential problems/advisories:

Do not use Bitbake as root.

How can I solve this error?

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 8 years ago

    Hi yangtuzi,

    Check out this thread on the Xilinx forums where others were experiencing a similar problem that was related to an incorrect version of Python being installed:

    https://forums.xilinx.com/t5/Embedded-Linux/Petalinux-2017-2-Failed-to-source-bitbake/td-p/796848/page/2

    Is it possible this is also the cause of your issue with bitbake?

    Best Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 8 years ago

    Hi yangtuzi,

    Check out this thread on the Xilinx forums where others were experiencing a similar problem that was related to an incorrect version of Python being installed:

    https://forums.xilinx.com/t5/Embedded-Linux/Petalinux-2017-2-Failed-to-source-bitbake/td-p/796848/page/2

    Is it possible this is also the cause of your issue with bitbake?

    Best Regards,

    -Kevin