Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Issue with uboot 2016.2 and QSPI
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 364 subscribers
  • Views 500 views
  • Users 0 members are here
Related

Issue with uboot 2016.2 and QSPI

e14 Contributor
e14 Contributor over 10 years ago

Hi,

I am running custom Linux 4.4 on a Picozed with a custom carrier.

I have recently upgraded to U-boot 2016.2 from 2015.2 and have attempted to make the transition from the config based setup to the devicetreein u-boot.

I have come across this issue:

U-Boot 2016.01-dirty (Sep 06 2016 - 16:24:18 +1200)

Model: Zynq PicoZed Board
Board: Xilinx Zynq
DRAM:  ECC disabled 0 Bytes
MMC:   sdhci@e0100000: 0, sdhci@e0101000: 1
*** Warning - spi_flash_probe() failed, using default environment

In:    serial@e0000000
Out:   serial@e0000000
Err:   serial@e0000000
Model: Zynq PicoZed Board
Board: Xilinx Zynq
Net:   ZYNQ GEM: e000b000, phyaddr 0, interface rgmii-id
eth0: ethernet@e000b000
Hit any key to stop autoboot:  0
Copying Linux from QSPI flash to RAM...
Failed to initialize SPI flash at 0:0 (error -2)

------------------

----

Anyone able to help?  Is there anything obvious I am doing wrong?

 

Thanks,

 

Tim

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Here is my uboot devicetree

    /dts-v1/;
    #include "zynq-7000.dtsi"

    / {
        model = "Zynq PicoZed Board";
        compatible = "xlnx,zynq-picozed", "xlnx,zynq-7000";

        aliases {
            serial0 = &uart0;
                    spi0 = &qspi;
                    mmc0 = &sdhci0;                
                    mmc1 = &sdhci1;
        };

        memory {
            device_type = "memory";
            reg = <0 0x40000000>;
        };
    };

    &clkc {
            ps-clk-frequency = <33333333>;
    };

    &uart0 {
        u-boot,dm-pre-reloc;
        status = "okay";
    };

    &qspi {
            u-boot,dm-pre-reloc;
            status = "okay";
            is-dual = <0x0>;
            num-cs = <0x1>;

            flash@0 {
                    compatible = "micron,n25q128a13";
                    reg = <0x0>;
                    spi-tx-bus-width = <0x1>;
                    spi-rx-bus-width = <0x4>;
                    spi-max-frequency = <0x2faf080>;
                    #address-cells = <0x1>;
                    #size-cells = <0x1>;

                    partition@qspi-bootimage {
                            label = "qspi-bootimage";
                            reg = <0x0 0x600000>;
                    };

                    partition@qspi-kernel {
                            label = "qspi-kernel";
                            reg = <0x600000 0x500000>;
                    };

                    partition@qspi-device-tree {
                            label = "qspi-device-tree";
                            reg = <0xb00000 0x80000>;
                    };

                    partition@qspi-bootargs {
                            label = "qspi-bootargs";
                            reg = <0xb80000 0x80000>;
                    };

                    partition@qspi-bootscript {
                            label = "qspi-bootscript";
                            reg = <0xc00000 0x40000>;

                   };

                    partition@qspi-rootfs {
                            label = "qspi-rootfs";
                            reg = <0xc40000 0x3c0000>;
                    };        
            };
    };


    &gem0 {
            status = "okay";
            phy-mode = "rgmii-id";
            phy-handle = <&ethernet_phy>;

            ethernet_phy: ethernet-phy@0 {
                    reg = <0>;
            };
    };

    &sdhci0 {
            u-boot,dm-pre-reloc;
            status = "okay";
    };

    &sdhci1 {
            u-boot,dm-pre-reloc;
            status = "okay";
    };

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 10 years ago

    Hello Timelmg,

    Unfortunatly we have not tried this methodology as of yet and cannot offer much support. I would suggest you head over to the xilinx forum and try asking your question there. 

    https://forums.xilinx.com/t5/Embedded-Linux/bd-p/ELINUX 

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to jafoste4

    Hi Josh,

    Thanks for the reply.   I have posted my query on the Xilinx forums and are awaiting response.

    Tim