Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Issue with uboot 2016.2 and QSPI
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 364 subscribers
  • Views 501 views
  • Users 0 members are here
Related

Issue with uboot 2016.2 and QSPI

e14 Contributor
e14 Contributor over 10 years ago

Hi,

I am running custom Linux 4.4 on a Picozed with a custom carrier.

I have recently upgraded to U-boot 2016.2 from 2015.2 and have attempted to make the transition from the config based setup to the devicetreein u-boot.

I have come across this issue:

U-Boot 2016.01-dirty (Sep 06 2016 - 16:24:18 +1200)

Model: Zynq PicoZed Board
Board: Xilinx Zynq
DRAM:  ECC disabled 0 Bytes
MMC:   sdhci@e0100000: 0, sdhci@e0101000: 1
*** Warning - spi_flash_probe() failed, using default environment

In:    serial@e0000000
Out:   serial@e0000000
Err:   serial@e0000000
Model: Zynq PicoZed Board
Board: Xilinx Zynq
Net:   ZYNQ GEM: e000b000, phyaddr 0, interface rgmii-id
eth0: ethernet@e000b000
Hit any key to stop autoboot:  0
Copying Linux from QSPI flash to RAM...
Failed to initialize SPI flash at 0:0 (error -2)

------------------

----

Anyone able to help?  Is there anything obvious I am doing wrong?

 

Thanks,

 

Tim

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 10 years ago

    Hello Timelmg,

    Unfortunatly we have not tried this methodology as of yet and cannot offer much support. I would suggest you head over to the xilinx forum and try asking your question there. 

    https://forums.xilinx.com/t5/Embedded-Linux/bd-p/ELINUX 

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to jafoste4

    Hi Josh,

    Thanks for the reply.   I have posted my query on the Xilinx forums and are awaiting response.

    Tim

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to jafoste4

    Hi Josh,

    Thanks for the reply.   I have posted my query on the Xilinx forums and are awaiting response.

    Tim