Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development sudo update sudo upgrade
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 363 subscribers
  • Views 1151 views
  • Users 0 members are here
Related

sudo update sudo upgrade

e14 Contributor
e14 Contributor over 14 years ago

Hi,

I'm trying just to update linux when I run into a fatal error.  When I try the command

$sudo aot-get update

there are no problems.  However, when I try

$sudo apt-get upgrade

it runs for some time before giving me the following error:

FATAL: Could not load /lib/modules/3.2.0-1412-omap4/modules.dep: No such file or directory

It repeats this a hundred times or so, and in the middle of that it gives the following warning just once:

cryptsetup: WARNING: could not determine root device from /etc/fstab

When I go looking for the directory that causes the fatal error, I find that within /lib/modules there is the 3.3.0-xillinux-1.0+ directory.  How do I configure this so I can update at the appropriate directory?  Also what sorts of problems might this fatal error cause in the future?  Thank you all in advance.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    jayjay71,

    What version of Linux are you running?  And from where?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    I'm using Xillinux, but after recompiling the kernel I was able to fix this issue.  I've since run into many more issues, but I'll spend a bit more time working through them before posting again.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    I guess I was wrong about that, as I am actually still having issues upgrading.  I was following the guide here http://xillybus.com/downloads/doc/xillybus_getting_started_linux.pdf and I recompiled the kernel using

    $make xilinx_zynq_defconfig

    am I missing something?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Hey,

    could you check whether you get and "update-initramfs" somewhere as well?
    I remember having a likewise problem with /lib/modules...

    If so the workaround for me was:
    "forcing update-initramfs on the particular version & dpkg --configure -a"
    found here:
    https://bugs.launchpad.net/ubuntu/+source/linux-meta-ti-omap4/+bug/1041607

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks for the response, alas it did not solve my problem.  The problem seems pretty simple, sudo apt-get upgrade is looking for the modules in the wrong directory, and I don't know how to change where it's supposed to look for them. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Maybe I'm not being clear.  I do not have the /lib/modules/3.2.0-1412-ompp4/modules.dep, as the directory 3.2.0-1412-omap4 doesn't exist but there is instead the 3.3.0-xillinux-1.0+ directory.  Do other people have both?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    So the issue seems to be running apt-get upgrade causes it to link to the omap4 kernel instead of the xillinux kernel, which causes all sorts of problems.  You can fix this by going to /boot and deleting the link to the omap4 kernel with

    $rm vmlinuz

    then

    $ln -s vmlinuz-3.3.0-xillinux-1.0 vmlinuz

    to link to the correct kernel.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Hi,

    The root of the problem is that Xillinux takes a detour from the package food chain, so changes made in the OS aren't necessarily reflected in the Debian package state.

    The kernel was indeed replaced, and an attempt to do a general update indeed exposes this.

    The question is why you want to do a general upgrade. There have been no problem for me installing individual packages, but I don't understand why you want to take a system that works and give it a shake. I'm quite confident that something would break, even if the packages were in sync.

        Eli

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Hi Eli,

    Thanks for the response.  I was just going through the motions to install OpenCV.  Typically I make sure everything is up to date before installing all of the dependencies.  Anyway, I'll give it another go without updating and see how well it works.