Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development sudo update sudo upgrade
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 363 subscribers
  • Views 1151 views
  • Users 0 members are here
Related

sudo update sudo upgrade

e14 Contributor
e14 Contributor over 14 years ago

Hi,

I'm trying just to update linux when I run into a fatal error.  When I try the command

$sudo aot-get update

there are no problems.  However, when I try

$sudo apt-get upgrade

it runs for some time before giving me the following error:

FATAL: Could not load /lib/modules/3.2.0-1412-omap4/modules.dep: No such file or directory

It repeats this a hundred times or so, and in the middle of that it gives the following warning just once:

cryptsetup: WARNING: could not determine root device from /etc/fstab

When I go looking for the directory that causes the fatal error, I find that within /lib/modules there is the 3.3.0-xillinux-1.0+ directory.  How do I configure this so I can update at the appropriate directory?  Also what sorts of problems might this fatal error cause in the future?  Thank you all in advance.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    So the issue seems to be running apt-get upgrade causes it to link to the omap4 kernel instead of the xillinux kernel, which causes all sorts of problems.  You can fix this by going to /boot and deleting the link to the omap4 kernel with

    $rm vmlinuz

    then

    $ln -s vmlinuz-3.3.0-xillinux-1.0 vmlinuz

    to link to the correct kernel.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    So the issue seems to be running apt-get upgrade causes it to link to the omap4 kernel instead of the xillinux kernel, which causes all sorts of problems.  You can fix this by going to /boot and deleting the link to the omap4 kernel with

    $rm vmlinuz

    then

    $ln -s vmlinuz-3.3.0-xillinux-1.0 vmlinuz

    to link to the correct kernel.