Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development picoZed boot from qspi
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Subscribers 364 subscribers
  • Views 1331 views
  • Users 0 members are here
Related

picoZed boot from qspi

lguser
lguser over 8 years ago

The default Pulsar Linux image (uImage) on the SD card that came with our picoZed board (FMC Carrier card v2) does not has the "flashcp" utility.  So we can not write to the QSPI flash from Linux.  Is there a Linux image with flashcp that we can download?

It seems that we might have to use JTAG to write BOOT.bin to the QSPI flash. Does Avnet has a BOOT.mcs file for download? 

In addition, the instructions from the tutorials specify that some on-board jumpers must be set.  But the jumpers don't seem to match those on our board. Are they for v1 or v2? 

I want to be careful since the on-board QSPI flash came with a bootloader.  It does not work well, but I  want to preserve it unless we have something better.

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 8 years ago

    Hi,

    Have yu taken a look at our existing petalinux BSPs? Unfortunatly our support is limited in respects to Pulsar Linux.

    -Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • lguser
    0 lguser over 8 years ago

    Since the Linux image does not has flashcp, I can going to use JTAG to write BOOT.mcs to the QSPI flash. Do you have the the instruction? (As I mentioned, the instructions from the tutorials specify that some on-board jumpers must be set.  But the jumpers don't seem to match those on our v2 board. Are they for v1 or v2?)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 8 years ago

    Hi,

    Please specify which tutorail you are referencing. Based on what your saying I believe you are refering to the boot mode switch which is located on the SOM.

    -Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • lguser
    0 lguser over 8 years ago

    02_MZPZ_Zynq_Hello_World_2016_4_01 2.pdf

    page 15

    b. PicoZed

     
      

    iii. Set the on-board jumpers as follows

      
         
    1.     

      JP1 is open

         
    2.    
    3.     

      JP3 is closed in position 1-2

         
    4.    
    5.     

      JP4 is closed

         
    6.    
    7.     

      JP6 is open

         
    8.    
    9.     

      J9 is closed in positions 3-5 and 4-6

         
    10.    
    11.     

      CON2 is open, which sets V_ADJ to 1.8V

         
    12.   
     
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • lguser
    0 lguser over 8 years ago

    Without setting any of the jumpers, I tried to use our Xilinx JTAG programmer to program the flash via the 'Program Flash Memory' SDK tool. It failed with the message.

    ERROR: Unable to detect JTAG cable.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 8 years ago

    Hi,

    Unfortunalty it looks like adding in the PicoZed FMC V2 board configuration section was missed in that lab.

    However, if you go into tutorial 05, it shows how to setup your picozed fmc v2. follow those steps and apply them to your current tutorial.

    -Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer