Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development picoZed boot from qspi
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Subscribers 364 subscribers
  • Views 1333 views
  • Users 0 members are here
Related

picoZed boot from qspi

lguser
lguser over 8 years ago

The default Pulsar Linux image (uImage) on the SD card that came with our picoZed board (FMC Carrier card v2) does not has the "flashcp" utility.  So we can not write to the QSPI flash from Linux.  Is there a Linux image with flashcp that we can download?

It seems that we might have to use JTAG to write BOOT.bin to the QSPI flash. Does Avnet has a BOOT.mcs file for download? 

In addition, the instructions from the tutorials specify that some on-board jumpers must be set.  But the jumpers don't seem to match those on our board. Are they for v1 or v2? 

I want to be careful since the on-board QSPI flash came with a bootloader.  It does not work well, but I  want to preserve it unless we have something better.

  • Sign in to reply
  • Cancel
Parents
  • lguser
    0 lguser over 8 years ago

    02_MZPZ_Zynq_Hello_World_2016_4_01 2.pdf

    page 15

    b. PicoZed

     
      

    iii. Set the on-board jumpers as follows

      
         
    1.     

      JP1 is open

         
    2.    
    3.     

      JP3 is closed in position 1-2

         
    4.    
    5.     

      JP4 is closed

         
    6.    
    7.     

      JP6 is open

         
    8.    
    9.     

      J9 is closed in positions 3-5 and 4-6

         
    10.    
    11.     

      CON2 is open, which sets V_ADJ to 1.8V

         
    12.   
     
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • lguser
    0 lguser over 8 years ago

    02_MZPZ_Zynq_Hello_World_2016_4_01 2.pdf

    page 15

    b. PicoZed

     
      

    iii. Set the on-board jumpers as follows

      
         
    1.     

      JP1 is open

         
    2.    
    3.     

      JP3 is closed in position 1-2

         
    4.    
    5.     

      JP4 is closed

         
    6.    
    7.     

      JP6 is open

         
    8.    
    9.     

      J9 is closed in positions 3-5 and 4-6

         
    10.    
    11.     

      CON2 is open, which sets V_ADJ to 1.8V

         
    12.