Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Ethernet driver (Bare-Metal Application)
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 34 replies
  • Subscribers 372 subscribers
  • Views 6660 views
  • Users 0 members are here
Related

Ethernet driver (Bare-Metal Application)

e14 Contributor
e14 Contributor over 12 years ago

Hi,

I'm starting to work with the Zedboard and I'm very lost. I want to establish an Ethernet connection between the board and a PC, running in the Zedboard a bare-metal application.

I've tried to make work the example of the Xilinx driver emacps (which don't seems very simple to me...), but I don't see any result. I'm running the example on the Zedboard and Wireshark in the PC. As long as I know, I should receive some frames from the board, but I don't see anything (after power up the board I see a lot of frames, but they aren't sent from mi application).

Maybe I'm wrong about what the example shoud do. I just want to learn the simplest way to send and receive frames and see it works...

Any help?

Thank you (and sorry for my English...).

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago +1
    Hey sysseon, you missunderstood the example. The example does not send anything to the PC, it makes a selftest useing the loopback function of the PHY. I got Ethernet to work with PC, so if someone needs…
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi Sysseon,
    I'm new to Zed, and can't find "the example of xilinx driver emacps". Actually I have worked on this driver without any example for a few days, so if you could help me with getting the example I will be appreciated very much.
    Thank you in advance.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Once the SDK is open, create an application project with peripheral test.

    Open the .mss file from the board support package folder.
    In that there would be a list of peripheral drivers. An d from there you can get the documentation and the example for the emacps.

    I hope this is what you wanted..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hey sysseon,
    you missunderstood the example. The example does not send anything to the PC, it makes a selftest useing the loopback function of the PHY.
    I got Ethernet to work with PC, so if someone needs an example, just send me a personal message (like that I get an email notification)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Yaro,

    I would very much like to see that example. I have a custom design running on the Pl side of Zedboard. I would like to send LTE baseband data from the Host via Ethernet. This example will help with that past of the code.

    Thanks

    JT

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Hello JT,

    you can download the design here:
    https://dl.dropboxusercontent.com/u/"replace with no bot number"/ethernet.7z

    No bot number is 15987625

    I use Zedboard revision C, but it should work with d, too.

    The program sends a frame (from PS) over gigabit Ethernet and then waits for one. As soon as it receives a frame, it is printed on the standard output.
    You can test it by receiving the frame with wiresharc. I have written a test program to send something to the Zedboard, so if you need that, I can give that to you, too.

    The main difference to the example project is that the Phy is no longer in loopback mode.
    Makeing the region of the BD-list uncacheable is verry important. If you do not know how that is done, read this:
    http://www.silica.com/fileadmin/02_Products/Productdetails/Xilinx/Zynq_MMU_caches_control_ver1.0.pdf

    The program is not well documented, so if you do not understand something, feel free to ask.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Guys,

      If you are looking for a simple example application that uses a TCP/IP protocol stack, you can just generate the echo server example Application in the SDK.  That should give you some working code that you can step through with the symbolic debugger to see exactly how the code is structured and how you can set up the low level Ethernet interface.

     

    Ron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    I'm going to jump in here and support yaro123 when he says that making the RxBDs and the Rx Buffers uncacheable is super important. I can't figure out how to download yaro123's program, though he posted a few snippets of it for me earlier. Here is how I was able to get the Rx Buffers out of cached memory while still not breaking the Xilinx IEEE1588PTP example (which sends and receives Ethernet packets):

    #define RX_BUF_ADDRESS 0x1FF00000
    #define RxBufMem (unsigned char **) RX_BUF_ADDRESS
    typedef struct packet {
    tu8 data[XEMACPS_RX_BUF_SIZE];
    } Packet;
    Packet *packets;

    int main(void)
    {
    tXil_SetTlbAttributes(RX_BUF_ADDRESS, 0xc02);
    tpackets = (Packet*)RX_BUF_ADDRESS;

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Heh... I get it, "replace with no bot number"...
    Now I just feel silly for not understanding it the first time I looked at it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Hi,

    thank you for sharing the project with us. If you could also share the program to send something to the zedboard with us this would be perfect!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Hello yaro123,

    thank you for sharing your project with us. It would be perfect if you could also share the test program for sending data to the Zedboard too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>