Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Ethernet driver (Bare-Metal Application)
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 34 replies
  • Subscribers 372 subscribers
  • Views 6662 views
  • Users 0 members are here
Related

Ethernet driver (Bare-Metal Application)

e14 Contributor
e14 Contributor over 12 years ago

Hi,

I'm starting to work with the Zedboard and I'm very lost. I want to establish an Ethernet connection between the board and a PC, running in the Zedboard a bare-metal application.

I've tried to make work the example of the Xilinx driver emacps (which don't seems very simple to me...), but I don't see any result. I'm running the example on the Zedboard and Wireshark in the PC. As long as I know, I should receive some frames from the board, but I don't see anything (after power up the board I see a lot of frames, but they aren't sent from mi application).

Maybe I'm wrong about what the example shoud do. I just want to learn the simplest way to send and receive frames and see it works...

Any help?

Thank you (and sorry for my English...).

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago +1
    Hey sysseon, you missunderstood the example. The example does not send anything to the PC, it makes a selftest useing the loopback function of the PHY. I got Ethernet to work with PC, so if someone needs…
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    I'm going to jump in here and support yaro123 when he says that making the RxBDs and the Rx Buffers uncacheable is super important. I can't figure out how to download yaro123's program, though he posted a few snippets of it for me earlier. Here is how I was able to get the Rx Buffers out of cached memory while still not breaking the Xilinx IEEE1588PTP example (which sends and receives Ethernet packets):

    #define RX_BUF_ADDRESS 0x1FF00000
    #define RxBufMem (unsigned char **) RX_BUF_ADDRESS
    typedef struct packet {
    tu8 data[XEMACPS_RX_BUF_SIZE];
    } Packet;
    Packet *packets;

    int main(void)
    {
    tXil_SetTlbAttributes(RX_BUF_ADDRESS, 0xc02);
    tpackets = (Packet*)RX_BUF_ADDRESS;

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Heh... I get it, "replace with no bot number"...
    Now I just feel silly for not understanding it the first time I looked at it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Heh... I get it, "replace with no bot number"...
    Now I just feel silly for not understanding it the first time I looked at it.