Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Ubuntu Desktop Linux on Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 363 subscribers
  • Views 607 views
  • Users 0 members are here
Related

Ubuntu Desktop Linux on Zedboard

e14 Contributor
e14 Contributor over 13 years ago

Hello,

I have tried to build and run the Reference design
Ubuntu Desktop Linux (http://www.zedboard.org/sites/default/files/design/Ubuntu_on_Zedboard_Tutorial_v14.4_02.pdf),
but I get the following message in TeraTerm when booting:

reading uImage
2880430 bytes read in 414 ms (6.6 MiB/s)
reading devicetree.dtb
8451 bytes read in 14 ms (588.9 KiB/s)
## Booting kernel from Legacy Image at 03000000 ...
   Image Name:   Linux kernel
   Image Type:   ARM Linux Kernel Image (gzip compressed)
   Data Size:    2880366 Bytes = 2.7 MiB
   Load Address: 00008000
   Entry Point:  00008000
   Verifying Checksum ... OK
## Loading init Ramdisk from FIT Image at 02a00000 ...
Bad FIT ramdisk image format!
Ramdisk image is corrupt or invalid
zynq-uboot>

Is something wrong with the ext4 partition that I created as described in the Reference or is it something else (i.e in the uImage, devicetree, etc)?

Thanks in advance

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Dear  jveleg ,

    Sorry i don't have answer to your question because I am new with zedboard .
    please can you tell me from where you downloaded the (Ubuntu-CentOS).iso that used in this labs .because i got error when using( CentOS) that used in the speedway labs.

    thanks in avance

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I too had the same problem. I guess some incompatibilities crept in with new releases. I suggest using Xillinux. It provides Ubuntu desktop but with VGA output instead of HDMI.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I searched the web, and I found out that the uImage is not properly compressed or compiled... I get the following error:

    U-Boot 2012.10-dirty (Jul 24 2013 - 07:47:39)

    DRAM:  512 MiB
    WARNING: Caches not enabled
    MMC:   SDHCI: 0
    SF: Detected S25FL256S with page size 64 KiB, total 32 MiB
    SF: Warning - Only lower 16MB is accessible in 3 byte addressing mode
    In:    serial
    Out:   serial
    Err:   serial
    Net:   zynq_gem
    Hit any key to stop autoboot:  0
    Copying Linux from SD to RAM...RFS in ext4
    Device: SDHCI
    Manufacturer ID: 41
    OEM: 3432
    Name: SD8GB
    Tran Speed: 50000000
    Rd Block Len: 512
    SD version 2.0
    High Capacity: Yes
    Capacity: 7.4 GiB
    Bus Width: 4-bit
    reading uImage

    2900592 bytes read
    reading devicetree.dtb

    8451 bytes read
    ## Booting kernel from Legacy Image at 03000000 ...
       Image Name:   Linux-3.9.0-g848125a
       Image Type:   ARM Linux Kernel Image (uncompressed)
       Data Size:    2900528 Bytes = 2.8 MiB
       Load Address: 00008000
       Entry Point:  00008000
       Verifying Checksum ... OK
    Wrong Ramdisk Image Format
    Ramdisk image is corrupt or invalid

    I used mkimage to build the uImage file after the compilation of the kernel, as described in the Reference

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    In fact I am also facing the same issues over it's management...what are the other alternatives of it? Check out http://www.googleappsmanagement.com