Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Ubuntu Desktop Linux on Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 363 subscribers
  • Views 607 views
  • Users 0 members are here
Related

Ubuntu Desktop Linux on Zedboard

e14 Contributor
e14 Contributor over 13 years ago

Hello,

I have tried to build and run the Reference design
Ubuntu Desktop Linux (http://www.zedboard.org/sites/default/files/design/Ubuntu_on_Zedboard_Tutorial_v14.4_02.pdf),
but I get the following message in TeraTerm when booting:

reading uImage
2880430 bytes read in 414 ms (6.6 MiB/s)
reading devicetree.dtb
8451 bytes read in 14 ms (588.9 KiB/s)
## Booting kernel from Legacy Image at 03000000 ...
   Image Name:   Linux kernel
   Image Type:   ARM Linux Kernel Image (gzip compressed)
   Data Size:    2880366 Bytes = 2.7 MiB
   Load Address: 00008000
   Entry Point:  00008000
   Verifying Checksum ... OK
## Loading init Ramdisk from FIT Image at 02a00000 ...
Bad FIT ramdisk image format!
Ramdisk image is corrupt or invalid
zynq-uboot>

Is something wrong with the ext4 partition that I created as described in the Reference or is it something else (i.e in the uImage, devicetree, etc)?

Thanks in advance

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    In fact I am also facing the same issues over it's management...what are the other alternatives of it? Check out http://www.googleappsmanagement.com

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    In fact I am also facing the same issues over it's management...what are the other alternatives of it? Check out http://www.googleappsmanagement.com