Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development SD Card example design using standalone?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 20 replies
  • Subscribers 366 subscribers
  • Views 6046 views
  • Users 0 members are here
Related

SD Card example design using standalone?

e14 Contributor
e14 Contributor over 14 years ago

Hello folks,

Quick question:  Is it possible to do read/writes to an SD card using standalone (bare-metal) OS? 

I tried building a Zynq-based SDK project with a standalone BSP + xilfatfs.  However when I do so I get this error in SDK:

ERROR:EDK:3900 - issued from TCL procedure "::sw_xilfatfs_v1_00_a::xilfatfs_drc"
   line 15
   xilfatfs () - Sysace HW module not present or not accessible from this
   processor. FATfs cannot be used without this module

So my guess is, standalone OS doesn't have libraries for SD/MMC support...

I know the typical flow is to use U-boot/Linux, but my application will be *dumb* simple and U-boot/Linux would be unnecessary overhead. 

The application will simply move a file from SD card over to memory, and buffer the data via GPIOs to an external device.

Thanks,

Eddie

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Eddie,

    Here is a great thread from the Xilinx forums talking about doing exactly what you would like to do (except on a MicroBlaze processor, however the flow will be very similar).

    http://forums.xilinx.com/t5/EDK-and-Platform-Studio/XPS-SPI-Core-and-SD-Card/td-p/173580

    Let me know if that helps, and if not we can go through it step by step.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Eddie,

    Here is a great thread from the Xilinx forums talking about doing exactly what you would like to do (except on a MicroBlaze processor, however the flow will be very similar).

    http://forums.xilinx.com/t5/EDK-and-Platform-Studio/XPS-SPI-Core-and-SD-Card/td-p/173580

    Let me know if that helps, and if not we can go through it step by step.