Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development When is it necessary to "Export to SDK"
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 364 subscribers
  • Views 633 views
  • Users 0 members are here
Related

When is it necessary to "Export to SDK"

ejubenville
ejubenville over 13 years ago

I'm learning the ZedBoard and the Xilinx tools, but am confused about the role of "Export to SDK" in PlanAhead.  I understand why I need to do it the first time after creating a new design, but when do I need to do it again?  In other words, what changes to my hardware design imply that my SDK's version of the hardware are out of date.

I am currently running bare metal applications, so it intuitively feels like as long as I don't add/delete peripherals or change the memory map, I shouldn't have to do another export.  Is that the rule?

Example:  I am debugging my peripheral code, and change a few lines of HDL, synthesize, etc., and download the new bit stream with Impact.  Would that scenario dictate that I do the export?

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    You never need to export. (Well, you need it once to create your Xilinx-BSP.)
    exporting will give you the system.xml (shows addresses of periperials).
    You can use all features of BSP (i think), even if you did not put them in PL-Fabric.
    It also copies the bitstream, so it is easier/faster to download it and create a boot image.

    I honestly thing you never need to update the export-project if you know what you are doing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jamestkennedy
    0 jamestkennedy over 13 years ago in reply to e14 Contributor

    I always export if I have regenerated the bitstream. maybe this is not necessary?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to jamestkennedy

    Export whenever there is a change to the embedded system (i.e you make changes in EDK).
    Last week I added a video timing controller to my embedded design, but neglected to export, so the SDK had no idea that there were new elements in the embedded system.

    ---
    Joe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    SDK does not care about FPGA stuff as long as you programm the bistream elsewhere

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 13 years ago in reply to e14 Contributor

    That's true except in the case where you've added processor IP in the PL and want the drivers to show up in the BSP. Then you need to export again.

    Bryan