Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Interrupt Handler in Kernel Module
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 365 subscribers
  • Views 2058 views
  • Users 0 members are here
Related

Interrupt Handler in Kernel Module

e14 Contributor
e14 Contributor over 13 years ago

Does anyone have a working linux device driver that works for interrupt of custom ip-cores?

The AR 51138 shows an example ip-core that contains an own interrupt controller that supports multiple interrupt sources and registers into the global interrupt controller of the Zynq. But the example software is only bare-metal not linux.

http://www.xilinx.com/support/answers/51138.htm

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    A short while ago i did the same. this is the thread i used to gather infrmation:
    http://forums.xilinx.com/t5/Embedded-Linux/AR-50572-Axi-timer-interrupts-in-linux/td-p/335077

    The driver i posted there is able to start on its own, but you can use a script/application to write&read.
    it stops after 100 interrupts, so you might need/want to change that too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Are you getting printk messages in irq handler.
    I have taken your module and compiled it and inserted this module.
    but i am not getting any messages
    could you please help me out in this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Yes, you should seee a number of messages just by loading the module.
    http://i259.photobucket.com/albums/hh290/Brogath/syscalldriver_zpsa4a391b1.png?t=1375971477

    The url is ascreenshot from my terminal after loading the module.

    you could try to see if the kernel messages appear if you type 'dmesg'.
    if youo do not see any messages at all you coudl try to replace the printk commands (especially in the init procedure) with a version that you know that works for you.

    if you still do not see any messages try to make another module that just prints something after insmod and rmmod and see if the problem remains. (becasue if it doesnt, you might want to check the kernel instead of the module)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Yes, you should seee a number of messages just by loading the module.
    http://i259.photobucket.com/albums/hh290/Brogath/syscalldriver_zpsa4a391b1.png?t=1375971477

    The url is ascreenshot from my terminal after loading the module.

    you could try to see if the kernel messages appear if you type 'dmesg'.
    if youo do not see any messages at all you coudl try to replace the printk commands (especially in the init procedure) with a version that you know that works for you.

    if you still do not see any messages try to make another module that just prints something after insmod and rmmod and see if the problem remains. (becasue if it doesnt, you might want to check the kernel instead of the module)