Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Block design: How to read and write to block RAM?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 362 subscribers
  • Views 4949 views
  • Users 0 members are here
Related

Block design: How to read and write to block RAM?

quadzilla
quadzilla over 2 years ago

This is surely a naive question.  I saw how one can use a block memory generator in the block designs.  It's not clear to me how one can read from or write to the block RAM using the block designs though.  At least, I couldn't find any IP to accomplish this task.

Can this be done via block design?  Or can it only be done via supplementary HDL code?  (I lack experience when it comes to doing so via Verilog or VHDL, so I was hoping that a block design would do the trick.)



image

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 2 years ago +2
    What's the end game here - without knowing where or what you want to write to the block ram it's not possible to answer your question. The kind of thing I mean is that, for example, you might have an…
  • padudle
    padudle over 2 years ago in reply to shabaz +1
    This a very standard way to use dual-port block ram. One side is wired to the processor so that it can accessed from software. The other side is connected to some part of your fpga logic. The clocks be…
Parents
  • michaelkellett
    michaelkellett over 2 years ago

    What's the end game here - without knowing where or what you want to write to the block ram it's not possible to answer your question.

    The kind of thing I mean is that, for example, you might have an ADC writing to the block RAM and read the data from a RAM port using the AXI controller.

    I'm working now on a system that does exactly that but it doesn't use Xilinx(AMD) FPGAs and all the FPGA stuff is done in VHDL.

    As Shabaz has said, typically you will need to use VHD or Verilog to interface the custom side of the design to the Xilinx IP stuff.

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • quadzilla
    quadzilla over 2 years ago in reply to michaelkellett

    Sorry for the late reply.  The end game here was just a simple  preliminary test -- to have the FPGA generate data, store it in block RAM, and have the PS read this data out.  The more complicated implementation will come much later.

    Thanks for all the tips, folks.  I eventually figured out how to do this without writing any VHDL or Verilog code.  Again, because this was just a simple initial test and I was making some naive mistakes at first.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • quadzilla
    quadzilla over 2 years ago in reply to michaelkellett

    Sorry for the late reply.  The end game here was just a simple  preliminary test -- to have the FPGA generate data, store it in block RAM, and have the PS read this data out.  The more complicated implementation will come much later.

    Thanks for all the tips, folks.  I eventually figured out how to do this without writing any VHDL or Verilog code.  Again, because this was just a simple initial test and I was making some naive mistakes at first.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • dyessgg
    dyessgg over 2 years ago in reply to quadzilla

    If you're just writing a stream of data into the block RAM and reading it out as a stream, look into using a FIFO block.  You can write into it with a much simplified AXI Stream interface.  You won't have to worry about addresses, wrap-around, etc.