Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Block design: How to read and write to block RAM?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 362 subscribers
  • Views 4947 views
  • Users 0 members are here
Related

Block design: How to read and write to block RAM?

quadzilla
quadzilla over 2 years ago

This is surely a naive question.  I saw how one can use a block memory generator in the block designs.  It's not clear to me how one can read from or write to the block RAM using the block designs though.  At least, I couldn't find any IP to accomplish this task.

Can this be done via block design?  Or can it only be done via supplementary HDL code?  (I lack experience when it comes to doing so via Verilog or VHDL, so I was hoping that a block design would do the trick.)



image

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 2 years ago +2
    What's the end game here - without knowing where or what you want to write to the block ram it's not possible to answer your question. The kind of thing I mean is that, for example, you might have an…
  • padudle
    padudle over 2 years ago in reply to shabaz +1
    This a very standard way to use dual-port block ram. One side is wired to the processor so that it can accessed from software. The other side is connected to some part of your fpga logic. The clocks be…
Parents
  • shabaz
    shabaz over 2 years ago

    That AXI interconnect in your diagram has to go to the Processing Subsystem (PS). Then you would use code (software) to read/write to BRAM.

    The AXI interconnect can't (I believe) be used without the PS (there are hundreds of signals between the AXI interconnect and the PS). 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • quadzilla
    quadzilla over 2 years ago in reply to shabaz

    I should have been more clear.  I was wondering how the FPGA fabric can write to the block RAM, after which the PS would read the contents.  (In the full diagram, the AXI interconnect is indeed connected to the PS.)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to quadzilla

    Your block RAM should have two ports. I would point you to a blog post which shows this, but there are site issues.

    I can't see how you're aiming to use it without writing a word of HDL..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • padudle
    padudle over 2 years ago in reply to shabaz

    This a very standard way to use dual-port block ram. One side is wired to the processor so that it can accessed from software.  The other side is connected to some part of your fpga logic. The clocks be and the ports widths can be different. Just make one of the ports external in your IPI block diagram and you can wire that side of the memory to your HDL.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • quadzilla
    quadzilla over 2 years ago in reply to shabaz

    Thanks for the pointers. I did eventually manage to implement this using nothing but block designs (i.e. no HDL).  It was just a simple test though, and HDL will doubtlessly be needed after we've designed the system more thoroughly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • padudle
    padudle over 2 years ago in reply to padudle

    The bram port that is connected to the axi block ram controller should not have any extra pipelining enabled. For reads, he controller expects to put the address on the bram one clock cycle and get the data on the next.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • padudle
    padudle over 2 years ago in reply to padudle

    The bram port that is connected to the axi block ram controller should not have any extra pipelining enabled. For reads, he controller expects to put the address on the bram one clock cycle and get the data on the next.