Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design Pynq with Ultra96
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 366 subscribers
  • Views 1690 views
  • Users 0 members are here
Related

Pynq with Ultra96

micallef25
micallef25 over 6 years ago

Hi All,

 

I am using SdSoC to generate a bit and elf file.

 

Is there a way to execute these on a PYNQ platform? I can execute elf that have no associated bitstreams no problem with PYNQ

 

But when I try to execute an elf that has hardware nothing happens. I read about the PYNQ overlays but was a bit confused. Do I use the overlays to re program the fabric and then I can execute the elf?

 

Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • drozwood90
    drozwood90 over 6 years ago +1
    Hi there, While what you are asking is technically, probably possible, it is not a supported flow at this time. As python has the ability to launch applications, you would need to ensure that all the proper…
  • narrucmot
    narrucmot over 6 years ago in reply to micallef25 +1
    Hi Eric, Where do you have the other end of the Ethernet cable connected? Directly to the host PC, or to a router/switch? If directly to a PC (and if the PC is not running a DHCP server) you will need…
  • narrucmot
    narrucmot over 6 years ago in reply to micallef25 +1
    I have been able to achieve ~740Mbps with the TU3-ETG adapter on my Ultra96-V2 board: This test was with the DisplayPort monitor connected, other USB ports idle, and WiFi inactive. The iperf3 server was…
Parents
  • jhane
    jhane over 6 years ago

    pynq is python so I'm not sure how that would help you.  However, if you build an image with the fpga manager it supports loading of bitstreams and linux devicetree overlays.  I haven't used SDSoC so can't say for sure this is what you  need but it sounds closer since it doesn't use python.

     

    jeff

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jhane
    jhane over 6 years ago

    pynq is python so I'm not sure how that would help you.  However, if you build an image with the fpga manager it supports loading of bitstreams and linux devicetree overlays.  I haven't used SDSoC so can't say for sure this is what you  need but it sounds closer since it doesn't use python.

     

    jeff