Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design RTL-kernel wizard example not working on ultra96
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 364 subscribers
  • Views 1836 views
  • Users 0 members are here
  • rtl-kernel-wizard
  • ultra96
  • open-cl
  • vitis
Related

RTL-kernel wizard example not working on ultra96

ece7498
ece7498 over 5 years ago

Hello,

I am trying to run the rtl-kernel wizard example on the ultra96. Where the same example is running fine on zcu102 and zcu104.

I am using the predefined avnet platform on Vitis, which I downloaded from your repository and I am running smoothly Vadd application on kernel. But when I run the example the Output is wrong and TEST FAILS. Here is the log:

root@ultra96v2-2020-1:/mnt/sd-mmcblk0p1/Projects/hello# ./dilithium vector_addition.xclbin

source_a[0]+source_b[0]=source_results[0]

10+32=0

[  219.740682] [drm] Pid 1124 opened device

[  219.747835] [drm] Pid 1124 closed device

[  219.752061] [drm] Pid 1124 opened device

[  219.756033] [drm] Pid 1124 closed device

Found Platform

Platform Name: Xilinx

INFO: Reading vector_addition.xclbin

Loading: 'vector_addition.xclbin'

[  220.010725] [drm] Pid 1124 opened device

Trying to program device[0]: edge

[  220.030024] [drm] sched_reset_exec: stop scheduler

[  220.030154] [drm] Finding IP_LAYOUT section header

[  220.034968] [drm] Section IP_LAYOUT details:

[  220.039765] [drm]   offset = 0x54fcf0

[  220.044023] [drm]   size = 0x58

[  220.047717] [drm] Finding DEBUG_IP_LAYOUT section header

[  220.050862] [drm] AXLF section DEBUG_IP_LAYOUT header not found

[  220.056177] [drm] Finding CONNECTIVITY section header

[  220.062100] [drm] Section CONNECTIVITY details:

[  220.067149] [drm]   offset = 0x54fd48

[  220.071667] [drm]   size = 0x28

[  220.075348] [drm] Finding MEM_TOPOLOGY section header

[  220.078504] [drm] Section MEM_TOPOLOGY details:

[  220.083552] [drm]   offset = 0x54fbf8

[  220.088073] [drm]   size = 0xf8

[  220.091763] [drm] Download new XCLBIN 6EA32464-41AE-4C49-8572-D4D2C86700B1 done.

[  220.094915] [drm] zocl_xclbin_read_axlf 6ea32464-41ae-4c49-8572-d4d2c86700b1 ret: 0.

[  220.104695] [drm] -> Hold xclbin 6EA32464-41AE-4C49-8572-D4D2C86700B1, from ref=0

[  220.112452] [drm] <- Hold xclbin 6EA32464-41AE-4C49-8572-D4D2C86700B1, to ref=1

[  220.119977] [drm] No ERT scheduler on MPSoC, using KDS

[  220.132510] [drm] scheduler config ert(0)

[  220.132511] [drm]   cus(1)

[  220.136511] [drm]   slots(16)

[  220.139210] [drm]   num_cu_masks(1)

[  220.142169] [drm]   cu_shift(16)

[  220.145648] [drm]   cu_base(0xb0000000)

[  220.148862] [drm]   polling(0)

[  220.152723] [drm] -> Release xclbin 6EA32464-41AE-4C49-8572-D4D2C86700B1, from ref=1

[  220.155774] [drm] now xclbin can be changed

[  220.163532] [drm] <- Release xclbin 6EA32464-41AE-4C49-8572-D4D2C86700B1, to ref=0

[  220.167966] [drm] -> Hold xclbin 6EA32464-41AE-4C49-8572-D4D2C86700B1, from ref=0

Device[0]: program successful!

Result =

source_a[0]+source_b[0]=source_results[0]

10+10=0

Err[  220.175552] [drm] <- Hold xclbin 6EA32464-41AE-4C49-8572-D4D2C86700B1, to ref=1

or: Result mismatch:

i = 0 CPU result = 20 Device result = 0

T[  220.190145] [drm] -> Release xclbin 6EA32464-41AE-4C49-8572-D4D2C86700B1, from ref=1

EST FAILED

[  220.201311] [drm] now xclbin can be changed

[  220.214599] [drm] <- Release xclbin 6EA32464-41AE-4C49-8572-D4D2C86700B1, to ref=0

[  220.223994] [drm] Pid 1124 closed device

 

I have concluded that probably there is an error with the BASE_ADDRESS of the board at non-hls-apps, as I am facing the same error on OpenCL Hello World example (where with HLS Hello World I don't have errors).

 

Has anyone faced the same error? Has anyone ran successfully the rtl-kernel wizard example?

Thanks,
AE