Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design SSD on the Ultra96v2 feasibility
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 366 subscribers
  • Views 2316 views
  • Users 0 members are here
  • ultra96
Related

SSD on the Ultra96v2 feasibility

riltonf
riltonf over 5 years ago

Is there a possible way to get an SSD connected to the Ultra96V2 and be able to boot from it? The Zynq Ultrascale+ seems to support SATA and PCIE, but there are no such connectors on the board for that. Could I maybe be able to create a custom Mezzanine card that brings out the required pins through the HS connector?

I haven't looked too much into the wiring of the SATA/PCIE. I know that reference boards of the Zynq Ultrascale+ from Xilinx has both SATA and PCIE connectors. What's the feasibility of this on the Ultra96v2?

 

Also would ssd to emmc converter modules work? https://www.seeedstudio.com/eMMC-Module-Adapter-for-ROCK-PI-4-p-4142.html

  • Sign in to reply
  • Cancel

Top Replies

  • mindaugas
    mindaugas over 5 years ago +1
    Hi riltonf , I have succesfully ran PYNQ rootfs from USB 3.0 flash drive on Ultra96. I did this because read speed from SD card was ~25MB/s, while reading from USB 3.0 flash drive was ~250MB/s. I think…
  • mindaugas
    mindaugas over 5 years ago in reply to riltonf +1
    I am booting BOOT.bin (FSBL, u-boot) and image.ub (kernel) from SD card and loading just rootfs from usb flash drive. To boot rootfs from usb I changed bootargs in device tree from root=/dev/mmcblk0p2…
  • narrucmot
    narrucmot over 5 years ago +1
    Unfortunately there aren't any transceivers brought out to the high speed mezzanine connector on the Ultra96-V2, so connecting a SATA SSD will not be possible. However, connecting a USB 3.0 disk or Flash…
  • spinden
    spinden over 5 years ago

    Interesting idea. From what I see in the schematic, only SPI and a few GPIO go/from the HS connector to the processors side of the SoC. If you go through the fabric, there may be some options but then you have to do custom hardware and I think you are going to be very limited in speed passing data to the processor.

     

    -David

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mindaugas
    mindaugas over 5 years ago

    Hi riltonf,

     

    I have succesfully ran PYNQ rootfs from USB 3.0 flash drive on Ultra96. I did this because read speed from SD card was ~25MB/s, while reading from USB 3.0 flash drive was ~250MB/s. I think you could do the same by connecting SSD to USB 3.0 port.

     

    With best regards,

    Mindaugas Sulcas

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • riltonf
    riltonf over 5 years ago in reply to mindaugas

    Do you only have uboot on the micro-sd and the kernel, bitstream, and the rootfs on the usb? Can you paste the config?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mindaugas
    mindaugas over 5 years ago in reply to riltonf

    I am booting BOOT.bin (FSBL, u-boot) and image.ub (kernel) from SD card and loading just rootfs from usb flash drive. To boot rootfs from usb I changed bootargs in device tree from root=/dev/mmcblk0p2 to root=/dev/sda1. Also if not written I suggest to add rootwait in bootargs.

     

    With best regards,

    Mindaugas Sulcas

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • narrucmot
    narrucmot over 5 years ago

    Unfortunately there aren't any transceivers brought out to the high speed mezzanine connector on the Ultra96-V2, so connecting a SATA SSD will not be possible.  However, connecting a USB 3.0 disk or Flash drive is something many people have done.

     

    --Tom

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • riltonf
    riltonf over 5 years ago in reply to narrucmot

    Going a bit off topic here, I see that the USB3's and mDP use the GT lanes, and there only seem to be up to 4 GT lanes on the board, all from bank 505. Two go to the USB3's, and two go to the mDP.

    Hypothetically I could route the GT-lane2 to the SATA0 instead of USB0 (only usb3 would be affected, USB2 should still function as normal. I think? Because I'm not changing ULPI).

    Afterwards, using a microA/B cable, stripping the SSTX and SSRX to be wired to SATA's A and B pins, respectively. This should in theory work I believe.

     

    What are your thoughts? I might try to make this this weekend. I just hope I won't break anything.

     

    P.S. Seeing as there are only 4 GT lanes available, was it the intention that you have to make a choice between PCIe x1/x2/x4, SATA, USB3, and DP combinations? Is this a limitation of this specific Zynq Ultrascale+ model?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • spinden
    spinden over 5 years ago

    The new Xilinx Kria K26 a board that may be more what is needed. The datasheet (https://www.xilinx.com/support/documentation/data_sheets/ds987-k26-som.pdf ) show both PL and PS transceivers going to the connectors on the block diagram on page 3.

     

    -David