Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design SSD on the Ultra96v2 feasibility
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 366 subscribers
  • Views 2259 views
  • Users 0 members are here
  • ultra96
Related

SSD on the Ultra96v2 feasibility

riltonf
riltonf over 5 years ago

Is there a possible way to get an SSD connected to the Ultra96V2 and be able to boot from it? The Zynq Ultrascale+ seems to support SATA and PCIE, but there are no such connectors on the board for that. Could I maybe be able to create a custom Mezzanine card that brings out the required pins through the HS connector?

I haven't looked too much into the wiring of the SATA/PCIE. I know that reference boards of the Zynq Ultrascale+ from Xilinx has both SATA and PCIE connectors. What's the feasibility of this on the Ultra96v2?

 

Also would ssd to emmc converter modules work? https://www.seeedstudio.com/eMMC-Module-Adapter-for-ROCK-PI-4-p-4142.html

  • Sign in to reply
  • Cancel

Top Replies

  • mindaugas
    mindaugas over 5 years ago +1
    Hi riltonf , I have succesfully ran PYNQ rootfs from USB 3.0 flash drive on Ultra96. I did this because read speed from SD card was ~25MB/s, while reading from USB 3.0 flash drive was ~250MB/s. I think…
  • mindaugas
    mindaugas over 5 years ago in reply to riltonf +1
    I am booting BOOT.bin (FSBL, u-boot) and image.ub (kernel) from SD card and loading just rootfs from usb flash drive. To boot rootfs from usb I changed bootargs in device tree from root=/dev/mmcblk0p2…
  • narrucmot
    narrucmot over 5 years ago +1
    Unfortunately there aren't any transceivers brought out to the high speed mezzanine connector on the Ultra96-V2, so connecting a SATA SSD will not be possible. However, connecting a USB 3.0 disk or Flash…
Parents
  • narrucmot
    narrucmot over 5 years ago

    Unfortunately there aren't any transceivers brought out to the high speed mezzanine connector on the Ultra96-V2, so connecting a SATA SSD will not be possible.  However, connecting a USB 3.0 disk or Flash drive is something many people have done.

     

    --Tom

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • riltonf
    riltonf over 5 years ago in reply to narrucmot

    Going a bit off topic here, I see that the USB3's and mDP use the GT lanes, and there only seem to be up to 4 GT lanes on the board, all from bank 505. Two go to the USB3's, and two go to the mDP.

    Hypothetically I could route the GT-lane2 to the SATA0 instead of USB0 (only usb3 would be affected, USB2 should still function as normal. I think? Because I'm not changing ULPI).

    Afterwards, using a microA/B cable, stripping the SSTX and SSRX to be wired to SATA's A and B pins, respectively. This should in theory work I believe.

     

    What are your thoughts? I might try to make this this weekend. I just hope I won't break anything.

     

    P.S. Seeing as there are only 4 GT lanes available, was it the intention that you have to make a choice between PCIe x1/x2/x4, SATA, USB3, and DP combinations? Is this a limitation of this specific Zynq Ultrascale+ model?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • riltonf
    riltonf over 5 years ago in reply to narrucmot

    Going a bit off topic here, I see that the USB3's and mDP use the GT lanes, and there only seem to be up to 4 GT lanes on the board, all from bank 505. Two go to the USB3's, and two go to the mDP.

    Hypothetically I could route the GT-lane2 to the SATA0 instead of USB0 (only usb3 would be affected, USB2 should still function as normal. I think? Because I'm not changing ULPI).

    Afterwards, using a microA/B cable, stripping the SSTX and SSRX to be wired to SATA's A and B pins, respectively. This should in theory work I believe.

     

    What are your thoughts? I might try to make this this weekend. I just hope I won't break anything.

     

    P.S. Seeing as there are only 4 GT lanes available, was it the intention that you have to make a choice between PCIe x1/x2/x4, SATA, USB3, and DP combinations? Is this a limitation of this specific Zynq Ultrascale+ model?