Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design Problem about access the output signal of vivado blocks
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 366 subscribers
  • Views 976 views
  • Users 0 members are here
Related

Problem about access the output signal of vivado blocks

pmuproject
pmuproject over 7 years ago

Hello there,

I'm current building a clock source in vivado by using the clk_wiz module. The output clock is the clk_out1 pin on the clk_wiz module. When I finish the design of vivado and export it to SDK I found that there is nothing can be used related to the clk_out1 pin. Just woundering how can I access to the clk_wiz and output the clk_out1 signal to a gpio pin in SDK?

Regards,

Han

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 7 years ago

    hello Han,

    Did you make your signal external and write constraints to output the signal to a specific GPIO pin?

    -Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • pmuproject
    0 pmuproject over 7 years ago in reply to jafoste4

    Hi Josh,

    Yes I made a external of the output clock from clk_wiz but I didn't write constraints for it in my .xdc file. I wrote all the gpio pins with the correspoding information from Ultra96 Schematic. Do I need to connect the output signal to the GPIO Pin directly such as :

    set_property PACKAGE_PIN D10  [get_ports { clk_out1_1       }];

    or set_property MIO36_PS_GPIO1_0  [get_ports {clk_out1_1        }];

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • pmuproject
    0 pmuproject over 7 years ago in reply to jafoste4

    Hi Josh,

    Yes I made a external of the output clock from clk_wiz but I didn't write constraints for it in my .xdc file. I wrote all the gpio pins with the correspoding information from Ultra96 Schematic. Do I need to connect the output signal to the GPIO Pin directly such as :

    set_property PACKAGE_PIN D10  [get_ports { clk_out1_1       }];

    or set_property MIO36_PS_GPIO1_0  [get_ports {clk_out1_1        }];