Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design Ultra96 died
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 11 replies
  • Answers 1 answer
  • Subscribers 369 subscribers
  • Views 1687 views
  • Users 0 members are here
Related

Ultra96 died

andycap
andycap over 7 years ago

Hi Guys,

 

My Ultra 96 just died, I was stepping through with the debugger and noticed the fan stopping.

All lights out, and now won't power up.

 

I have tested the PSU and that is fine.

Anyone any ideas?

 

Cheers

 

Andy

  • Sign in to reply
  • Cancel

Top Replies

  • ctammann
    ctammann over 6 years ago in reply to slimt +2 suggested
    ok, so in the past instances something failed on the board. KILL_N is an output of the ZU+ on MIO34. If the user creates a design that mis-handles MIO34, then they could be inadvertently forcing the shutdown…
  • andycap
    0 andycap over 7 years ago

    Here are some readings:

     

    POWER_PB_B = 1.95v

    PS_POR_PB_B = 3.3V

    VSYS_IN = 12.273

    VCC_5V0 = 0V

    VCC_PSAUX = 0V

     

    Pressing the on button raises VCC_5V0 to 5V and then it falls to 0.

    Pressing the on button raises VCC_PSAUX to 0.8V and then it falls to 0.

     

    These were just done with a meter, I can grab some scope readings from VCC_5V0 and VCC_PSAUX if that would be usefull?

     
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 7 years ago

    Hi acapon,

    How long have you had the board for? If you have had it for less then 60 days, I would suggest you contact your local Avnet office for an RMA as the product is still under warranty.

    If you have had it for more then 60 days, I can do my best to help you trouble shoot.

    -Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • andycap
    0 andycap over 7 years ago

    Hi Josh,

    Farnell in the UK have replaced it for me.

    Haven't tried the replacement yet, fingers crossed!

     

    Andy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ctammann
    0 ctammann over 7 years ago

    Hey Andy,

    Were you running anything intensive on the board when it failed? Was the fan running? This is the first failure like this I've heard of, my first thought is potentially thermal so I was curious about the run conditions.

    thanks
    Chris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • andycap
    0 andycap over 7 years ago

    Fan was running up to the point it died.

    Nothing intensive was going on, linux was not running. I was testing out a PWM AIX component to one of the gpios and stepping through the code in the debugger over jtag.

    there seems to be something similar maybe here: http://community.avnet.com/t5/Other-Avnet-Boards/Ultra96-board-won-t-power-up/td-p/19573

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • andycap
    0 andycap over 7 years ago

    Is there no thermal cutoff ob the board?

    I had in previous days used the gpio to turn the fan on and off, maximum fan off time would have been < 10 secs.

    I am going to be attaching the design I am working on and to the fan signal in the coming days do I have to be aware that the board won't power down if temps get too hot?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100helgelangen
    0 100helgelangen over 6 years ago

    Reviving this thread since I have the same problem, just with an Ultra96-V2. Reading 12.1 V on VIN, 3.32 V on 3V3_PRI, 0 V on 5V0. Curiously, I'm also reading 0 V on the KILL_N input to the ON/OFF controller and the same for the EN output of it (which is obviously why the 5V regulator does not turn on). Has anybody looked into if this might be a design flaw, particularly regarding the ON/OFF controller circuit? What can I do to bring my board back to life?

     

    Also, does anyone know where to find the datasheet for the SLG4G42480V ON/OFF controller? Google tells me nothing beyond that it's probably manufactured by Dialog and distributed by Avnet...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • slimt
    0 slimt over 6 years ago

    Hi, bumping since I have the same problem. A coworker came to me after the Ultra96-V2 he is working on seemingly died.

    The 3V3 LED and other indicators would light up for only a second after pressing SW4.

     

    I traced the problem back to the interrupt controller SLG4G42480V ON/OFF controller. The signal KILL_N is pulled low as soon as VCC from the power controllers is pulled high, which effectively kills the power.

     

    I found the datasheet for SLG4G42480V but have no idea how to pull out of this loop and be able to boot up again.

     

    Anybody else had to deal with this?

     

    Cheers

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ctammann
    0 ctammann over 6 years ago in reply to slimt

    I'm looking into this now, one of us will respond shortly. I'm digging through to see if we were able to root cause this failure. If the on/off controller failed we could possibly get around that, but if it is shutting down because something else failed then disabling it would just further fry the board. I'll get back to you asap

    Thanks

    Chris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ctammann
    0 ctammann over 6 years ago in reply to slimt

    ok, so in the past instances something failed on the board.

     

    KILL_N is an output of the ZU+ on MIO34. If the user creates a design that mis-handles MIO34, then they could be inadvertently forcing the shutdown. They could try one of our known-good designs, like our out-of-box design to see if it works with that. If it does, then they need to fix their own design.

     

    If it still fails with one of our known-good designs, then it’s likely a board failure.

     

    That being said, I would check on when you purchased the board and see if it might still be under warranty. We have seen very few of these cases so it doesn't point to a specific issue that could be addressed. Sorry I couldn't be more help.

    Thanks

    Chris

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
>