Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design Ultra96 died
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 11 replies
  • Answers 1 answer
  • Subscribers 369 subscribers
  • Views 1688 views
  • Users 0 members are here
Related

Ultra96 died

andycap
andycap over 7 years ago

Hi Guys,

 

My Ultra 96 just died, I was stepping through with the debugger and noticed the fan stopping.

All lights out, and now won't power up.

 

I have tested the PSU and that is fine.

Anyone any ideas?

 

Cheers

 

Andy

  • Sign in to reply
  • Cancel

Top Replies

  • ctammann
    ctammann over 6 years ago in reply to slimt +2 suggested
    ok, so in the past instances something failed on the board. KILL_N is an output of the ZU+ on MIO34. If the user creates a design that mis-handles MIO34, then they could be inadvertently forcing the shutdown…
Parents
  • 100helgelangen
    0 100helgelangen over 6 years ago

    Reviving this thread since I have the same problem, just with an Ultra96-V2. Reading 12.1 V on VIN, 3.32 V on 3V3_PRI, 0 V on 5V0. Curiously, I'm also reading 0 V on the KILL_N input to the ON/OFF controller and the same for the EN output of it (which is obviously why the 5V regulator does not turn on). Has anybody looked into if this might be a design flaw, particularly regarding the ON/OFF controller circuit? What can I do to bring my board back to life?

     

    Also, does anyone know where to find the datasheet for the SLG4G42480V ON/OFF controller? Google tells me nothing beyond that it's probably manufactured by Dialog and distributed by Avnet...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • 100helgelangen
    0 100helgelangen over 6 years ago

    Reviving this thread since I have the same problem, just with an Ultra96-V2. Reading 12.1 V on VIN, 3.32 V on 3V3_PRI, 0 V on 5V0. Curiously, I'm also reading 0 V on the KILL_N input to the ON/OFF controller and the same for the EN output of it (which is obviously why the 5V regulator does not turn on). Has anybody looked into if this might be a design flaw, particularly regarding the ON/OFF controller circuit? What can I do to bring my board back to life?

     

    Also, does anyone know where to find the datasheet for the SLG4G42480V ON/OFF controller? Google tells me nothing beyond that it's probably manufactured by Dialog and distributed by Avnet...