Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design Upgrading Ultra96-v2 Pmic & Heat sink
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 11 replies
  • Answers 2 answers
  • Subscribers 367 subscribers
  • Views 2052 views
  • Users 0 members are here
Related

Upgrading Ultra96-v2 Pmic & Heat sink

skiphs
skiphs over 6 years ago

I picked up an Ultra96-v2 in May last year, and really enjoy it. However, there's two things that have popped up that I'm hoping someone will be able to answer.

 

First, it sounds a bit petty, but the one thing that always discourages me from using it is the volume and pitch of the fan sound.

I saw there was a recent hardware revision that solves this problem by replacing the fan with a heat sink, and I'm wondering if there's any way to purchase the new heat sink myself or send the device in for an "upgrade"?

So far I've mitigated this by including some level of fan control in my projects, but it's a hassle to say the least.

 

The other question is in regards to the Pmic issue. With the recent DPU work being done, I've been looking at pushing what the board can do. My understanding is that there's a 195Mhz clock limit unless the Pmic is upgraded.

Unfortunately, this seems to require an IR dongle. I'm wondering if there's any other way to go about this?

 

 

Ultimately, this is a hobby for me. I can understand if there's nothing that can be done, but I figure there's no harm in asking.

  • Sign in to reply
  • Cancel

Top Replies

  • bhfletcher
    bhfletcher over 6 years ago +2 verified
    We are working on a utility that will allow you to update the Pmic from the MPSoC device, which means no soldering and no Infineon dongle. My colleague ctammann will have more information on that soon…
  • bhfletcher
    bhfletcher over 6 years ago in reply to bhfletcher +1 suggested
    Part Number: AES-ACC-U96-PHS1 Resale: $10 Availability: mid-August estimate Note that if you do some really aggressive stuff, the passive heatsink can get hot as it does quite an amazing job of sucking…
Parents
  • bhfletcher
    0 bhfletcher over 6 years ago

    We are working on a utility that will allow you to update the Pmic from the MPSoC device, which means no soldering and no Infineon dongle. My colleague ctammann will have more information on that soon. I believe he is planning a webinar where this will be one of the things that he demonstrates.

     

    Regarding the heatsink, we have final approval to sell the Ultra96-V2 heatsink as a separate item. This is a passive heatsink that was co-developed between Avnet and Boyd/Aavid Thermalloy. You can see references to this heatsink in several places.

     

    Ultra96-V2 Heatsink Alone

    Thermal relief is critical - design example around Ultra96-V2

    Industrial Temperature Ultra96-V2 Single Board Computer

     

    I will check to see when you will be able to order this, what the PN is, and what we expect the cost to be.

     

    Bryan

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 6 years ago in reply to bhfletcher

    Part Number:     AES-ACC-U96-PHS1

    Resale:              $10

    Availability:        mid-August estimate

     

    Note that if you do some really aggressive stuff, the passive heatsink can get hot as it does quite an amazing job of sucking the heat away from the MPSoC and PMICs. However, just be cautious that you don't handle it while cranking out DPU algorithms at 250+ MHz. A small desktop fan or add-on fan will drop the temp immediately by 20C, so you may not get away from the fan in cases where you are pushing the board to its performance limits.

     

    Bryan

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jlamp
    0 jlamp over 6 years ago in reply to bhfletcher

    Hi,

     

    I would like to update the PMIC but I don't have any Infineon dongle. What do I need to do? Is the MPSoC utility ready?

     

    Regards,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ctammann
    0 ctammann over 6 years ago in reply to jlamp

    We are working on a software based solution to update the PMICs using an SDcard image. That process isn't fully released yet, but as soon as it is I will post an announcement in this forum and make the image available.

    Thanks

    Chris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jlamp
    0 jlamp over 6 years ago in reply to ctammann

    Thank you Chris for your support,

     

    Do you think that this release will come out before the end of the month? I am doing lpcv.ai fpga competition which ends the 1st of August and I would like to know if I can wait  or else I have to buy Infineon programming dongle.

     

    Do I need a license for Infineon PowIRCenter GUI software?

     

    Regards.

    Jorge

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jlamp
    0 jlamp over 6 years ago in reply to bhfletcher

    Hi Bryan,

     

    After fixing PMIC which is the maximum frequency that I can use for DPU? Can I use 325/650Mhz?

     

    Best regards,

     

    Jorge

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jlamp
    0 jlamp over 6 years ago in reply to bhfletcher

    Hi Bryan,

     

    After fixing PMIC which is the maximum frequency that I can use for DPU? Can I use 325/650Mhz?

     

    Best regards,

     

    Jorge

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • narrucmot
    0 narrucmot over 5 years ago in reply to jlamp

    Hi Jorge,

     

    This article on Hackster.io should answer your questions about max frequency for the DPU in the Ultra96-V2:

    http://avnet.me/vitis-ai-1.2-project

     

    In particular the section "Known Issues - Ultra96-V2 PMIC firmware update".

    https://www.hackster.io/AlbertaBeef/vitis-ai-1-2-flow-for-avnet-vitis-platforms-7cb3aa#toc-known-issues---ultra96-v2-pmi…

     

    --Tom