Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design PetaLinux u-boot issue with ultra96v2
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 365 subscribers
  • Views 5083 views
  • Users 0 members are here
Related

PetaLinux u-boot issue with ultra96v2

talvlad29
talvlad29 over 6 years ago

HI,

I work with ultra96v2 board from AVNET (Part="xczu3eg-sbva484-1-e"). I created HW design (I used vivado 2019.2) based on step by step tutorial (https://highlevel-synthesis.com/2019/11/07/how-to-create-ultra96v2-linux-based-platform-in-xilinx-vitis-2019-2/comment-page-1/#comment-1383) and build PetaLinux package (I used PetaLinux 2019.2). I tried to run it from SD card but it got stuck at boot stage (boot mode was selected to boot from SD). I tried to download the same image via JTAG and received the following response:

vladimir@vladimir-virtual:~/vitis/ultra96v2_vitis_pkg/ultra96v2-petalinux$
vladimir@vladimir-virtual:~/vitis/ultra96v2_vitis_pkg/ultra96v2-petalinux/images/linux$ petalinux-boot --jtag --u-boot --fpga --pmufw
INFO: sourcing build tools
INFO: Use bitstream: "/home/vladimir/vitis/ultra96v2_vitis_pkg/ultra96v2-petalinux/images/linux/system.bit.
INFO: Please use --fpga --bitstream <BITSTREAM> to specify a bitstream if you want to use other bitstream.
INFO: Launching XSDB for file download and boot.
INFO: This may take a few minutes, depending on the size of your image.
rlwrap: warning: your $TERM is 'xterm-256color' but rlwrap couldn't find it in the terminfo database. Expect some problems.: Inappropriate ioctl for device
INFO: Configuring the FPGA...
INFO: Downloading bitstream: /home/vladimir/vitis/ultra96v2_vitis_pkg/ultra96v2-petalinux/images/linux/system.bit to the target.
INFO: Downloading ELF file: /home/vladimir/vitis/ultra96v2_vitis_pkg/ultra96v2-petalinux/images/linux/pmufw.elf to the target.
INFO: Downloading ELF file: /home/vladimir/vitis/ultra96v2_vitis_pkg/ultra96v2-petalinux/images/linux/zynqmp_fsbl.elf to the target.
INFO: Downloading ELF file: /home/vladimir/vitis/ultra96v2_vitis_pkg/ultra96v2-petalinux/images/linux/u-boot.elf to the target.
Memory write error at 0x8000000. MMU fault at VA 0x8000000. Translation fault, second level
invoked from within
"::tcf::eval -progress {
apply {{info} {
switch -- [lindex $info 0] {
"info" {
puts -nonewline "\r[lindex $info 1]"
}
"warning" {
puts "\n[lindex $info 1]"
}
"data" {
puts -nonewline "\r[lindex $info 1] of [lindex $info 2] complete"
}
"done" {
puts "\n[lindex $info 1]"
}
}
flush stdout
::xsdb::abort_check
}}} {::tcf::cache_enter tcfchan#0 {tcf_cache_eval {download_cache_client ::tcfclient#0::arg}}}"
(procedure "::tcf::cache_eval_with_progress" line 2)
invoked from within
"::tcf::cache_eval_with_progress $params(chan) [list download_cache_client $argvar] {
apply {{info} {
switch -- [lindex $info 0] {
"info" ..."
(procedure "dow" line 78)
invoked from within
"dow "/home/vladimir/vitis/ultra96v2_vitis_pkg/ultra96v2-petalinux/images/linux/u-boot.elf""
(file "/tmp/tmp.tBvV3aPdLo" line 28)
INFO: The XSDB log is as follows
attempting to launch hw_server

****** Xilinx hw_server v2019.2
**** Build date : Oct 23 2019 at 23:11:29
** Copyright 1986-2019 Xilinx, Inc. All Rights Reserved.

INFO: hw_server application started
INFO: Use Ctrl-C to exit hw_server application

INFO: To connect to this hw_server instance use url: TCP:127.0.0.1:3121

100% 5MB 0.8MB/s 00:06
Downloading Program -- /home/vladimir/vitis/ultra96v2_vitis_pkg/ultra96v2-petalinux/images/linux/pmufw.elf
section, .vectors.reset: 0xffdc0000 - 0xffdc0007
section, .vectors.sw_exception: 0xffdc0008 - 0xffdc000f
section, .vectors.interrupt: 0xffdc0010 - 0xffdc0017
section, .vectors.hw_exception: 0xffdc0020 - 0xffdc0027
section, .text: 0xffdc0050 - 0xffdd11bb
section, .rodata: 0xffdd11bc - 0xffdd32d3
section, .data: 0xffdd32d4 - 0xffdd75cb
section, .sdata2: 0xffdd75cc - 0xffdd75cf
section, .sdata: 0xffdd75d0 - 0xffdd75cf
section, .sbss: 0xffdd75d0 - 0xffdd75cf
section, .bss: 0xffdd75e0 - 0xffddb60f
section, .srdata: 0xffddb610 - 0xffddbf33
section, .stack: 0xffddbf34 - 0xffddcf37
section, .xpbr_serv_ext_tbl: 0xffddf6e0 - 0xffddfadf
100% 0MB 0.0MB/s 00:02
Setting PC to Program Start Address 0xffdd03dc
Successfully downloaded /home/vladimir/vitis/ultra96v2_vitis_pkg/ultra96v2-petalinux/images/linux/pmufw.elf
Downloading Program -- /home/vladimir/vitis/ultra96v2_vitis_pkg/ultra96v2-petalinux/images/linux/zynqmp_fsbl.elf
section, .text: 0xfffc0000 - 0xfffce353
section, .init: 0xfffce380 - 0xfffce3b3
section, .fini: 0xfffce3c0 - 0xfffce3f3
section, .note.gnu.build-id: 0xfffce3f4 - 0xfffce417
section, .rodata: 0xfffce440 - 0xfffce8b7
section, .sys_cfg_data: 0xfffce8c0 - 0xfffcf117
section, .mmu_tbl0: 0xfffd0000 - 0xfffd000f
section, .mmu_tbl1: 0xfffd1000 - 0xfffd2fff
section, .mmu_tbl2: 0xfffd3000 - 0xfffd6fff
section, .data: 0xfffd7000 - 0xfffd83b7
section, .sbss: 0xfffd83b8 - 0xfffd83bf
section, .bss: 0xfffd83c0 - 0xfffda47f
section, .heap: 0xfffda480 - 0xfffda87f
section, .stack: 0xfffda880 - 0xfffdc87f
section, .dup_data: 0xfffdc880 - 0xfffddc37
section, .handoff_params: 0xfffe9e00 - 0xfffe9e87
section, .bitstream_buffer: 0xffff0040 - 0xfffffc3f
100% 0MB 0.0MB/s 01:07
Setting PC to Program Start Address 0xfffc0000
Successfully downloaded /home/vladimir/vitis/ultra96v2_vitis_pkg/ultra96v2-petalinux/images/linux/zynqmp_fsbl.elf
Downloading Program -- /home/vladimir/vitis/ultra96v2_vitis_pkg/ultra96v2-petalinux/images/linux/u-boot.elf
section, .data: 0x08000000 - 0x080863a5
aborting, 1 pending requests...
Failed to download /home/vladimir/vitis/ultra96v2_vitis_pkg/ultra96v2-petalinux/images/linux/u-boot.elf

How can I fix this issue?

Thank you,

Vladimir

  • Sign in to reply
  • Cancel

Top Replies

  • quiqueacín
    quiqueacín over 4 years ago +3
    I have just a similar problem with another board (which is not AVNET) but may be can help you. As you I faced the same problem. when I do " petalinux-boot --jtag xxxx ", it gave me the following output…
  • shredEngineer
    shredEngineer over 4 years ago in reply to quiqueacín +2
    Dear Quique, I just registered to say THANK YOU! I found this solution via Google and this solved the same problem for me, using a Xilinx ZCU111 board . Have a nice weekend! Best regards Pau…
Parents
  • narrucmot
    0 narrucmot over 6 years ago

    Hi Vladimir,

     

    This could be something as simple a u-boot configuration issue, or a memory map issue.  There is a clue early on in the boot log:
    Memory write error at 0x8000000. MMU fault at VA 0x8000000. Translation fault, second level

    The address '0x8000000' does not appear to be reachable to store the u-boot executable on JTAG download.

     

    You may want to start with a known-good PetaLinux and Vitis 2019.2 example for the Ultra96-V2 board:

    https://www.element14.com/community/community/designcenter/zedboardcommunity/ultra96#e14tab2

    image

     

    --Tom

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • narrucmot
    0 narrucmot over 6 years ago

    Hi Vladimir,

     

    This could be something as simple a u-boot configuration issue, or a memory map issue.  There is a clue early on in the boot log:
    Memory write error at 0x8000000. MMU fault at VA 0x8000000. Translation fault, second level

    The address '0x8000000' does not appear to be reachable to store the u-boot executable on JTAG download.

     

    You may want to start with a known-good PetaLinux and Vitis 2019.2 example for the Ultra96-V2 board:

    https://www.element14.com/community/community/designcenter/zedboardcommunity/ultra96#e14tab2

    image

     

    --Tom