Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design Mini DP to HDMI converter CD0095
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 365 subscribers
  • Views 1490 views
  • Users 0 members are here
  • video
  • displayport
  • petalinux
Related

Mini DP to HDMI converter CD0095

e14 Contributor
e14 Contributor over 4 years ago

Hi everyone,

I've been working on a MPSoC design with a XU5Ev plateform. I've managed to get a video output from display port controller using petalinux and modetest.

Like many, I'd like to get an HDMI output, which is why I thought about using DP to HDMI adapter. I found this discussion on the forum : /products/devtools/avnetboardscommunity/avnetboard-forums/f/ultra96-hardware-design/38397/ultra96-v2-mini-dp-to-hdmi-adapter

In which the CD0095 seems to the solution. So I got the cable and tried it out !

Unfortunatly, no pattern on screen.

But, I did get the EDID from the screen : 

image

which is quite encouraging.

I did see this two warnings when I disconnected/reconnected the adapter 

image

I'm starting to think that it could be a bug from Xilinx SDK (that wouldn't be a first)

Do you guys use modetest and Petalinux for your tests ? Or do you have another method ? 

I'm starting to think about getting a Ultra96 kit

Regards

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    bhfletcher over 4 years ago

    How many channels have you allocated to DisplayPort in your design? Did you see this comment? "Be aware that the active mini-DP to HDMI CableCreation cable does not support 5.4 Gbps per channel mode and that the ultra96 has only 2 channels for miniDP out."

    I'm not sure about modetest, but I know that our out-of-box design for Ultra96-V2 is PetaLinux-based. Perhaps narrucmot can provide more detail.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 4 years ago in reply to bhfletcher

    Hello Bryan,

    If by channels you mean lanes, the design I use is configured with two lanes for displayport. 

    My assumption of the training phase of displayport is that the controler start with a pattern emitted as HBR2 (5.4 Gbps) then switch to HBR if failing then RBR if failing again. Regarding the comment you mention, I'm thinking that because the adapter does not support HBR2, it would be drived with HBR or RBR automaticly after the training phase (but maybe I'm wrong about that). 

    Perhaps, modetest try only the HBR2 rate and should be modified to use HBR directly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 4 years ago in reply to bhfletcher

    Hello Bryan,

    If by channels you mean lanes, the design I use is configured with two lanes for displayport. 

    My assumption of the training phase of displayport is that the controler start with a pattern emitted as HBR2 (5.4 Gbps) then switch to HBR if failing then RBR if failing again. Regarding the comment you mention, I'm thinking that because the adapter does not support HBR2, it would be drived with HBR or RBR automaticly after the training phase (but maybe I'm wrong about that). 

    Perhaps, modetest try only the HBR2 rate and should be modified to use HBR directly.