Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design Board power via USB UART click mezzanine - expected?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 365 subscribers
  • Views 2698 views
  • Users 0 members are here
  • ultra96v2
  • mezzanine
  • usb
  • click
  • power
Related

Board power via USB UART click mezzanine - expected?

dqlb
dqlb over 4 years ago

I have been experimenting with the USB UART click board included with the click mezzanine starter kit (AES-ACC-U96-ME-SK) and was surprised to see that the USB UART/I2C click board appears to be supplying power to the Ultra96 when connected to a powered USB cable, but when the main 12v barrel jack supply is disconnected. It is possible to power on the board with only the click board USB connected (no 12V barrel jack) though the boot does not complete, presumably due to some detection of low power. Furthermore, the VIN_LED, also lights up when ONLY the click board USB cable is connected (no 12v power supply) although noticeably dimmer.

Looking at the Ultra96v2 schematic, this behaviour appears to make some amount of sense, as the 5V output on the low speed expansion header is directly connected to the main 5V rail that feeds into the "Rocky PMICs". However what I cannot explain is why the VIN_LED, which is supposed to indicate that 12V is connected to the board, would light up when only the 5V USB is connected. There doesn't appear to be any direct connection between the 5V rail and the VIN_LED based on the schematic.

The Ultra96 HW user guide does not mention anything about supplying board power with the 5V pin on the low speed expansion header. Is this expected behaviour, or is there potentially something wrong with my board?

  • Sign in to reply
  • Cancel

Top Replies

  • bhfletcher
    bhfletcher over 4 years ago +3
    Here are a few relevant links to various schematics: MIKROE-1985 https://download.mikroe.com/documents/add-on-boards/click/usb-i2c/usb-i2c-click-schematic-v101.pdf 96Boards Click Mezzanine https:/…
  • ctammann
    ctammann over 4 years ago +3
    The short answer is yes, there is a leakage path from output to input on the 38060 (and most switching regulators). As you may know, supporting power from multiple sources becomes a game of "whack a mole…
  • bhfletcher
    bhfletcher over 4 years ago in reply to bhfletcher +2 verified
    My contact at MikroElektronika gave me the following information Some of the early Click boards were developed without a diode. It was intentionally allowed to power up your board with the peripherals…
Parents
  • dougw
    0 dougw over 4 years ago

    I can't picture the circuit arrangement and I don't have these boards to examine but the MIKROE-1985 USB-UART Click can generate full RS232 signals, which means it probably generates +-12 volts on the card. I have no idea if these voltages can make their way to the indicator but it is something to check.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dougw
    0 dougw over 4 years ago

    I can't picture the circuit arrangement and I don't have these boards to examine but the MIKROE-1985 USB-UART Click can generate full RS232 signals, which means it probably generates +-12 volts on the card. I have no idea if these voltages can make their way to the indicator but it is something to check.