Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design Ultra96 FPGA board stopped working after few minutes - LEDs only flashing
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 365 subscribers
  • Views 863 views
  • Users 0 members are here
  • ultra96-v2
  • avnet_ultra96
  • hardware
  • avnet design
  • avnet
  • ultra96_hardware
  • ultrascale+
  • avnet_product
Related

Ultra96 FPGA board stopped working after few minutes - LEDs only flashing

xcatpc
xcatpc over 3 years ago

Long time ago, I guess it was around 2020, I bought a Ultra96 board.
I played around a bit and then it was stored in good conditions.
Yesterday I tried to start a new project and it worked but suddenly I the board was of. As I tried to start it again I realized that all LEDs are blinking at the same time for a second and then the board don't start. Do you know something about this issue.

I would be very sad, if the board is broken :(

A video of the Ultra96 issue is attached here: https://omesh.io/VID_20231003_212227.mp4

H
opefully I can do something to fix it. 

  • Sign in to reply
  • Cancel
  • lightcollector
    lightcollector over 2 years ago

    Hi, not sure from the video what position the boot dip switches are in.  I also see you have the optional JTAG adapter connected along with an SD card, not sure which boot method you are attempting.

    On page 12 the switches as shown are set to boot from the SD card:

    https://www.avnet.com/wps/wcm/connect/onesite/f21462c6-4997-41a2-a95e-80122b73aea9/Ultra96-V2-GSG-v2_0.pdf?MOD=AJPERES

    If that doesn't fix your issue, not really sure what else it could be.

    Good luck!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • xcatpc
    xcatpc over 2 years ago in reply to lightcollector

    Thank you for your reply!
    I tried every mode its the same issue. I tried also to boot or start the board without the JTAG adapter. 
    I guess its a hardware issue. The interesting thing would be, where the flashing of leds is coming from.