Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design No power on base board
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 362 subscribers
  • Views 1048 views
  • Users 0 members are here
Related

No power on base board

cone83
cone83 over 9 years ago

I just received my Ultrazed starter kit. I tried powering it up but unfortunately the only thing that happens when flipping the power switch is that the power LED lights up. The fan doesn't power up, none of the LEDs on the Ultrazed light up and of course there's no output on the UART.

I measured the voltages on the VMON header and received this:

+ VIN = 12 V
+5.0V =  0V
+3.3V = 0 V
+3.3V_PRI = 3.3 V
+MGTRAVCC = 0.1 V
+MGTRAVTT = 0 V
+VCC1_V8 = 0 V

Did I just receive a faulty base board or am I missing something?
 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    Please make sure JP1 jumper is NOT installed on the UltraZed-EG SOM. Installing this jumper will disable all voltage regulators.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    Please make sure JP1 jumper is NOT installed on the UltraZed-EG SOM. Installing this jumper will disable all voltage regulators.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer