Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design Engineering Silicon / Produciton Silicon diff
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 360 subscribers
  • Views 658 views
  • Users 0 members are here
Related

Engineering Silicon / Produciton Silicon diff

tobinhall
tobinhall over 9 years ago

We have a petalinux image which ethernet works fine on the Engineering silicon / board, but does not work on the Production version.  

Petalinux was generated from hdf export from a vivado project with an empty (other than the ZYNQ block) PL system.  PS was configured for ethernet and such, similar if not identical to the default done by the configuration wizzard.  (this is to support reprogramming the PL system.  Not sure why I need this but but that's another issue for another day.)

Ethernet through u-boot seems to work fine in both cases.

I also noticed that there are different schematics for the Engineering and Production boards.  Both of our setups are the starter kits meaning that each SOM has the carrier designed for it.

1. are there any significant hardware changes in the schematics (besides the ZYNQ) requiring newer versions of software or a different configuration?

2. does the zynq itself require newer versions of software? (petalinux or vivado)

All our tools are 2017.1

  • Sign in to reply
  • Cancel
  • tobinhall
    0 tobinhall over 9 years ago

    Linux boot is as follows

    Production Silicon

    _________________________________

    Starting kernel ...
     
    [    0.000000] Booting Linux on physical CPU 0x0
    [    0.000000] Linux version 4.9.0-xilinx-v2017.1 (hallt@petalinuxHost) (gcc version 6.2.1 20161016 (Linaro GCC 6.2-2016.11) ) #1 SMP Fri Jul 21 11:41:49 PDT 2017
    [    0.000000] Boot CPU: AArch64 Processor [410fd034]
    [    0.000000] earlycon: cdns0 at MMIO 0x00000000ff000000 (options '115200n8')
    [    0.000000] bootconsole [cdns0] enabled
    [    0.000000] cma: Reserved 128 MiB at 0x0000000036000000
    [    0.000000] psci: probing for conduit method from DT.
    [    0.000000] psci: PSCIv1.0 detected in firmware.
    [    0.000000] psci: Using standard PSCI v0.2 function IDs
    [    0.000000] psci: MIGRATE_INFO_TYPE not supported.
    [    0.000000] percpu: Embedded 20 pages/cpu @ffffffc035f7b000 s44056 r8192 d29672 u81920
    [    0.000000] Detected VIPT I-cache on CPU0
    [    0.000000] CPU features: enabling workaround for ARM erratum 845719
    [    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 250480
    [    0.000000] Kernel command line: earlycon clk_ignore_unused root=/dev/nfs nfsroot=172.16.40.137:/tftpboot/nfsroot,tcp ip=dhcp rw uio_pdrv_genirq.of_id=generic-uio
    [    0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)
    [    0.000000] Dentry cache hash table entries: 131072 (order: 8, 1048576 bytes)
    [    0.000000] Inode-cache hash table entries: 65536 (order: 7, 524288 bytes)
    [    0.000000] Memory: 753508K/1015808K available (7358K kernel code, 500K rwdata, 2284K rodata, 448K init, 346K bss, 131228K reserved, 131072K cma-reserved)
    [    0.000000] Virtual kernel memory layout:
    [    0.000000]     modules : 0xffffff8000000000 - 0xffffff8008000000   (   128 MB)
    [    0.000000]     vmalloc : 0xffffff8008000000 - 0xffffffbebfff0000   (   250 GB)
    [    0.000000]       .text : 0xffffff8008080000 - 0xffffff80087b0000   (  7360 KB)
    [    0.000000]     .rodata : 0xffffff80087b0000 - 0xffffff80089f0000   (  2304 KB)
    [    0.000000]       .init : 0xffffff80089f0000 - 0xffffff8008a60000   (   448 KB)
    [    0.000000]       .data : 0xffffff8008a60000 - 0xffffff8008add008   (   501 KB)
    [    0.000000]        .bss : 0xffffff8008add008 - 0xffffff8008b33924   (   347 KB)
    [    0.000000]     fixed   : 0xffffffbefe7fd000 - 0xffffffbefec00000   (  4108 KB)
    [    0.000000]     PCI I/O : 0xffffffbefee00000 - 0xffffffbeffe00000   (    16 MB)
    [    0.000000]     vmemmap : 0xffffffbf00000000 - 0xffffffc000000000   (     4 GB maximum)
    [    0.000000]               0xffffffbf00000000 - 0xffffffbf00d90000   (    13 MB actual)
    [    0.000000]     memory  : 0xffffffc000000000 - 0xffffffc03e000000   (   992 MB)
    [    0.000000] Hierarchical RCU implementation.
    [    0.000000]  Build-time adjustment of leaf fanout to 64.
    [    0.000000]  RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.
    [    0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=64, nr_cpu_ids=4
    [    0.000000] NR_IRQS:64 nr_irqs:64 0
    [    0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000
    [    0.000000] GIC: Using split EOI/Deactivate mode
    [    0.000000] arm_arch_timer: Architected cp15 timer(s) running at 100.00MHz (phys).
    [    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x171024e7e0, max_idle_ns: 440795205315 ns
    [    0.000003] sched_clock: 56 bits at 100MHz, resolution 10ns, wraps every 4398046511100ns
    [    0.008344] Console: colour dummy device 80x25
    [    0.012604] console [tty0] enabled
    [    0.015967] bootconsole [cdns0] disabled
    [    0.000000] Booting Linux on physical CPU 0x0
    [    0.000000] Linux version 4.9.0-xilinx-v2017.1 (hallt@petalinuxHost) (gcc version 6.2.1 20161016 (Linaro GCC 6.2-2016.11) ) #1 SMP Fri Jul 21 11:41:49 PDT 2017
    [    0.000000] Boot CPU: AArch64 Processor [410fd034]
    [    0.000000] earlycon: cdns0 at MMIO 0x00000000ff000000 (options '115200n8')
    [    0.000000] bootconsole [cdns0] enabled
    [    0.000000] cma: Reserved 128 MiB at 0x0000000036000000
    [    0.000000] psci: probing for conduit method from DT.
    [    0.000000] psci: PSCIv1.0 detected in firmware.
    [    0.000000] psci: Using standard PSCI v0.2 function IDs
    [    0.000000] psci: MIGRATE_INFO_TYPE not supported.
    [    0.000000] percpu: Embedded 20 pages/cpu @ffffffc035f7b000 s44056 r8192 d29672 u81920
    [    0.000000] Detected VIPT I-cache on CPU0
    [    0.000000] CPU features: enabling workaround for ARM erratum 845719
    [    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 250480
    [    0.000000] Kernel command line: earlycon clk_ignore_unused root=/dev/nfs nfsroot=172.16.40.137:/tftpboot/nfsroot,tcp ip=dhcp rw uio_pdrv_genirq.of_id=generic-uio
    [    0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)
    [    0.000000] Dentry cache hash table entries: 131072 (order: 8, 1048576 bytes)
    [    0.000000] Inode-cache hash table entries: 65536 (order: 7, 524288 bytes)
    [    0.000000] Memory: 753508K/1015808K available (7358K kernel code, 500K rwdata, 2284K rodata, 448K init, 346K bss, 131228K reserved, 131072K cma-reserved)
    [    0.000000] Virtual kernel memory layout:
    [    0.000000]     modules : 0xffffff8000000000 - 0xffffff8008000000   (   128 MB)
    [    0.000000]     vmalloc : 0xffffff8008000000 - 0xffffffbebfff0000   (   250 GB)
    [    0.000000]       .text : 0xffffff8008080000 - 0xffffff80087b0000   (  7360 KB)
    [    0.000000]     .rodata : 0xffffff80087b0000 - 0xffffff80089f0000   (  2304 KB)
    [    0.000000]       .init : 0xffffff80089f0000 - 0xffffff8008a60000   (   448 KB)
    [    0.000000]       .data : 0xffffff8008a60000 - 0xffffff8008add008   (   501 KB)
    [    0.000000]        .bss : 0xffffff8008add008 - 0xffffff8008b33924   (   347 KB)
    [    0.000000]     fixed   : 0xffffffbefe7fd000 - 0xffffffbefec00000   (  4108 KB)
    [    0.000000]     PCI I/O : 0xffffffbefee00000 - 0xffffffbeffe00000   (    16 MB)
    [    0.000000]     vmemmap : 0xffffffbf00000000 - 0xffffffc000000000   (     4 GB maximum)
    [    0.000000]               0xffffffbf00000000 - 0xffffffbf00d90000   (    13 MB actual)
    [    0.000000]     memory  : 0xffffffc000000000 - 0xffffffc03e000000   (   992 MB)
    [    0.000000] Hierarchical RCU implementation.
    [    0.000000]  Build-time adjustment of leaf fanout to 64.
    [    0.000000]  RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.
    [    0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=64, nr_cpu_ids=4
    [    0.000000] NR_IRQS:64 nr_irqs:64 0
    [    0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000
    [    0.000000] GIC: Using split EOI/Deactivate mode
    [    0.000000] arm_arch_timer: Architected cp15 timer(s) running at 100.00MHz (phys).
    [    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x171024e7e0, max_idle_ns: 440795205315 ns
    [    0.000003] sched_clock: 56 bits at 100MHz, resolution 10ns, wraps every 4398046511100ns
    [    0.008344] Console: colour dummy device 80x25
    [    0.012604] console [tty0] enabled
    [    0.015967] bootconsole [cdns0] disabled
    [    0.019881] Calibrating delay loop (skipped), value calculated using timer frequency.. 200.00 BogoMIPS (lpj=400000)
    [    0.019896] pid_max: default: 32768 minimum: 301
    [    0.020013] Mount-cache hash table entries: 2048 (order: 2, 16384 bytes)
    [    0.020023] Mountpoint-cache hash table entries: 2048 (order: 2, 16384 bytes)
    [    0.020647] ASID allocator initialised with 65536 entries
    [    0.021225] zynqmp_plat_init Power management API v0.3
    [    0.021750] Detected VIPT I-cache on CPU1
    [    0.021789] CPU1: Booted secondary processor [410fd034]
    [    0.022144] Detected VIPT I-cache on CPU2
    [    0.022172] CPU2: Booted secondary processor [410fd034]
    [    0.022512] Detected VIPT I-cache on CPU3
    [    0.022541] CPU3: Booted secondary processor [410fd034]
    [    0.022583] Brought up 4 CPUs
    [    0.022618] SMP: Total of 4 processors activated.
    [    0.022627] CPU features: detected feature: 32-bit EL0 Support
    [    0.022637] CPU: All CPU(s) started at EL2
    [    0.022661] alternatives: patching kernel code
    [    0.023209] devtmpfs: initialized
    [    0.027924] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
    [    0.030951] xor: measuring software checksum speed
    [    0.067974]    8regs     :  2110.000 MB/sec
    [    0.108030]    8regs_prefetch:  1881.000 MB/sec
    [    0.148093]    32regs    :  2594.000 MB/sec
    [    0.188145]    32regs_prefetch:  2180.000 MB/sec
    [    0.188158] xor: using function: 32regs (2594.000 MB/sec)
    [    0.188264] pinctrl core: initialized pinctrl subsystem
    [    0.188982] NET: Registered protocol family 16
    [    0.210459] cpuidle: using governor menu
    [    0.210678] Failed to initialise IOMMU /amba/smmu@fd800000
    [    0.210884] vdso: 2 pages (1 code @ ffffff80087b7000, 1 data @ ffffff8008a64000)
    [    0.210911] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
    [    0.211543] DMA: preallocated 256 KiB pool for atomic allocations
    [    0.223833] reset_zynqmp reset-controller: Xilinx zynqmp reset driver probed
    [    0.224273] ARM CCI_400_r1 PMU driver probed
    [    0.227697] zynqmp-pinctrl ff180000.pinctrl: zynqmp pinctrl initialized
    [    0.246790] HugeTLB registered 2 MB page size, pre-allocated 0 pages
    [    0.312472] raid6: int64x1  gen()   372 MB/s
    [    0.380518] raid6: int64x1  xor()   402 MB/s
    [    0.448625] raid6: int64x2  gen()   610 MB/s
    [    0.516672] raid6: int64x2  xor()   547 MB/s
    [    0.584787] raid6: int64x4  gen()   899 MB/s
    [    0.652852] raid6: int64x4  xor()   678 MB/s
    [    0.720946] raid6: int64x8  gen()  1051 MB/s
    [    0.789066] raid6: int64x8  xor()   684 MB/s
    [    0.857135] raid6: neonx1   gen()   662 MB/s
    [    0.925250] raid6: neonx1   xor()   670 MB/s
    [    0.993344] raid6: neonx2   gen()  1064 MB/s
    [    1.061428] raid6: neonx2   xor()   949 MB/s
    [    1.129528] raid6: neonx4   gen()  1380 MB/s
    [    1.197617] raid6: neonx4   xor()  1082 MB/s
    [    1.265705] raid6: neonx8   gen()  1456 MB/s
    [    1.333804] raid6: neonx8   xor()  1119 MB/s
    [    1.333817] raid6: using algorithm neonx8 gen() 1456 MB/s
    [    1.333830] raid6: .... xor() 1119 MB/s, rmw enabled
    [    1.333842] raid6: using intx1 recovery algorithm
    [    1.334676] usbcore: registered new interface driver usbfs
    [    1.334725] usbcore: registered new interface driver hub
    [    1.334783] usbcore: registered new device driver usb
    [    1.334886] pps_core: LinuxPPS API ver. 1 registered
    [    1.334900] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
    [    1.334932] PTP clock support registered
    [    1.334971] EDAC MC: Ver: 3.0.0
    [    1.335289] FPGA manager framework
    [    1.336001] clocksource: Switched to clocksource arch_sys_counter
    [    1.336121] VFS: Disk quotas dquot_6.6.0
    [    1.336178] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
    [    1.341358] NET: Registered protocol family 2
    [    1.341771] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
    [    1.341845] TCP bind hash table entries: 8192 (order: 5, 131072 bytes)
    [    1.341996] TCP: Hash tables configured (established 8192 bind 8192)
    [    1.342072] UDP hash table entries: 512 (order: 2, 16384 bytes)
    [    1.342106] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
    [    1.342255] NET: Registered protocol family 1
    [    1.342515] RPC: Registered named UNIX socket transport module.
    [    1.342531] RPC: Registered udp transport module.
    [    1.342543] RPC: Registered tcp transport module.
    [    1.342555] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [    1.342691] Trying to unpack rootfs image as initramfs...
    [    6.394241] Freeing initrd memory: 103780K (ffffffc001aa6000 - ffffffc007fff000)
    [    6.394638] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
    [    6.395580] futex hash table entries: 1024 (order: 5, 131072 bytes)
    [    6.395671] audit: initializing netlink subsys (disabled)
    [    6.395719] audit: type=2000 audit(6.380:1): initialized
    [    6.396385] workingset: timestamp_bits=62 max_order=18 bucket_order=0
    [    6.397241] NFS: Registering the id_resolver key type
    [    6.397269] Key type id_resolver registered
    [    6.397281] Key type id_legacy registered
    [    6.397298] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
    [    6.397328] jffs2: version 2.2. (NAND) (SUMMARY)  Copyright 2001-2006 Red Hat, Inc.
    [    6.398483] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 248)
    [    6.398507] io scheduler noop registered
    [    6.398519] io scheduler deadline registered
    [    6.398538] io scheduler cfq registered (default)
    [    6.399587] Write failed gate address:1000f02
    [    6.399733] xilinx-zynqmp-dma fd500000.dma: ZynqMP DMA driver Probe success
    [    6.399903] xilinx-zynqmp-dma fd510000.dma: ZynqMP DMA driver Probe success
    [    6.400091] xilinx-zynqmp-dma fd520000.dma: ZynqMP DMA driver Probe success
    [    6.400253] xilinx-zynqmp-dma fd530000.dma: ZynqMP DMA driver Probe success
    [    6.400411] xilinx-zynqmp-dma fd540000.dma: ZynqMP DMA driver Probe success
    [    6.400571] xilinx-zynqmp-dma fd550000.dma: ZynqMP DMA driver Probe success
    [    6.400733] xilinx-zynqmp-dma fd560000.dma: ZynqMP DMA driver Probe success
    [    6.400893] xilinx-zynqmp-dma fd570000.dma: ZynqMP DMA driver Probe success
    [    6.401138] xilinx-zynqmp-dma ffa80000.dma: ZynqMP DMA driver Probe success
    [    6.401301] xilinx-zynqmp-dma ffa90000.dma: ZynqMP DMA driver Probe success
    [    6.401456] xilinx-zynqmp-dma ffaa0000.dma: ZynqMP DMA driver Probe success
    [    6.401613] xilinx-zynqmp-dma ffab0000.dma: ZynqMP DMA driver Probe success
    [    6.401768] xilinx-zynqmp-dma ffac0000.dma: ZynqMP DMA driver Probe success
    [    6.401926] xilinx-zynqmp-dma ffad0000.dma: ZynqMP DMA driver Probe success
    [    6.402081] xilinx-zynqmp-dma ffae0000.dma: ZynqMP DMA driver Probe success
    [    6.402238] xilinx-zynqmp-dma ffaf0000.dma: ZynqMP DMA driver Probe success
    [    6.402356] zynqmp_pm firmware: Power management API v0.3
    [    6.402462] xenfs: not registering filesystem on non-xen platform
    [    6.434583] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled
    [    6.436051] ff000000.serial: ttyPS0 at MMIO 0xff000000 (irq = 39, base_baud = 6249999) is a xuartps
    [    7.365939] console [ttyPS0] enabled
    [    7.369775] [drm] Initialized
    [    7.372757] Unable to detect cache hierarchy from DT for CPU 0
    [    7.384110] brd: module loaded
    [    7.390411] loop: module loaded
    [    7.393983] mtdoops: mtd device (mtddev=name/number) must be supplied
    [    7.402137] libphy: Fixed MDIO Bus: probed
    [    7.407286] tun: Universal TUN/TAP device driver, 1.6
    [    7.412277] tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>
    [    7.419606] libphy: MACB_mii_bus: probed
    [    7.472571] usbcore: registered new interface driver asix
    [    7.477947] usbcore: registered new interface driver ax88179_178a
    [    7.484018] usbcore: registered new interface driver cdc_ether
    [    7.489822] usbcore: registered new interface driver net1080
    [    7.495463] usbcore: registered new interface driver cdc_subset
    [    7.501367] usbcore: registered new interface driver zaurus
    [    7.506934] usbcore: registered new interface driver cdc_ncm
    [    7.512932] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
    [    7.519388] ehci-pci: EHCI PCI platform driver
    [    7.524366] mousedev: PS/2 mouse device common for all mice
    [    7.530316] rtc_zynqmp ffa60000.rtc: rtc core: registered ffa60000.rtc as rtc0
    [    7.537510] i2c /dev entries driver
    [    7.541179] cdns-i2c ff030000.i2c: 400 kHz mmio ff030000 irq 32
    [    7.548041] EDAC MC: ECC not enabled
    [    7.551673] EDAC DEVICE0: Giving out device to module edac controller cache_err: DEV edac (POLLED)
    [    7.560730] EDAC DEVICE1: Giving out device to module zynqmp-ocm-edac controller zynqmp_ocm: DEV ff960000.memory-controller (INTERRUPT)
    [    7.573331] cpufreq: cpufreq_online: CPU0: Running at unlisted freq: 1099999 KHz
    [    7.580738] cpufreq: cpufreq_online: CPU0: Unlisted initial frequency changed to: 1199999 KHz
    [    7.589621] sdhci: Secure Digital Host Controller Interface driver
    [    7.595726] sdhci: Copyright(c) Pierre Ossman
    [    7.600066] sdhci-pltfm: SDHCI platform and OF driver helper
    [    7.652017] mmc0: SDHCI controller on ff160000.sdhci [ff160000.sdhci] using ADMA 64-bit
    [    7.708013] mmc1: SDHCI controller on ff170000.sdhci [ff170000.sdhci] using ADMA 64-bit
    [    7.716203] usbcore: registered new interface driver usbhid
    [    7.721712] usbhid: USB HID core driver
    [    7.728352] fpga_manager fpga0: Xilinx ZynqMP FPGA Manager registered
    [    7.734826] pktgen: Packet Generator for packet performance testing. Version: 2.75
    [    7.742589] Netfilter messages via NETLINK v0.30.
    [    7.747340] ip_tables: (C) 2000-2006 Netfilter Core Team
    [    7.752638] Initializing XFRM netlink socket
    [    7.756912] NET: Registered protocol family 10
    [    7.759612] mmc0: new HS200 MMC card at address 0001
    [    7.759900] mmcblk0: mmc0:0001 Q2J55L 7.09 GiB
    [    7.760049] mmcblk0boot0: mmc0:0001 Q2J55L partition 1 16.0 MiB
    [    7.760176] mmcblk0boot1: mmc0:0001 Q2J55L partition 2 16.0 MiB
    [    7.760300] mmcblk0rpmb: mmc0:0001 Q2J55L partition 3 4.00 MiB
    [    7.761176]  mmcblk0: p1
    [    7.791328] ip6_tables: (C) 2000-2006 Netfilter Core Team
    [    7.796704] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
    [    7.802947] NET: Registered protocol family 17
    [    7.807331] NET: Registered protocol family 15
    [    7.811758] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.
    [    7.824694] Ebtables v2.0 registered
    [    7.828466] 9pnet: Installing 9P2000 support
    [    7.832687] Key type dns_resolver registered
    [    7.837392] registered taskstats version 1
    [    7.841896] Btrfs loaded, crc32c=crc32c-generic
    [    7.857578] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
    [    7.863022] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
    [    7.870919] xhci-hcd xhci-hcd.0.auto: hcc params 0x0238f625 hci version 0x100 quirks 0x00010010
    [    7.879590] xhci-hcd xhci-hcd.0.auto: irq 217, io mem 0xfe200000
    [    7.885671] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
    [    7.892400] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    [    7.899609] usb usb1: Product: xHCI Host Controller
    [    7.904458] usb usb1: Manufacturer: Linux 4.9.0-xilinx-v2017.1 xhci-hcd
    [    7.911055] usb usb1: SerialNumber: xhci-hcd.0.auto
    [    7.916293] hub 1-0:1.0: USB hub found
    [    7.919979] hub 1-0:1.0: 1 port detected
    [    7.924064] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
    [    7.929487] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
    [    7.937173] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
    [    7.945281] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003
    [    7.952002] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    [    7.959216] usb usb2: Product: xHCI Host Controller
    [    7.964066] usb usb2: Manufacturer: Linux 4.9.0-xilinx-v2017.1 xhci-hcd
    [    7.970661] usb usb2: SerialNumber: xhci-hcd.0.auto
    [    7.975810] hub 2-0:1.0: USB hub found
    [    7.979506] hub 2-0:1.0: 1 port detected
    [    7.983812] rtc_zynqmp ffa60000.rtc: setting system clock to 1970-01-01 00:03:14 UTC (194)
    [    7.992015] of_cfs_init
    [    7.994445] of_cfs_init: OK
    [   20.296008] clk: Not disabling unused clocks
    [   20.300780] Freeing unused kernel memory: 448K (ffffffc0009f0000 - ffffffc000a60000)
    INIT: version 2.88 booting
    Starting udev
    [   20.424584] udevd[1402]: starting version 3.2
    [   20.429317] random: udevd: uninitialized urandom read (16 bytes read)
    [   20.435789] random: udevd: uninitialized urandom read (16 bytes read)
    [   20.442251] random: udevd: uninitialized urandom read (16 bytes read)
    [   20.448657] random: udevd: uninitialized urandom read (16 bytes read)
    [   20.459131] udevd[1403]: starting eudev-3.2
    [   20.502110] random: udevd: uninitialized urandom read (16 bytes read)
    [   20.510525] random: udevd: uninitialized urandom read (16 bytes read)
    [   20.526965] zynqmp_r5_remoteproc ff9a0100.zynqmp_r5_rproc: RPU core_conf: split0
    [   20.535014] remoteproc remoteproc0: ff9a0100.zynqmp_r5_rproc is available
    [   20.541791] remoteproc remoteproc0: Note: remoteproc is still under development and considered experimental.
    [   20.551573] remoteproc remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
    [   20.562924] remoteproc remoteproc0: Direct firmware load for rproc-ff9a0100.zynqmp_r5_rproc-fw failed with error -2
    [   20.573408] zynqmp_r5_remoteproc ff9a0200.zynqmp_r5_rproc: RPU core_conf: split1
    [   20.582412] remoteproc remoteproc1: ff9a0200.zynqmp_r5_rproc is available
    [   20.589163] remoteproc remoteproc1: Note: remoteproc is still under development and considered experimental.
    [   20.598972] remoteproc remoteproc1: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
    [   20.610467] remoteproc remoteproc1: Direct firmware load for rproc-ff9a0200.zynqmp_r5_rproc-fw failed with error -2
    [   20.705443] random: fast init done
    Populating dev cache
    Tue Jul 25 03:32:10 UTC 2017
    Starting internet superserver: inetd.
    Starting tcf32-agent: OK
    INIT: Entering runlevel: 5
    Configuring network interfaces... ifconfig: SIOCGIFFLAGS: No such device
    Starting system message bus: dbus.
    Starting Dropbear SSH server: Generating key, this may take a while...
    Public key portion is:
    ssh-rsa AAAAB3NzaC1yc2EAAAADAQABAAABAQDJ5jjvLGzIAafu0jw9QbxSfTP2ATJOoaSa3LlS/0Hp6oGQtpZtTdh4L63vayAtJ4RvTCmicHiVO+WHQr6Ap1jMO4Qn9zZEJqpPw8Mz8j5OzSt33fxdcrdhwQuwErV82H7ObWZ1PkSTLq9XvPK9tWmPgQn/sD1IPd3UC8UGpuP299QhabYDwpMWDKAAT2tIgp8L5HoGdH3w173IS4PmS+sk3mLAJtYuKU05zTvYS9OPqBuWu2+rkG9S38C1oAkpyVOG5TtaA3GyF5K3NmTCA73/POlv/lmhSXov0Aovoi1PnDIQbOHQgpgatbTNqAxLZvFEswWErvuvlRumGb/2DmEd root@plnx_aarch64
    Fingerprint: md5 e0:95:3b:19:55:6b:81:e6:0f:23:7a:eb:49:00:29:70
    dropbear.
    Starting watchdog:
     
    Starting watchdog keepalive daemon: wd_keepalive.
    Starting syslogd/klogd: done
    Starting tcf-agent: OK
    INIT: Id "hvc0" respawning too fast: disabled for 5 minutes
     
    PetaLinux 2017.1 plnx_aarch64 /dev/ttyPS0
     
    plnx_aarch64 login: root
    Password:
    root@plnx_aarch64:~# ifconfig
    lo        Link encap:Local Loopback
              inet addr:127.0.0.1  Mask:255.0.0.0
              inet6 addr: ::1%4879704/128 Scope:Host
              UP LOOPBACK RUNNING  MTU:65536  Metric:1
              RX packets:11 errors:0 dropped:0 overruns:0 frame:0
              TX packets:11 errors:0 dropped:0 overruns:0 carrier:0
              collisions:0 txqueuelen:1
              RX bytes:2228 (2.1 KiB)  TX bytes:2228 (2.1 KiB)
     
    root@plnx_aarch64:~#
    _______________________________________
    Engineering silicon
     
    _________________________________________
     
      Starting kernel ...
       
      [    0.000000] Booting Linux on physical CPU 0x0
      [    0.000000] Linux version 4.9.0-xilinx-v2017.1 (hallt@petalinuxHost) (gcc version 6.2.1 20161016 (Linaro GCC 6.2-2016.11) ) #1 SMP Fri Jul 21 11:41:49 PDT 2017
      [    0.000000] Boot CPU: AArch64 Processor [410fd034]
      [    0.000000] earlycon: cdns0 at MMIO 0x00000000ff000000 (options '115200n8')
      [    0.000000] bootconsole [cdns0] enabled
      [    0.000000] cma: Reserved 128 MiB at 0x0000000036000000
      [    0.000000] psci: probing for conduit method from DT.
      [    0.000000] psci: PSCIv1.0 detected in firmware.
      [    0.000000] psci: Using standard PSCI v0.2 function IDs
      [    0.000000] psci: MIGRATE_INFO_TYPE not supported.
      [    0.000000] percpu: Embedded 20 pages/cpu @ffffffc035f7b000 s44056 r8192 d29672 u81920
      [    0.000000] Detected VIPT I-cache on CPU0
      [    0.000000] CPU features: enabling workaround for ARM erratum 845719
      [    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 250480
      [    0.000000] Kernel command line: earlycon clk_ignore_unused root=/dev/nfs nfsroot=172.16.40.137:/tftpboot/nfsroot,tcp ip=dhcp rw uio_pdrv_genirq.of_id=generic-uio
      [    0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)
      [    0.000000] Dentry cache hash table entries: 131072 (order: 8, 1048576 bytes)
      [    0.000000] Inode-cache hash table entries: 65536 (order: 7, 524288 bytes)
      [    0.000000] Memory: 753508K/1015808K available (7358K kernel code, 500K rwdata, 2284K rodata, 448K init, 346K bss, 131228K reserved, 131072K cma-reserved)
      [    0.000000] Virtual kernel memory layout:
      [    0.000000]     modules : 0xffffff8000000000 - 0xffffff8008000000   (   128 MB)
      [    0.000000]     vmalloc : 0xffffff8008000000 - 0xffffffbebfff0000   (   250 GB)
      [    0.000000]       .text : 0xffffff8008080000 - 0xffffff80087b0000   (  7360 KB)
      [    0.000000]     .rodata : 0xffffff80087b0000 - 0xffffff80089f0000   (  2304 KB)
      [    0.000000]       .init : 0xffffff80089f0000 - 0xffffff8008a60000   (   448 KB)
      [    0.000000]       .data : 0xffffff8008a60000 - 0xffffff8008add008   (   501 KB)
      [    0.000000]        .bss : 0xffffff8008add008 - 0xffffff8008b33924   (   347 KB)
      [    0.000000]     fixed   : 0xffffffbefe7fd000 - 0xffffffbefec00000   (  4108 KB)
      [    0.000000]     PCI I/O : 0xffffffbefee00000 - 0xffffffbeffe00000   (    16 MB)
      [    0.000000]     vmemmap : 0xffffffbf00000000 - 0xffffffc000000000   (     4 GB maximum)
      [    0.000000]               0xffffffbf00000000 - 0xffffffbf00d90000   (    13 MB actual)
      [    0.000000]     memory  : 0xffffffc000000000 - 0xffffffc03e000000   (   992 MB)
      [    0.000000] Hierarchical RCU implementation.
      [    0.000000]  Build-time adjustment of leaf fanout to 64.
      [    0.000000]  RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.
      [    0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=64, nr_cpu_ids=4
      [    0.000000] NR_IRQS:64 nr_irqs:64 0
      [    0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000
      [    0.000000] GIC: Using split EOI/Deactivate mode
      [    0.000000] arm_arch_timer: Architected cp15 timer(s) running at 100.00MHz (phys).
      [    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x171024e7e0, max_idle_ns: 440795205315 ns
      [    0.000003] sched_clock: 56 bits at 100MHz, resolution 10ns, wraps every 4398046511100ns
      [    0.008347] Console: colour dummy device 80x25
      [    0.012605] console [tty0] enabled
      [    0.015967] bootconsole [cdns0] disabled
      [    0.000000] Booting Linux on physical CPU 0x0
      [    0.000000] Linux version 4.9.0-xilinx-v2017.1 (hallt@petalinuxHost) (gcc version 6.2.1 20161016 (Linaro GCC 6.2-2016.11) ) #1 SMP Fri Jul 21 11:41:49 PDT 2017
      [    0.000000] Boot CPU: AArch64 Processor [410fd034]
      [    0.000000] earlycon: cdns0 at MMIO 0x00000000ff000000 (options '115200n8')
      [    0.000000] bootconsole [cdns0] enabled
      [    0.000000] cma: Reserved 128 MiB at 0x0000000036000000
      [    0.000000] psci: probing for conduit method from DT.
      [    0.000000] psci: PSCIv1.0 detected in firmware.
      [    0.000000] psci: Using standard PSCI v0.2 function IDs
      [    0.000000] psci: MIGRATE_INFO_TYPE not supported.
      [    0.000000] percpu: Embedded 20 pages/cpu @ffffffc035f7b000 s44056 r8192 d29672 u81920
      [    0.000000] Detected VIPT I-cache on CPU0
      [    0.000000] CPU features: enabling workaround for ARM erratum 845719
      [    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 250480
      [    0.000000] Kernel command line: earlycon clk_ignore_unused root=/dev/nfs nfsroot=172.16.40.137:/tftpboot/nfsroot,tcp ip=dhcp rw uio_pdrv_genirq.of_id=generic-uio
      [    0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)
      [    0.000000] Dentry cache hash table entries: 131072 (order: 8, 1048576 bytes)
      [    0.000000] Inode-cache hash table entries: 65536 (order: 7, 524288 bytes)
      [    0.000000] Memory: 753508K/1015808K available (7358K kernel code, 500K rwdata, 2284K rodata, 448K init, 346K bss, 131228K reserved, 131072K cma-reserved)
      [    0.000000] Virtual kernel memory layout:
      [    0.000000]     modules : 0xffffff8000000000 - 0xffffff8008000000   (   128 MB)
      [    0.000000]     vmalloc : 0xffffff8008000000 - 0xffffffbebfff0000   (   250 GB)
      [    0.000000]       .text : 0xffffff8008080000 - 0xffffff80087b0000   (  7360 KB)
      [    0.000000]     .rodata : 0xffffff80087b0000 - 0xffffff80089f0000   (  2304 KB)
      [    0.000000]       .init : 0xffffff80089f0000 - 0xffffff8008a60000   (   448 KB)
      [    0.000000]       .data : 0xffffff8008a60000 - 0xffffff8008add008   (   501 KB)
      [    0.000000]        .bss : 0xffffff8008add008 - 0xffffff8008b33924   (   347 KB)
      [    0.000000]     fixed   : 0xffffffbefe7fd000 - 0xffffffbefec00000   (  4108 KB)
      [    0.000000]     PCI I/O : 0xffffffbefee00000 - 0xffffffbeffe00000   (    16 MB)
      [    0.000000]     vmemmap : 0xffffffbf00000000 - 0xffffffc000000000   (     4 GB maximum)
      [    0.000000]               0xffffffbf00000000 - 0xffffffbf00d90000   (    13 MB actual)
      [    0.000000]     memory  : 0xffffffc000000000 - 0xffffffc03e000000   (   992 MB)
      [    0.000000] Hierarchical RCU implementation.
      [    0.000000]  Build-time adjustment of leaf fanout to 64.
      [    0.000000]  RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.
      [    0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=64, nr_cpu_ids=4
      [    0.000000] NR_IRQS:64 nr_irqs:64 0
      [    0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000
      [    0.000000] GIC: Using split EOI/Deactivate mode
      [    0.000000] arm_arch_timer: Architected cp15 timer(s) running at 100.00MHz (phys).
      [    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x171024e7e0, max_idle_ns: 440795205315 ns
      [    0.000003] sched_clock: 56 bits at 100MHz, resolution 10ns, wraps every 4398046511100ns
      [    0.008347] Console: colour dummy device 80x25
      [    0.012605] console [tty0] enabled
      [    0.015967] bootconsole [cdns0] disabled
      [    0.019881] Calibrating delay loop (skipped), value calculated using timer frequency.. 200.00 BogoMIPS (lpj=400000)
      [    0.019896] pid_max: default: 32768 minimum: 301
      [    0.020014] Mount-cache hash table entries: 2048 (order: 2, 16384 bytes)
      [    0.020024] Mountpoint-cache hash table entries: 2048 (order: 2, 16384 bytes)
      [    0.020653] ASID allocator initialised with 65536 entries
      [    0.021265] zynqmp_plat_init Power management API v0.3
      [    0.021861] Detected VIPT I-cache on CPU1
      [    0.021901] CPU1: Booted secondary processor [410fd034]
      [    0.022327] Detected VIPT I-cache on CPU2
      [    0.022356] CPU2: Booted secondary processor [410fd034]
      [    0.022767] Detected VIPT I-cache on CPU3
      [    0.022796] CPU3: Booted secondary processor [410fd034]
      [    0.022838] Brought up 4 CPUs
      [    0.022873] SMP: Total of 4 processors activated.
      [    0.022882] CPU features: detected feature: 32-bit EL0 Support
      [    0.022892] CPU: All CPU(s) started at EL2
      [    0.022914] alternatives: patching kernel code
      [    0.023459] devtmpfs: initialized
      [    0.028187] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
      [    0.031207] xor: measuring software checksum speed
      [    0.067982]    8regs     :  2110.000 MB/sec
      [    0.108037]    8regs_prefetch:  1881.000 MB/sec
      [    0.148100]    32regs    :  2594.000 MB/sec
      [    0.188152]    32regs_prefetch:  2180.000 MB/sec
      [    0.188165] xor: using function: 32regs (2594.000 MB/sec)
      [    0.188271] pinctrl core: initialized pinctrl subsystem
      [    0.188988] NET: Registered protocol family 16
      [    0.210634] cpuidle: using governor menu
      [    0.210862] Failed to initialise IOMMU /amba/smmu@fd800000
      [    0.211063] vdso: 2 pages (1 code @ ffffff80087b7000, 1 data @ ffffff8008a64000)
      [    0.211090] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
      [    0.211729] DMA: preallocated 256 KiB pool for atomic allocations
      [    0.238531] reset_zynqmp reset-controller: Xilinx zynqmp reset driver probed
      [    0.238982] ARM CCI_400_r1 PMU driver probed
      [    0.242382] zynqmp-pinctrl ff180000.pinctrl: zynqmp pinctrl initialized
      [    0.267124] HugeTLB registered 2 MB page size, pre-allocated 0 pages
      [    0.332516] raid6: int64x1  gen()   372 MB/s
      [    0.400549] raid6: int64x1  xor()   402 MB/s
      [    0.468617] raid6: int64x2  gen()   609 MB/s
      [    0.536690] raid6: int64x2  xor()   547 MB/s
      [    0.604801] raid6: int64x4  gen()   899 MB/s
      [    0.672889] raid6: int64x4  xor()   678 MB/s
      [    0.740979] raid6: int64x8  gen()  1051 MB/s
      [    0.809066] raid6: int64x8  xor()   684 MB/s
      [    0.877252] raid6: neonx1   gen()   663 MB/s
      [    0.945280] raid6: neonx1   xor()   670 MB/s
      [    1.013370] raid6: neonx2   gen()  1064 MB/s
      [    1.081450] raid6: neonx2   xor()   948 MB/s
      [    1.149553] raid6: neonx4   gen()  1381 MB/s
      [    1.217646] raid6: neonx4   xor()  1084 MB/s
      [    1.285753] raid6: neonx8   gen()  1456 MB/s
      [    1.353847] raid6: neonx8   xor()  1119 MB/s
      [    1.353860] raid6: using algorithm neonx8 gen() 1456 MB/s
      [    1.353873] raid6: .... xor() 1119 MB/s, rmw enabled
      [    1.353885] raid6: using intx1 recovery algorithm
      [    1.354719] usbcore: registered new interface driver usbfs
      [    1.354766] usbcore: registered new interface driver hub
      [    1.354820] usbcore: registered new device driver usb
      [    1.354916] pps_core: LinuxPPS API ver. 1 registered
      [    1.354931] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
      [    1.354963] PTP clock support registered
      [    1.355000] EDAC MC: Ver: 3.0.0
      [    1.355328] FPGA manager framework
      [    1.356045] clocksource: Switched to clocksource arch_sys_counter
      [    1.356145] VFS: Disk quotas dquot_6.6.0
      [    1.356202] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
      [    1.363078] NET: Registered protocol family 2
      [    1.363493] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
      [    1.363567] TCP bind hash table entries: 8192 (order: 5, 131072 bytes)
      [    1.363714] TCP: Hash tables configured (established 8192 bind 8192)
      [    1.363791] UDP hash table entries: 512 (order: 2, 16384 bytes)
      [    1.363825] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
      [    1.363972] NET: Registered protocol family 1
      [    1.364323] RPC: Registered named UNIX socket transport module.
      [    1.364338] RPC: Registered udp transport module.
      [    1.364350] RPC: Registered tcp transport module.
      [    1.364362] RPC: Registered tcp NFSv4.1 backchannel transport module.
      [    1.364504] Trying to unpack rootfs image as initramfs...
      [    6.417071] Freeing initrd memory: 103780K (ffffffc001aa6000 - ffffffc007fff000)
      [    6.417482] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
      [    6.418402] futex hash table entries: 1024 (order: 5, 131072 bytes)
      [    6.418496] audit: initializing netlink subsys (disabled)
      [    6.418552] audit: type=2000 audit(6.404:1): initialized
      [    6.419155] workingset: timestamp_bits=62 max_order=18 bucket_order=0
      [    6.420031] NFS: Registering the id_resolver key type
      [    6.420084] Key type id_resolver registered
      [    6.420097] Key type id_legacy registered
      [    6.420114] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
      [    6.420143] jffs2: version 2.2. (NAND) (SUMMARY)  Copyright 2001-2006 Red Hat, Inc.
      [    6.421318] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 248)
      [    6.421342] io scheduler noop registered
      [    6.421354] io scheduler deadline registered
      [    6.421372] io scheduler cfq registered (default)
      [    6.422721] Write failed gate address:1000f02
      [    6.422864] xilinx-zynqmp-dma fd500000.dma: ZynqMP DMA driver Probe success
      [    6.423033] xilinx-zynqmp-dma fd510000.dma: ZynqMP DMA driver Probe success
      [    6.423194] xilinx-zynqmp-dma fd520000.dma: ZynqMP DMA driver Probe success
      [    6.423352] xilinx-zynqmp-dma fd530000.dma: ZynqMP DMA driver Probe success
      [    6.423510] xilinx-zynqmp-dma fd540000.dma: ZynqMP DMA driver Probe success
      [    6.423665] xilinx-zynqmp-dma fd550000.dma: ZynqMP DMA driver Probe success
      [    6.423823] xilinx-zynqmp-dma fd560000.dma: ZynqMP DMA driver Probe success
      [    6.423980] xilinx-zynqmp-dma fd570000.dma: ZynqMP DMA driver Probe success
      [    6.424466] xilinx-zynqmp-dma ffa80000.dma: ZynqMP DMA driver Probe success
      [    6.424619] xilinx-zynqmp-dma ffa90000.dma: ZynqMP DMA driver Probe success
      [    6.424773] xilinx-zynqmp-dma ffaa0000.dma: ZynqMP DMA driver Probe success
      [    6.424927] xilinx-zynqmp-dma ffab0000.dma: ZynqMP DMA driver Probe success
      [    6.425081] xilinx-zynqmp-dma ffac0000.dma: ZynqMP DMA driver Probe success
      [    6.425235] xilinx-zynqmp-dma ffad0000.dma: ZynqMP DMA driver Probe success
      [    6.425390] xilinx-zynqmp-dma ffae0000.dma: ZynqMP DMA driver Probe success
      [    6.425545] xilinx-zynqmp-dma ffaf0000.dma: ZynqMP DMA driver Probe success
      [    6.425657] zynqmp_pm firmware: Power management API v0.3
      [    6.425768] xenfs: not registering filesystem on non-xen platform
      [    6.458004] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled
      [    6.459653] ff000000.serial: ttyPS0 at MMIO 0xff000000 (irq = 39, base_baud = 6249999) is a xuartps
      [    7.389536] console [ttyPS0] enabled
      [    7.393346] [drm] Initialized
      [    7.396331] Unable to detect cache hierarchy from DT for CPU 0
      [    7.407552] brd: module loaded
      [    7.413934] loop: module loaded
      [    7.417503] mtdoops: mtd device (mtddev=name/number) must be supplied
      [    7.425895] libphy: Fixed MDIO Bus: probed
      [    7.431047] tun: Universal TUN/TAP device driver, 1.6
      [    7.436051] tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>
      [    7.443681] libphy: MACB_mii_bus: probed
      [    7.451153] macb ff0e0000.ethernet eth0: Cadence GEM rev 0x50070106 at 0xff0e0000 irq 30 (00:0a:35:00:22:02)
      [    7.460923] TI DP83867 ff0e0000.etherne:05: attached PHY driver [TI DP83867] (mii_bus:phy_addr=ff0e0000.etherne:05, irq=-1)
      [    7.472509] usbcore: registered new interface driver asix
      [    7.477880] usbcore: registered new interface driver ax88179_178a
      [    7.483944] usbcore: registered new interface driver cdc_ether
      [    7.489761] usbcore: registered new interface driver net1080
      [    7.495401] usbcore: registered new interface driver cdc_subset
      [    7.501303] usbcore: registered new interface driver zaurus
      [    7.506870] usbcore: registered new interface driver cdc_ncm
      [    7.513013] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
      [    7.519472] ehci-pci: EHCI PCI platform driver
      [    7.524446] mousedev: PS/2 mouse device common for all mice
      [    7.530394] rtc_zynqmp ffa60000.rtc: rtc core: registered ffa60000.rtc as rtc0
      [    7.537588] i2c /dev entries driver
      [    7.541480] cdns-i2c ff030000.i2c: 400 kHz mmio ff030000 irq 32
      [    7.548554] EDAC MC: ECC not enabled
      [    7.552207] EDAC DEVICE0: Giving out device to module edac controller cache_err: DEV edac (POLLED)
      [    7.561256] EDAC DEVICE1: Giving out device to module zynqmp-ocm-edac controller zynqmp_ocm: DEV ff960000.memory-controller (INTERRUPT)
      [    7.573863] cpufreq: cpufreq_online: CPU0: Running at unlisted freq: 1099999 KHz
      [    7.581390] cpufreq: cpufreq_online: CPU0: Unlisted initial frequency changed to: 1199999 KHz
      [    7.590272] sdhci: Secure Digital Host Controller Interface driver
      [    7.596384] sdhci: Copyright(c) Pierre Ossman
      [    7.600722] sdhci-pltfm: SDHCI platform and OF driver helper
      [    7.652058] mmc0: SDHCI controller on ff160000.sdhci [ff160000.sdhci] using ADMA 64-bit
      [    7.708053] mmc1: SDHCI controller on ff170000.sdhci [ff170000.sdhci] using ADMA 64-bit
      [    7.716232] usbcore: registered new interface driver usbhid
      [    7.721736] usbhid: USB HID core driver
      [    7.727422] fpga_manager fpga0: Xilinx ZynqMP FPGA Manager registered
      [    7.733895] pktgen: Packet Generator for packet performance testing. Version: 2.75
      [    7.741663] Netfilter messages via NETLINK v0.30.
      [    7.746416] ip_tables: (C) 2000-2006 Netfilter Core Team
      [    7.751707] Initializing XFRM netlink socket
      [    7.755987] NET: Registered protocol family 10
      [    7.760483] mmc0: new HS200 MMC card at address 0001
      [    7.765423] ip6_tables: (C) 2000-2006 Netfilter Core Team
      [    7.765671] mmcblk0: mmc0:0001 Q2J55L 7.09 GiB
      [    7.765806] mmcblk0boot0: mmc0:0001 Q2J55L partition 1 16.0 MiB
      [    7.765938] mmcblk0boot1: mmc0:0001 Q2J55L partition 2 16.0 MiB
      [    7.766070] mmcblk0rpmb: mmc0:0001 Q2J55L partition 3 4.00 MiB
      [    7.766936]  mmcblk0: p1
      [    7.795439] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
      [    7.801712] NET: Registered protocol family 17
      [    7.806095] NET: Registered protocol family 15
      [    7.810528] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.
      [    7.823455] Ebtables v2.0 registered
      [    7.827235] 9pnet: Installing 9P2000 support
      [    7.831459] Key type dns_resolver registered
      [    7.836174] registered taskstats version 1
      [    7.840690] Btrfs loaded, crc32c=crc32c-generic
      [    7.856772] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
      [    7.862213] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
      [    7.870092] xhci-hcd xhci-hcd.0.auto: hcc params 0x0238f625 hci version 0x100 quirks 0x00010010
      [    7.878766] xhci-hcd xhci-hcd.0.auto: irq 217, io mem 0xfe200000
      [    7.884839] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
      [    7.891563] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
      [    7.898771] usb usb1: Product: xHCI Host Controller
      [    7.903622] usb usb1: Manufacturer: Linux 4.9.0-xilinx-v2017.1 xhci-hcd
      [    7.910219] usb usb1: SerialNumber: xhci-hcd.0.auto
      [    7.915448] hub 1-0:1.0: USB hub found
      [    7.919148] hub 1-0:1.0: 1 port detected
      [    7.923210] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
      [    7.928638] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
      [    7.936323] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
      [    7.944428] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003
      [    7.951148] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
      [    7.958359] usb usb2: Product: xHCI Host Controller
      [    7.963211] usb usb2: Manufacturer: Linux 4.9.0-xilinx-v2017.1 xhci-hcd
      [    7.969807] usb usb2: SerialNumber: xhci-hcd.0.auto
      [    7.975009] hub 2-0:1.0: USB hub found
      [    7.978707] hub 2-0:1.0: 1 port detected
      [    7.983017] rtc_zynqmp ffa60000.rtc: setting system clock to 2017-08-07 00:36:35 UTC (1502066195)
      [    7.991833] of_cfs_init
      [    7.994266] of_cfs_init: OK
      [    7.998499] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
      [   11.080739] macb ff0e0000.ethernet eth0: link up (1000/Full)
      [   11.088059] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
      [   11.108048] Sending DHCP requests ., OK
      [   11.144046] IP-Config: Got DHCP answer from 172.16.47.254, my address is 172.16.42.2
      [   11.151732] IP-Config: Complete:
      [   11.154933]      device=eth0, hwaddr=00:0a:35:00:22:02, ipaddr=172.16.42.2, mask=255.255.248.0, gw=172.16.47.254
      [   11.165095]      host=172.16.42.2, domain=esi.com, nis-domain=(none)
      [   11.171423]      bootserver=0.0.0.0, rootserver=172.16.40.137, rootpath=     nameserver0=172.17.5.4, nameserver1=172.17.5.120
      [   11.182810] clk: Not disabling unused clocks
      [   11.187729] Freeing unused kernel memory: 448K (ffffffc0009f0000 - ffffffc000a60000)
      INIT: version 2.88 booting
      Starting udev
      [   11.312499] udevd[1394]: starting version 3.2
      [   11.317132] random: udevd: uninitialized urandom read (16 bytes read)
      [   11.323595] random: udevd: uninitialized urandom read (16 bytes read)
      [   11.330055] random: udevd: uninitialized urandom read (16 bytes read)
      [   11.336463] random: udevd: uninitialized urandom read (16 bytes read)
      [   11.346931] udevd[1395]: starting eudev-3.2
      [   11.385281] random: udevd: uninitialized urandom read (16 bytes read)
      [   11.391748] random: udevd: uninitialized urandom read (16 bytes read)
      [   11.406723] random: udevd: uninitialized urandom read (16 bytes read)
      [   11.415258] random: udevd: uninitialized urandom read (16 bytes read)
      [   11.431229] zynqmp_r5_remoteproc ff9a0100.zynqmp_r5_rproc: RPU core_conf: split0
      [   11.440283] remoteproc remoteproc0: ff9a0100.zynqmp_r5_rproc is available
      [   11.447059] remoteproc remoteproc0: Note: remoteproc is still under development and considered experimental.
      [   11.456837] remoteproc remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
      [   11.468201] remoteproc remoteproc0: Direct firmware load for rproc-ff9a0100.zynqmp_r5_rproc-fw failed with error -2
      [   11.478697] zynqmp_r5_remoteproc ff9a0200.zynqmp_r5_rproc: RPU core_conf: split1
      [   11.486789] remoteproc remoteproc1: ff9a0200.zynqmp_r5_rproc is available
      [   11.493563] remoteproc remoteproc1: Note: remoteproc is still under development and considered experimental.
      [   11.503346] remoteproc remoteproc1: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
      [   11.514699] remoteproc remoteproc1: Direct firmware load for rproc-ff9a0200.zynqmp_r5_rproc-fw failed with error -2
      [   11.574043] random: fast init done
      Populating dev cache
      Starting internet superserver: inetd.
      Starting tcf32-agent: OK
      INIT: Entering runlevel: 5
      Configuring network interfaces... udhcpc (v1.24.1) started
      Sending discover...
      Sending select for 172.16.42.2...
      Lease of 172.16.42.2 obtained, lease time 86400
      /etc/udhcpc.d/50default: Adding DNS 172.17.5.4
      /etc/udhcpc.d/50default: Adding DNS 172.17.5.120
      done.
      Starting system message bus: dbus.
      Starting Dropbear SSH server: Generating key, this may take a while...
      Public key portion is:
      ssh-rsa AAAAB3NzaC1yc2EAAAADAQABAAABAQC3Xzxt21pqORs2Inmx4EnLWFGLkORmR8AsO1osixurBehw1amQwWmHF2A6shN49hW9ky49mAw4EJR+dm5FFlxlxWZyUBnbwRRlFAvbnEq8muOjsg9qlDvf4wvBvX9EhSNddbdvGWb7TJ8q++s/FVOPDWFgoeedTr3Fc7YgxtT6F4U+ev/HgJfuzQzvajltIQXCnOlI+vJA2P4i8asRV6izoRd37Tq0d5Vi8uUTYvjUTCCXKLpSb6jGV+1vF2lzIdWlZw3VwMPFPdWcoIoGMI0IsgXuh2/VAnOFuP3JKas9PZB7NDbiE7nFIkhr0IczsAasePPWv5uoXirgvQc0xBcj root@plnx_aarch64
      Fingerprint: md5 2a:d1:e8:50:57:5f:0a:ab:39:40:f8:b4:4d:ab:17:58
      dropbear.
      Starting watchdog:
       
      Starting watchdog keepalive daemon: wd_keepalive.
      Starting syslogd/klogd: done
      Starting tcf-agent: OK
      INIT: Id "hvc0" respawning too fast: disabled for 5 minutes
       
      PetaLinux 2017.1 plnx_aarch64 /dev/ttyPS0
       
      plnx_aarch64 login: root
      Password:
      root@plnx_aarch64:~# ifconfig
      eth0      Link encap:Ethernet  HWaddr 00:0A:35:00:22:02
                inet addr:172.16.42.2  Bcast:172.16.47.255  Mask:255.255.248.0
                UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1
                RX packets:1025 errors:0 dropped:6 overruns:0 frame:0
                TX packets:270 errors:0 dropped:0 overruns:0 carrier:0
                collisions:0 txqueuelen:1000
                RX bytes:79542 (77.6 KiB)  TX bytes:76172 (74.3 KiB)
                Interrupt:30
       
      lo        Link encap:Local Loopback
                inet addr:127.0.0.1  Mask:255.0.0.0
                inet6 addr: ::1%4879704/128 Scope:Host
                UP LOOPBACK RUNNING  MTU:65536  Metric:1
                RX packets:86 errors:0 dropped:0 overruns:0 frame:0
                TX packets:86 errors:0 dropped:0 overruns:0 carrier:0
                collisions:0 txqueuelen:1
                RX bytes:22461 (21.9 KiB)  TX bytes:22461 (21.9 KiB)
       
      root@plnx_aarch64:~# [  231.232677] random: crng init done
       
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi Tobinhall,

    In your Hardware Project are you targeting the ES1 EG device or the production silicon EG device? It would cause an issue that you are describing where the ES1 SOM functions and then you swap to the Production SOM caused by the Hardware project not being defined correctly. (its looking for the ES1 device when you boot and you are using the production device)

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tobinhall
    0 tobinhall over 9 years ago

    Initially I thought that was the problem that doesn't explain why u-boot worked, but after checking with tech support it appears that the phy address was changed from 5 to 9 in the production board.  I was able to confirm this with a "mii info" command in u-boot.  I changed the device tree and now I am fine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Tobin,

    Thanks for sharing your solution!

    I have made a  post here in hope of helping others that highlights your solution.

    http://zedboard.org/content/production-ultrazed-eg-som-eth-phy-address-change

    --Josh