Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design Engineering Silicon / Produciton Silicon diff
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 360 subscribers
  • Views 660 views
  • Users 0 members are here
Related

Engineering Silicon / Produciton Silicon diff

tobinhall
tobinhall over 9 years ago

We have a petalinux image which ethernet works fine on the Engineering silicon / board, but does not work on the Production version.  

Petalinux was generated from hdf export from a vivado project with an empty (other than the ZYNQ block) PL system.  PS was configured for ethernet and such, similar if not identical to the default done by the configuration wizzard.  (this is to support reprogramming the PL system.  Not sure why I need this but but that's another issue for another day.)

Ethernet through u-boot seems to work fine in both cases.

I also noticed that there are different schematics for the Engineering and Production boards.  Both of our setups are the starter kits meaning that each SOM has the carrier designed for it.

1. are there any significant hardware changes in the schematics (besides the ZYNQ) requiring newer versions of software or a different configuration?

2. does the zynq itself require newer versions of software? (petalinux or vivado)

All our tools are 2017.1

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi Tobinhall,

    In your Hardware Project are you targeting the ES1 EG device or the production silicon EG device? It would cause an issue that you are describing where the ES1 SOM functions and then you swap to the Production SOM caused by the Hardware project not being defined correctly. (its looking for the ES1 device when you boot and you are using the production device)

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi Tobinhall,

    In your Hardware Project are you targeting the ES1 EG device or the production silicon EG device? It would cause an issue that you are describing where the ES1 SOM functions and then you swap to the Production SOM caused by the Hardware project not being defined correctly. (its looking for the ES1 device when you boot and you are using the production device)

    --Josh