Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design SPI0 example with I/O carrier board
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 359 subscribers
  • Views 537 views
  • Users 0 members are here
Related

SPI0 example with I/O carrier board

jarvisroach
jarvisroach over 8 years ago

I'm looking for a reference example of using SPI0 via the PS PMOD connector. For example, one thing that I'm wondering about is if anything needs to be done to enable the signals (SCLK, MISO,MOSI, SS). They seem to either be tri-stated or simply driven high to 3.3V, no change in state even though the driver seems to be working correctly (and SPI module control registers responding correctly). Another thought is that I'll need a slightly different bitstream or HDF to enable this.

The UZ I/O Carrier Card doc seems to indicate that SPI0 should be available as default (as opposed to I2C or UART) on pg 18.

  • Sign in to reply
  • Cancel
Parents
  • jarvisroach
    0 jarvisroach over 8 years ago

    However, this should probably be updated in the Vivado design to get the FSBL tto set those registers correctly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jarvisroach
    0 jarvisroach over 8 years ago

    However, this should probably be updated in the Vivado design to get the FSBL tto set those registers correctly.