Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design Ubuntu Server on UltraZed
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 13 replies
  • Subscribers 360 subscribers
  • Views 1533 views
  • Users 0 members are here
Related

Ubuntu Server on UltraZed

tchoyt
tchoyt over 9 years ago

I've written up a guide on getting the UltraZed starter kit up and running on Ubuntu Server 16.04.2.  

There's no display port interface - just serial console and ethernet connectivity.  The included base design is very simple - just a ZynqMP PS with LED's and a block RAM.  

 

Please read the issues section at the bottom of the blog post as there area ALOT of things that don't work properly with the Xilinx 2016.4 release.  

 

The intent here is to use the associated github repo as a framework for getting your own custom design up and running on Linux.  

 

Blog Post:

http://www.twosixlabs.com/ubuntu-on-ultrazed-embedded-high-performance-computing/

 

Github Repo:

https://github.com/invincealabs/ultrazed_dev

 

EDIT:  We're in the middle of a company re-branding right now so the blog post has moved to our new website.  The github is currently still under Invincea Labs

  • Sign in to reply
  • Cancel

Top Replies

  • tchoyt
    tchoyt over 8 years ago in reply to dyessgg +1
    I don't think you did anything wrong. I've also seen that before in the Petalinux config - it seems to want to use full path names instead of relative path names. It could also be something I'm doing wrong…
Parents
  • tchoyt
    0 tchoyt over 9 years ago

    I was contacted by another engineer using the blog post and github repo to develop on the UltraZed who was experiencing a failure to boot that seemed to be a result of the clock generator jumpers being installed incorrectly.  The FSBL and uBoot would come up and then would stall when booting the kernel.  

     

    The 2017.1 update seems to disable the PS-PL reference clocks during the boot process, possibly in the PMU firmware to save power?  To work around this issue I now use the PL reference clock from the I/O breakout boards clock generator as a reference for the FPGA logic and the AXI HPM0 interface.  It's possible without this clock present the AXI interface could cause the kernel to fail to boot?

     

    The correct jumper locations are:  JP1 - OPEN,  J1- 1-2, J2 - 1-2

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • tchoyt
    0 tchoyt over 9 years ago

    I was contacted by another engineer using the blog post and github repo to develop on the UltraZed who was experiencing a failure to boot that seemed to be a result of the clock generator jumpers being installed incorrectly.  The FSBL and uBoot would come up and then would stall when booting the kernel.  

     

    The 2017.1 update seems to disable the PS-PL reference clocks during the boot process, possibly in the PMU firmware to save power?  To work around this issue I now use the PL reference clock from the I/O breakout boards clock generator as a reference for the FPGA logic and the AXI HPM0 interface.  It's possible without this clock present the AXI interface could cause the kernel to fail to boot?

     

    The correct jumper locations are:  JP1 - OPEN,  J1- 1-2, J2 - 1-2