Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design Ubuntu Server on UltraZed
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 13 replies
  • Subscribers 360 subscribers
  • Views 1532 views
  • Users 0 members are here
Related

Ubuntu Server on UltraZed

tchoyt
tchoyt over 9 years ago

I've written up a guide on getting the UltraZed starter kit up and running on Ubuntu Server 16.04.2.  

There's no display port interface - just serial console and ethernet connectivity.  The included base design is very simple - just a ZynqMP PS with LED's and a block RAM.  

 

Please read the issues section at the bottom of the blog post as there area ALOT of things that don't work properly with the Xilinx 2016.4 release.  

 

The intent here is to use the associated github repo as a framework for getting your own custom design up and running on Linux.  

 

Blog Post:

http://www.twosixlabs.com/ubuntu-on-ultrazed-embedded-high-performance-computing/

 

Github Repo:

https://github.com/invincealabs/ultrazed_dev

 

EDIT:  We're in the middle of a company re-branding right now so the blog post has moved to our new website.  The github is currently still under Invincea Labs

  • Sign in to reply
  • Cancel

Top Replies

  • tchoyt
    tchoyt over 8 years ago in reply to dyessgg +1
    I don't think you did anything wrong. I've also seen that before in the Petalinux config - it seems to want to use full path names instead of relative path names. It could also be something I'm doing wrong…
  • drozwood90
    0 drozwood90 over 9 years ago

    HI there,

    Thanks for the awesome write up using UltraZed!
    It seems pretty detailed and step-by-step!
    I'm going to ensure this gets stickied to help out the rest of the UltraZed community!

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tchoyt
    0 tchoyt over 9 years ago

    I've updated the Ubuntu on UltraZed design to the 2017.1 tools.  Pretty much all of the stability issues have been resolved so it's a very usable system at this point.

    Requirements:

    Vivado 2017.1, Xilinx SDK 2017.1 and Petalinx 2017.1

    Updates: 

    Petalinx 2017.1 is now used to build uBoot, ATF and the Linux kernel.

    The FSBL is ran on the RPU in lock-step mode.

    I've added a dummy AXI4-Lite register block to use as a starting point for interfacing to custom FPGA logic as well as a heartbeat LED.

    Blog Post/User Guide:
    https://www.invincealabs.com/blog/2017/03/ubuntu-ultrazed/
     
    Github Repo:
    https://github.com/invincealabs/ultrazed_dev

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tchoyt
    0 tchoyt over 9 years ago

    I was contacted by another engineer using the blog post and github repo to develop on the UltraZed who was experiencing a failure to boot that seemed to be a result of the clock generator jumpers being installed incorrectly.  The FSBL and uBoot would come up and then would stall when booting the kernel.  

     

    The 2017.1 update seems to disable the PS-PL reference clocks during the boot process, possibly in the PMU firmware to save power?  To work around this issue I now use the PL reference clock from the I/O breakout boards clock generator as a reference for the FPGA logic and the AXI HPM0 interface.  It's possible without this clock present the AXI interface could cause the kernel to fail to boot?

     

    The correct jumper locations are:  JP1 - OPEN,  J1- 1-2, J2 - 1-2

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tchoyt
    0 tchoyt over 8 years ago

    The repo has been updated to the 2017.3 tools and I'm now using Petalinux to build the Linux kernel, uBoot, device tree, FSBL and PMU firmware.  I'm still lagging behind updating the blog post but you *should* be able to use the 'build_all.sh' script to build everything.

     

    Stay tuned for a FreeRTOShellow world application running alongside Ubuntu on on the RPU

     

    Blog Post:

    https://www.twosixlabs.com/ubuntu-on-ultrazed-embedded-high-performance-computing/

     


    GitHub Repo:

    https://github.com/twosixlabs/ultrazed_dev

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • zjeng
    0 zjeng over 8 years ago

    Hi, super job!

    Do this build still address ES1 silicon?

    Any clue what to change to use production silicon?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tchoyt
    0 tchoyt over 8 years ago in reply to zjeng

    Hi,  Sorry it wasn't that clear in my post, this update is targeting the production silicon using the free webpack Vivado tools.

     

    I have verified that an FPGA image built against the production parts will configure and operate just fine in ES1 silicon so you should be fine using the ES Ultrazed starter kits. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dyessgg
    0 dyessgg over 8 years ago

    I pulled down the examples and tried to build the Ubuntu image.  It appears a path was embedded in a couple of the config files that reference paths with "thoyt" in the path.  Once I manually fixed those, I was able to build completely. 

    Am I possibly skipping a step somewhere to automatically update these?

    Now if my UltraZed Starter kit would come in, I can test it!

    Greg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tchoyt
    0 tchoyt over 8 years ago in reply to dyessgg

    I don't think you did anything wrong.  I've also seen that before in the Petalinux config - it seems to want to use full path names instead of relative path names. 

     

    It could also be something I'm doing wrong when i package up the Petalinux project.  I haven't come up with an easy way to fix instead of manually editing the path name before a build.  

     

    Thanks for the feedback.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tchoyt
    0 tchoyt over 8 years ago

    I've pushed an update that will fix the absolute path error in the Petalinux config file. 

    I added a PETA_TMP environment variable to replace the absolute path for CONFIG_TMP_DIR_LOCATION variable in this file './software/petalinux_build/project-spec/configs/config'.  

    PETA_TMP will be set every time you run ./scripts/env_setup.sh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dyessgg
    0 dyessgg over 8 years ago in reply to tchoyt

    Great news!  Thanks for your hard work and sharing it the rest of us.

    My UltraZed board is *scheduled* to arrive "mid-May".  I can't wait!

     

    Greg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>