Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design Ubuntu Server on UltraZed
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 13 replies
  • Subscribers 360 subscribers
  • Views 1533 views
  • Users 0 members are here
Related

Ubuntu Server on UltraZed

tchoyt
tchoyt over 9 years ago

I've written up a guide on getting the UltraZed starter kit up and running on Ubuntu Server 16.04.2.  

There's no display port interface - just serial console and ethernet connectivity.  The included base design is very simple - just a ZynqMP PS with LED's and a block RAM.  

 

Please read the issues section at the bottom of the blog post as there area ALOT of things that don't work properly with the Xilinx 2016.4 release.  

 

The intent here is to use the associated github repo as a framework for getting your own custom design up and running on Linux.  

 

Blog Post:

http://www.twosixlabs.com/ubuntu-on-ultrazed-embedded-high-performance-computing/

 

Github Repo:

https://github.com/invincealabs/ultrazed_dev

 

EDIT:  We're in the middle of a company re-branding right now so the blog post has moved to our new website.  The github is currently still under Invincea Labs

  • Sign in to reply
  • Cancel

Top Replies

  • tchoyt
    tchoyt over 8 years ago in reply to dyessgg +1
    I don't think you did anything wrong. I've also seen that before in the Petalinux config - it seems to want to use full path names instead of relative path names. It could also be something I'm doing wrong…
Parents
  • tchoyt
    0 tchoyt over 8 years ago

    I've pushed an update that will fix the absolute path error in the Petalinux config file. 

    I added a PETA_TMP environment variable to replace the absolute path for CONFIG_TMP_DIR_LOCATION variable in this file './software/petalinux_build/project-spec/configs/config'.  

    PETA_TMP will be set every time you run ./scripts/env_setup.sh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • tchoyt
    0 tchoyt over 8 years ago

    I've pushed an update that will fix the absolute path error in the Petalinux config file. 

    I added a PETA_TMP environment variable to replace the absolute path for CONFIG_TMP_DIR_LOCATION variable in this file './software/petalinux_build/project-spec/configs/config'.  

    PETA_TMP will be set every time you run ./scripts/env_setup.sh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • dyessgg
    0 dyessgg over 8 years ago in reply to tchoyt

    Great news!  Thanks for your hard work and sharing it the rest of us.

    My UltraZed board is *scheduled* to arrive "mid-May".  I can't wait!

     

    Greg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dyessgg
    0 dyessgg over 8 years ago in reply to tchoyt

    I received my UltraZed starter kit.  I've installed Vivado 2017.4, PetaLinux 2017.4, installed and activated the GIT large file support, cloned the repo, built the image, wrote the SD card, etc.  This was (seemingly) all successful.

    I set the jumpers according to instructions above (JP1 open, J1: 1-2, J2: 1-2) as well as the OOB settings.

    I set up the board to boot from SD card.
    It is loading uBoot from the SD card and attempting to boot the kernel.  Everything just hanges at "Starting kernel...".

    I did see a message from UBoot:
    treading ultrazed_base.bit
    t** Unable to read file ultrazed_base.bit **
    tWrong parameters for FPGA request
    tfpga - loadable FPGA image support

    Any thoughts?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dyessgg
    0 dyessgg over 8 years ago in reply to dyessgg

    Apparently I missed an error early in the build during the Vivado phase.
    1. There is an embedded "thoyt" in the ultrazed_base.xpr file.  Editing that got me a step further.

    2. There seems to be a missing directory:
    WARNING: [filemgmt 56-3] IPUserFilesDir: Could not find the directory '/home/arm/projects/ultrazed_dev/fpga/ultrazed_base/ultrazed_base.ip_user_files'.

    More as I get further along