Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design Debian/Linaro on Ultrazed, X11 does not start
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 360 subscribers
  • Views 624 views
  • Users 0 members are here
Related

Debian/Linaro on Ultrazed, X11 does not start

vcouvert
vcouvert over 8 years ago
 

Hello,

 

 

 

When trying to migrate from my Petalinux rootfs to a Debian (downloaded from Linaro), X11 no more starts on my UltraZed. Any ideas?

 

 

 

Here is the Xorg.0.log

 

[ 16.617] (II) Loader magic: 0x55710a2d70
   [ 16.617] (II) Module ABI versions:
   [ 16.617] X.Org ANSI C Emulation: 0.4
   [ 16.617] X.Org Video Driver: 19.0
   [ 16.617] X.Org XInput driver : 21.0
   [ 16.617] X.Org Server Extension : 9.0
   [ 16.621] (EE) systemd-logind: failed to get session: PID 4522 does not belon
   g to any known session
   [ 16.624] (II) xfree86: Adding drm device (/dev/dri/card0)
   [ 16.625] (II) no primary bus or device found
   [ 16.625] falling back to /sys/devices/platform/amba/amba:xilinx_drm/drm/c
   ard0
   [ 16.625] (II) "glx" will be loaded by default.
   [ 16.625] (II) LoadModule: "glx"
   [ 16.625] (II) Loading /usr/lib/xorg/modules/extensions/libglx.so
   [ 16.631] (II) Module glx: vendor="X.Org Foundation"
   [ 16.631] compiled for 1.17.3, module version = 1.0.0
   [ 16.631] ABI class: X.Org Server Extension, version 9.0
   [ 16.631] (==) AIGLX enabled
   [ 16.631] (II) LoadModule: "armsoc"
   [ 16.631] (II) Loading /usr/lib/xorg/modules/drivers/armsoc_drv.so
   [ 16.632] (II) Module armsoc: vendor="X.Org Foundation"
   [ 16.632] compiled for 1.17.3, module version = 1.4.0
   [ 16.632] Module class: X.Org Video Driver
   [ 16.632] ABI class: X.Org Video Driver, version 19.0
   [ 16.632] (II) ARMSOC: Driver for ARM Mali compatible chipsets
   [ 16.632] (++) using VT number 7

 

[ 16.632] (WW) Falling back to old probe method for armsoc
   [ 16.632] (II) No BusID or DriverName specified - opening /dev/dri/card0
   [ 16.632] (II) Got BusID
   [ 16.632] (II) Opened DRM
   [ 16.633] (II) DeviceName is [/dev/dri/card0]
   [ 16.633] (II) bus_id is []
   [ 16.633] (II) DriverName is [xilinx_drm]
   [ 16.633] (II) version is [1.0.0]
   [ 16.633] (II) Screen:0, CRTC:-1
   [ 16.633] (WW) VGA arbiter: cannot open kernel arbiter, no multi-card support
   [ 16.633] (II) ARMSOC(0): Creating default Display subsection in Screen secti
   on
   "Default Screen Section" for depth/fbbpp 24/32
   [ 16.633] (==) ARMSOC(0): Depth 24, (==) framebuffer bpp 32
   [ 16.633] (==) ARMSOC(0): RGB weight 888
   [ 16.633] (==) ARMSOC(0): Using gamma correction (1.0, 1.0, 1.0)
   [ 16.633] (==) ARMSOC(0): Default visual is TrueColor
   [ 16.633] (II) No BusID or DriverName specified - opening /dev/dri/card0
   [ 16.633] (II) Got BusID
   [ 16.633] (II) Opened DRM
   [ 16.633] (II) DeviceName is [/dev/dri/card0]
   [ 16.633] (II) bus_id is []
   [ 16.633] (II) DriverName is [xilinx_drm]
   [ 16.633] (II) version is [1.0.0]
   [ 16.634] (II) UnloadModule: "armsoc"
   [ 16.634] (EE) Screen(s) found, but none have a usable configuration.
   [ 16.634] (EE)
   Fatal server error:
   [ 16.634] (EE) no screens found(EE)
   [ 16.634] (EE)
   Please consult the The X.Org Foundation support
   at http://wiki.x.org
   for help.
   [ 16.634] (EE) Please also check the log file at "/var/log/Xorg.0.log" for ad
   ditional information.
   [ 16.634] (EE)
   [ 16.654] (EE) Server terminated with error (1). Closing log file.

 

 

 

Thanks for your help.

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 8 years ago

    Hi vcouvert,

    What changes when you migrate from your Petalinux rootfs to a Debian build?

    Do you change your HW platform (from Vivado) or your device tree (from PetaLinux) at all?

    Best Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • vcouvert
    0 vcouvert over 8 years ago in reply to zedhed

    Hi zedhed,

    Thanks for your answer.

    I did not change anything in the HW platform and I just removed the PCI support in the kernel (as explained here: http://www.wiki.xilinx.com/Zynq+UltraScale%EF%BC%8B+MPSoC+Ubuntu+part+2+-+Building+and+Running+the+Ubuntu+Desktop+From+Sources).

    I also tried with the roofs from the image given on this Wiki page (Ubuntu_Desktop_Release_2017_1.zip) and I see the mouse cursor displayed on my screen for a few seconds (I can even move it using the mouse) a nd then it disappear...

    Vincent

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • vcouvert
    0 vcouvert over 8 years ago in reply to zedhed

    Hi zedhed,

    Thanks for your answer.

    I did not change anything in the HW platform and I just removed the PCI support in the kernel (as explained here: http://www.wiki.xilinx.com/Zynq+UltraScale%EF%BC%8B+MPSoC+Ubuntu+part+2+-+Building+and+Running+the+Ubuntu+Desktop+From+Sources).

    I also tried with the roofs from the image given on this Wiki page (Ubuntu_Desktop_Release_2017_1.zip) and I see the mouse cursor displayed on my screen for a few seconds (I can even move it using the mouse) a nd then it disappear...

    Vincent