Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design SD card boot + rootfs
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Subscribers 361 subscribers
  • Views 3446 views
  • Users 0 members are here
Related

SD card boot + rootfs

micahstevens
micahstevens over 8 years ago

Hi,

I've been attempting to get the UltraZed_IOCC_BSP to boot and run the rootfs off the SD card. I can import the fresh BSP and build it, using those images the example boots as an initramfs image fine. I can log in, etc. 

Step 1:

If I merely switch Image Packaging Configuration -> Root Filesystem Type to "SD card". Then I rebuild with petalinux-build. I then put BOOT.BIN, image.ub and system.dtb on the first fat32 partition of 1 gig on a 16 gig sd-card. I then use 'dd' to write rootfs.ext3 to the second partition. 

Kernel begins to boot, but fails some time after the logging to the serial port stops. (See #2 below).  Here is a link to the boot log: 

Pastebin Log

Step 2: 

If I go in and add the console=ttyPS0,115200 stuff to the boot args (petalinux-config -> Kernel Bootargs) I notice it's pointing the rootfs to the wrong partition, so I update the argument string. 

Original: earlycon clk_ignore_unused root=/dev/mmcblk0p2 rw rootwait

Updated: earlycon earlyprintk clk_ignore_unused root=/dev/mmcblk1p2 rw rootwait console=ttyPS0,115200

This works better as I can now see that I'm getting a kernel panic:

Bad mode in Error handler detected on CPU1, code 0xbf000000 -- SError

Pastebin Log

Step 3: 

Based on some research I discovered that as it's delivered, the BSP does not configure a write protect pin for the SD card in the device tree. (MIO 44) - however the system will look for the write protect jumper status (SD_WP_N on the carrier board). This prevents a partition from being mounted in RW mode. If you put 'disable-wp;' in the @sdhci0/1 device tree entries in system-user.dtsi, this pin (MIO 44?) will no be referenced and you can mount the filesystems on the card in RW mode.

I was able to verify this works in initramfs, but it did not fix the above kernel panic. 

Question: Do you see that I'm doing something wrong here? Has anyone run into this before? It seems like this should be a simple operation, but I've been working on various iterations of the build for several days and nothing seems to work. I would love some insight on a procedure that works (or a working BSP would be AMAZING) 

Thank you in advance for any help! 

My system-user.dtsi.

My project config.

My u-boot environment.

  • Sign in to reply
  • Cancel

Top Replies

  • micahstevens
    micahstevens over 8 years ago +1 verified
    Boot from SD Card: I started with a project from scratch, instead of the downloaded BSP. I then added this manual kernel bootcmd: earlycon earlyprintk clk_ignore_unused root=/dev/mmcblk1p2 rw rootwait…
Parents
  • e14 Contributor
    0 e14 Contributor over 8 years ago

    The lines in your log just before things fall apart are:

    [    1.596896] GPIO IRQ not connected
    [    1.600109] XGpio: /amba_pl@0/gpio@80000000: registered, base is 504
    [    1.606638] GPIO IRQ not connected
    [    1.609849] XGpio: /amba_pl@0/gpio@80010000: registered, base is 496
    [    1.616214] Bad mode in Error handler detected on CPU1, code 0xbf000000 -- SError

    On my system, the equivalent lines are:

    [    1.337569] GPIO IRQ not connected
    [    1.337583] XGpio: /amba_pl@0/gpio@80000000: registered, base is 330
    [    1.337727] GPIO IRQ not connected
    [    1.337740] XGpio: /amba_pl@0/gpio@80010000: registered, base is 322
    [    1.337878] GPIO IRQ not connected
    [    1.337890] XGpio: /amba_pl@0/gpio@80020000: registered, base is 319

    So perhaps you're missing a GPIO block that it's expecting to find at 0x80020000?

    We've gotten this working on the IOCC by building off of the DisplayPort reference design.  PM me and I can send you a document explaining what we've done so far.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 8 years ago

    The lines in your log just before things fall apart are:

    [    1.596896] GPIO IRQ not connected
    [    1.600109] XGpio: /amba_pl@0/gpio@80000000: registered, base is 504
    [    1.606638] GPIO IRQ not connected
    [    1.609849] XGpio: /amba_pl@0/gpio@80010000: registered, base is 496
    [    1.616214] Bad mode in Error handler detected on CPU1, code 0xbf000000 -- SError

    On my system, the equivalent lines are:

    [    1.337569] GPIO IRQ not connected
    [    1.337583] XGpio: /amba_pl@0/gpio@80000000: registered, base is 330
    [    1.337727] GPIO IRQ not connected
    [    1.337740] XGpio: /amba_pl@0/gpio@80010000: registered, base is 322
    [    1.337878] GPIO IRQ not connected
    [    1.337890] XGpio: /amba_pl@0/gpio@80020000: registered, base is 319

    So perhaps you're missing a GPIO block that it's expecting to find at 0x80020000?

    We've gotten this working on the IOCC by building off of the DisplayPort reference design.  PM me and I can send you a document explaining what we've done so far.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 8 years ago in reply to e14 Contributor

    I went back and looked at my design, and I've got three GPIO blocks instantiated in the fabric, so that's why those are in my boot log.  Yours is probably different.  If it helps, my boot log is here: https://pastebin.com/XkUyX1xV

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • micahstevens
    0 micahstevens over 8 years ago in reply to e14 Contributor

    Hi!

    Thanks for taking a look. This is a good point, I'm expecting 3, but it's not hanging when I boot into a RAM rootfs, so I wonder what the difference is there? I'll look more into it, I missed this entirely. 

    I'll also try the same experiment with the DisplayPort design. I'll PM you.