Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design SD card boot + rootfs
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Subscribers 361 subscribers
  • Views 3446 views
  • Users 0 members are here
Related

SD card boot + rootfs

micahstevens
micahstevens over 8 years ago

Hi,

I've been attempting to get the UltraZed_IOCC_BSP to boot and run the rootfs off the SD card. I can import the fresh BSP and build it, using those images the example boots as an initramfs image fine. I can log in, etc. 

Step 1:

If I merely switch Image Packaging Configuration -> Root Filesystem Type to "SD card". Then I rebuild with petalinux-build. I then put BOOT.BIN, image.ub and system.dtb on the first fat32 partition of 1 gig on a 16 gig sd-card. I then use 'dd' to write rootfs.ext3 to the second partition. 

Kernel begins to boot, but fails some time after the logging to the serial port stops. (See #2 below).  Here is a link to the boot log: 

Pastebin Log

Step 2: 

If I go in and add the console=ttyPS0,115200 stuff to the boot args (petalinux-config -> Kernel Bootargs) I notice it's pointing the rootfs to the wrong partition, so I update the argument string. 

Original: earlycon clk_ignore_unused root=/dev/mmcblk0p2 rw rootwait

Updated: earlycon earlyprintk clk_ignore_unused root=/dev/mmcblk1p2 rw rootwait console=ttyPS0,115200

This works better as I can now see that I'm getting a kernel panic:

Bad mode in Error handler detected on CPU1, code 0xbf000000 -- SError

Pastebin Log

Step 3: 

Based on some research I discovered that as it's delivered, the BSP does not configure a write protect pin for the SD card in the device tree. (MIO 44) - however the system will look for the write protect jumper status (SD_WP_N on the carrier board). This prevents a partition from being mounted in RW mode. If you put 'disable-wp;' in the @sdhci0/1 device tree entries in system-user.dtsi, this pin (MIO 44?) will no be referenced and you can mount the filesystems on the card in RW mode.

I was able to verify this works in initramfs, but it did not fix the above kernel panic. 

Question: Do you see that I'm doing something wrong here? Has anyone run into this before? It seems like this should be a simple operation, but I've been working on various iterations of the build for several days and nothing seems to work. I would love some insight on a procedure that works (or a working BSP would be AMAZING) 

Thank you in advance for any help! 

My system-user.dtsi.

My project config.

My u-boot environment.

  • Sign in to reply
  • Cancel

Top Replies

  • micahstevens
    micahstevens over 8 years ago +1 verified
    Boot from SD Card: I started with a project from scratch, instead of the downloaded BSP. I then added this manual kernel bootcmd: earlycon earlyprintk clk_ignore_unused root=/dev/mmcblk1p2 rw rootwait…
Parents
  • e14 Contributor
    0 e14 Contributor over 8 years ago

    The lines in your log just before things fall apart are:

    [    1.596896] GPIO IRQ not connected
    [    1.600109] XGpio: /amba_pl@0/gpio@80000000: registered, base is 504
    [    1.606638] GPIO IRQ not connected
    [    1.609849] XGpio: /amba_pl@0/gpio@80010000: registered, base is 496
    [    1.616214] Bad mode in Error handler detected on CPU1, code 0xbf000000 -- SError

    On my system, the equivalent lines are:

    [    1.337569] GPIO IRQ not connected
    [    1.337583] XGpio: /amba_pl@0/gpio@80000000: registered, base is 330
    [    1.337727] GPIO IRQ not connected
    [    1.337740] XGpio: /amba_pl@0/gpio@80010000: registered, base is 322
    [    1.337878] GPIO IRQ not connected
    [    1.337890] XGpio: /amba_pl@0/gpio@80020000: registered, base is 319

    So perhaps you're missing a GPIO block that it's expecting to find at 0x80020000?

    We've gotten this working on the IOCC by building off of the DisplayPort reference design.  PM me and I can send you a document explaining what we've done so far.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • micahstevens
    0 micahstevens over 8 years ago in reply to e14 Contributor

    Hi!

    Thanks for taking a look. This is a good point, I'm expecting 3, but it's not hanging when I boot into a RAM rootfs, so I wonder what the difference is there? I'll look more into it, I missed this entirely. 

    I'll also try the same experiment with the DisplayPort design. I'll PM you. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • micahstevens
    0 micahstevens over 8 years ago in reply to e14 Contributor

    Hi!

    Thanks for taking a look. This is a good point, I'm expecting 3, but it's not hanging when I boot into a RAM rootfs, so I wonder what the difference is there? I'll look more into it, I missed this entirely. 

    I'll also try the same experiment with the DisplayPort design. I'll PM you.