Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design Ultrazed EG PCIe Carrier Card definition files
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 359 subscribers
  • Views 986 views
  • Users 0 members are here
Related

Ultrazed EG PCIe Carrier Card definition files

ramuzed
ramuzed over 7 years ago

Hi,

I am attempting to build the U-boot to run on the UltraZed-EG PCIe Carrier card with the UltraZed EG SOM. I have downloaded the
latest snapshot of U-boot from the Git repo.   Searching through the configs directory, I do not see a defconfig file for your board. Could anyone
please tell me where I can find the correct defconfig file to use?  I believe one must exist or there is a compatible defconfig file to use because I
have been able to run  the prebuilt U-BOOT that is part of the AES-ZU3EGES-1-SOM-G-OOB-Release-RC3_0 package.

  • Sign in to reply
  • Cancel
  • drozwood90
    0 drozwood90 over 7 years ago

    Hi!,

    I believe if there is a file, it is located in the BSP, have you checked within there?  We include everything that is needed to work with our systems within those BSP files.

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • zedusage
    0 zedusage over 7 years ago in reply to drozwood90

    Hi
    Dan,

     
    I am trying to build UBoot for UZ3EG-PCIEC but having trouble finding the
    defconfig file in the zedboard BSP. I need help identifying the correct
    defconfig file to use. There are close to 500 defconfig files within the
    uz3eg_pciec_2018_2 BSP and 115 defconfig files in the arm folder, so it
    would help to identify the correct one to use.

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • narrucmot
    0 narrucmot over 7 years ago

    Hi Karthick,

     

    The u-boot defconfig is specified in the PetaLinux project config file (<project folder>/project-spec/configs/config):

     

    #

    # u-boot Configuration

    #

    CONFIG_SUBSYSTEM_UBOOT_CONFIG_PETALINUX=y

    # CONFIG_SUBSYSTEM_UBOOT_CONFIG_OTHER is not set

    CONFIG_SUBSYSTEM_UBOOT_CONFIG_TARGET="xilinx_zynqmp_zcu102_rev1_0_defconfig"

    CONFIG_SUBSYSTEM_NETBOOT_OFFSET=0x10000000

    CONFIG_SUBSYSTEM_U__BOOT_TFTPSERVER_IP="AUTO"

     

    The Ultrazed SOM is similar enough to the ZCU102 board that it can use the same u-boot defconfig.  You can either hand edit this file or run 'petalinux-config' from the PetaLinux project folder.

     

    I hope this helps.

     

    --Tom