Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design UltraZed-EV SATA Drive Power Sequence
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Answers 2 answers
  • Subscribers 359 subscribers
  • Views 1100 views
  • Users 0 members are here
  • ultrazed-ev starter kit
  • sata
Related

UltraZed-EV SATA Drive Power Sequence

ralphjy
ralphjy over 6 years ago

I want to add an external SATA 3 SSD drive to the UltraZed-EV Carrier Card interface and the drive uses a separate power source than the Carrier Card.  Should I power up the carrier card first and then the drive?  That would seem like the correct sequence.  I don't see a sequence specifically mentioned in the documentation (UltraZed SATA Performance Test Tutorial) but it seems to imply that the drive is powered first.  Just wanted to check -- hate to have any smoke.

 

Thanks,

Ralph

  • Sign in to reply
  • Cancel

Top Replies

  • ctammann
    ctammann over 6 years ago +1 verified
    Hey Ralph, yes I would recommend powering up the UltraZed EV first. If the drive powers up first and sends data over the I/O before the Ultrascale is configured it "could" damage it. I'm not saying it…
  • narrucmot
    narrucmot over 6 years ago in reply to ralphjy +1 suggested
    Hi Ralph, The PMIC programming and telemetry reading app that Chris mentioned in his webinar today will be released as part of the upcoming PetaLinux 2020.1 BSP releases for the Ultra96-V2 and UltraZed…
  • narrucmot
    narrucmot over 6 years ago in reply to ralphjy +1 suggested
    The app will also work in PetaLinux 2019.2 if one wishes to back-port it. --Tom
  • ctammann
    0 ctammann over 6 years ago

    Hey Ralph, yes I would recommend powering up the UltraZed EV first. If the drive powers up first and sends data over the I/O before the Ultrascale is configured it "could" damage it. I'm not saying it definitely will, but safest bet is to power the EV system, then power the drive

    Thanks
    Chris

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ralphjy
    0 ralphjy over 6 years ago in reply to ctammann

    Thanks Chris.

     

    Somewhat unrelated question.  I attended your PMBus webinar which was great.  You mentioned that the program to update the Ultra96 isn’t available yet but are the monitoring programs for the Ultra96 and UltraZed-EV boards that you demonstrated available? 

    Ralph

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • narrucmot
    0 narrucmot over 6 years ago in reply to ralphjy

    Hi Ralph,

     

    The PMIC programming and telemetry reading app that Chris mentioned in his webinar today will be released as part of the upcoming PetaLinux 2020.1 BSP releases for the Ultra96-V2 and UltraZed SOMs.  It will also be public via github at the same time.  Stay tuned!

     

    --Tom

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ralphjy
    0 ralphjy over 6 years ago in reply to narrucmot

    Thanks Tom - I’ll be watching for it.  Really useful stuff!

     

    Does the app require something in the 2020.1 BSP or will it work with 2019.2?

     

    Ralph

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • narrucmot
    0 narrucmot over 6 years ago in reply to ralphjy

    The app will also work in PetaLinux 2019.2 if one wishes to back-port it.

     

    --Tom

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer