Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design Infineon Power Supplies in UltraZed EV Carrier Card
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 359 subscribers
  • Views 1439 views
  • Users 0 members are here
  • ultrazed
Related

Infineon Power Supplies in UltraZed EV Carrier Card

abhishekkunal
abhishekkunal over 4 years ago

Hi,

 

I have designed a custom carrier card for UltraZed EV SOM( AES-ZU7EV-1-SOM-I-G).In my custom Carrier card, I have retained power section comprising of Infineon devices

same as in Carrier card Evaluation board .

 

For programming Infineon PMICs. I have received three column  configuration files for all the Infineon ICs from  Avnet Local FAE.

Also, we have an Evaluation board comprising of AES-ZU7EV-1-SOM-I-G  along with Carrier Card with us which is being used for initial prototyping.

 

We are finding that there is a mismatch at few places in the three column configuration files received from AVNET FAE and the files which we have saved by using PMBUS USB005

dongle  and PowIRCenter GUI from the existing Eval board carrier card for Infineon ICs IRPS5401 (I2C Addresses:0x19,0x1A). Also, the CRC32 checksum is not matching.

However, the configuration files for Manhattan devices IR38063 on carrier card are identical.

 

Is there any version issue related to Infineon PMIC(schematic:U21 and U22 ,I2C Addresses:0x19,0x1A) between AVNET supplied file and file obtained from carrier card evaluation board?

 

Pl suggest, which configuration files should be used for custom carrier card. Otherwise, pl send latest three column files for these two IRPS5401 PMICs.

 

I am attaching one pair of files for reference.

 

Meanwhile we are trying to understand the differences between those files and their significance.

Attachments:
111617_cc_0x1A.txt.zip
1A_3col.txt.zip
  • Sign in to reply
  • Cancel
Parents
  • ctammann
    ctammann over 4 years ago

    Hi, sorry for the really late reply on this post. I believe I may have followed up with you through email and the FAE, if not I apologize I never saw this post. The mix match is most likely due to a different PMIC config version being in the carrier. There was an updated file in April of 2021 that improved thermal performance and became the new "default" files. I've attached the zip file here for all UltraZed IRPS5401 configurations. Keep in mind this zip contains EG and EV files so be sure to use the right file that matches your address. The files in the attached zip are the latest and current versions for all UltraZed IRPS5401 PMICs. UltraZed_IRPS5401_04_21_2021_Master.zip

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ctammann
    ctammann over 4 years ago

    Hi, sorry for the really late reply on this post. I believe I may have followed up with you through email and the FAE, if not I apologize I never saw this post. The mix match is most likely due to a different PMIC config version being in the carrier. There was an updated file in April of 2021 that improved thermal performance and became the new "default" files. I've attached the zip file here for all UltraZed IRPS5401 configurations. Keep in mind this zip contains EG and EV files so be sure to use the right file that matches your address. The files in the attached zip are the latest and current versions for all UltraZed IRPS5401 PMICs. UltraZed_IRPS5401_04_21_2021_Master.zip