Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design Replicate the pre-built/linux/images/BOOT.BIN
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 359 subscribers
  • Views 2163 views
  • Users 0 members are here
Related

Replicate the pre-built/linux/images/BOOT.BIN

AshwinRavisankar
AshwinRavisankar over 4 years ago

Hi, I am using Xilinx AVNET 2020.2 BSP to create a petalinux project. Link to BSP : https://avtinc.sharepoint.com/teams/ET-Downloads/Shared%20Documents/Forms/AllItems.aspx?id=%2Fteams%2FET%2DDownloads%2FShared%20Documents%2Fprojects%2Fpublic%5Frelease%2F2020%2E2%2FBSP&viewid=dba68156%2Dce4b%2D4ebb%2Db7a7%2Dec03b27b013d

 When i create the project, the BSP provides me with a pre-built-/linux/images/* folder which contains all the boot images which can be used to boot using SD card. I am trying to replicate the pre-built/linux/images/BOOT.BIN by using the following command :

 petalinux-package --boot --fsbl ./pre-built/linux/images/zynqmp_fsbl.elf --atf pre-built/linux/images/bl31.elf --kernel pre-built/linux/images/image.ub --pmufw ./pre-built/linux/images/pmufw.elf --psmfw no --u-boot ./pre-built/linux/images/u-boot.elf --dtb ./pre-built/linux/images/system.dtb --force

 The above command ideally should create an identical BOOT.BIN in the images/linux/ area since i am using the pre-built *.elf files (boot loader files) to package. But when i try to boot using the generated BOOT.BIN the FPGA hangs at the kernel boot stage. Whereas the already existing BOOT.BIN in the pre-built/linux/images area does not cause this hang issue and boots successfully, I am not able to understand where I am going wrong.

 I am trying this debug step, inorder to debug another similar boot hang issue which is related to boot from SD card where in i modify the device tree to enable GEM0 ethernet MAC , do a petalinux-build and then finally package the generated boot images into a BOOT.BIN. To clean up the flow i was trying the above but I am stuck here. Kindly help.

BootLog :

Xilinx Zynq MP First Stage Boot Loader
Release 2020.2   Apr 28 2021  -  07:36:59
NOTICE:  ATF running on XCZU7EV/silicon v4/RTL5.1 at 0xfffea000
NOTICE:  BL31: v2.2(release):xlnx_rebase_v2.2_2020.3
NOTICE:  BL31: Built : 12:52:01, Dec  2 2021


U-Boot 2020.01 (Dec 02 2021 - 12:52:05 +0000)

Board: Xilinx ZynqMP
DRAM:  4 GiB
PMUFW:  v1.1
EL Level:       EL2
Chip ID:        zu7ev
NAND:  0 MiB
MMC:   mmc@ff160000: 0, mmc@ff170000: 1
In:    serial@ff000000
Out:   serial@ff000000
Err:   serial@ff000000
Bootmode: SD_MODE1
Reset reason:   EXTERNAL
Net:
ZYNQ GEM: ff0e0000, mdio bus ff0e0000, phyaddr 0, interface rgmii-id

Warning: ethernet@ff0e0000 using MAC address from DT
eth0: ethernet@ff0e0000
Hit any key to stop autoboot:  0
switch to partitions #0, OK
mmc1 is current device
Scanning mmc 1:1...
Found U-Boot script /boot.scr
2007 bytes read in 16 ms (122.1 KiB/s)
## Executing script at 20000000
8653876 bytes read in 596 ms (13.8 MiB/s)
## Loading kernel from FIT Image at 10000000 ...
   Using 'conf@system-top.dtb' configuration
   Trying 'kernel@1' kernel subimage
     Description:  Linux kernel
     Type:         Kernel Image
     Compression:  gzip compressed
     Data Start:   0x100000f4
     Data Size:    8609540 Bytes = 8.2 MiB
     Architecture: AArch64
     OS:           Linux
     Load Address: 0x00080000
     Entry Point:  0x00080000
     Hash algo:    sha256
     Hash value:   47d9532b392e118b3285ad44b32a9ed2dc51193a7a98087e2d1e12d2dcf6db04
   Verifying Hash Integrity ... sha256+ OK
## Loading fdt from FIT Image at 10000000 ...
   Using 'conf@system-top.dtb' configuration
   Trying 'fdt@system-top.dtb' fdt subimage
     Description:  Flattened Device Tree blob
     Type:         Flat Device Tree
     Compression:  uncompressed
     Data Start:   0x10836108
     Data Size:    42435 Bytes = 41.4 KiB
     Architecture: AArch64
     Hash algo:    sha256
     Hash value:   d9a4798dfee82827ce54d447f24ca3d7daa68c65aed768120d521d31b22c9b1a
   Verifying Hash Integrity ... sha256+ OK
   Booting using the fdt blob at 0x10836108
   Uncompressing Kernel Image
   Loading Device Tree to 000000000fff2000, end 000000000ffff5c2 ... OK

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[    0.000000] Linux version 5.4.0-xilinx-v2020.2 (oe-user@oe-host) (gcc version 9.2.0 (GCC)) #1 SMP Tue Nov 30 15:28:10 UTC 2021
[    0.000000] Machine model: xlnx,zynqmp
[    0.000000] earlycon: cdns0 at MMIO 0x00000000ff000000 (options '115200n8')
[    0.000000] printk: bootconsole [cdns0] enabled
[    0.000000] efi: Getting EFI parameters from FDT:
[    0.000000] efi: UEFI not found.
[    0.000000] cma: Reserved 1024 MiB at 0x000000003fc00000
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: MIGRATE_INFO_TYPE not supported.
[    0.000000] psci: SMC Calling Convention v1.1
[    0.000000] percpu: Embedded 21 pages/cpu s48600 r8192 d29224 u86016
[    0.000000] Detected VIPT I-cache on CPU0
[    0.000000] CPU features: detected: ARM erratum 845719
[    0.000000] Speculative Store Bypass Disable mitigation not required
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 1031940
[    0.000000] Kernel command line:  earlycon console=ttyPS0,115200 clk_ignore_unused root=/dev/mmcblk1p2 rw rootwait
[    0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
[    0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[    0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[    0.000000] software IO TLB: mapped [mem 0x3bc00000-0x3fc00000] (64MB)
[    0.000000] Memory: 2979980K/4193280K available (12412K kernel code, 756K rwdata, 3808K rodata, 768K init, 562K bss, 164724K reserved, 1048576K cma-reserved)
[    0.000000] rcu: Hierarchical RCU implementation.
[    0.000000] rcu:     RCU event tracing is enabled.
[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000
[    0.000000] GIC: Using split EOI/Deactivate mode
[    0.000000] irq-xilinx: /amba/axi-interrupt-ctrl: num_irq=32, sw_irq=0, edge=0x0

  • Sign in to reply
  • Cancel
  • bhfletcher
    0 bhfletcher over 4 years ago

    I notice in this blog from narrucmot that Avnet has provided rebuilt scripts that should do some of this automatically for you. Have you tried those already? If the rebuild scripts work but yours do not, then it would be worth a line by line comparison to see what the differences are.

    /technologies/fpga-group/b/blog/posts/using-avnet-build-scripts-to-build-a-petalinux-bsp-2020-1-and-later

    Bryan