Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design UltraZed-EG™︎ SOM power and boot issue
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 359 subscribers
  • Views 893 views
  • Users 0 members are here
  • UltraZed-EG™ SOM
Related

UltraZed-EG™︎ SOM power and boot issue

Cpt.5xtar
Cpt.5xtar over 3 years ago

Accidently +28V applied to Vin. Now SOM doesn't boot up and current is also limited. red led is glowing

How to reset? or how to debugg this issue.

Kindly help

  • Sign in to reply
  • Cancel

Top Replies

  • baldengineer
    baldengineer over 3 years ago +1
    Looking at the schematic (link under "Schematics" on this page ) there are three active parts connected to VIN: A switching regulator and two PMICs. (Page 15, 16, 17.) The switching regulator, TPS62173…
  • baldengineer
    0 baldengineer over 3 years ago

    Looking at the schematic (link under "Schematics" on this page) there are three active parts connected to VIN: A switching regulator and two PMICs.

    (Page 15, 16, 17.)

    The switching regulator, TPS62173, has a maximum input of 20 V.

    Both PMICs are an IRPS5401. These have an absolute max of 16 V.

    So either all three chips are blown are some combination of them. I would suspect the PMICs are the most likely to be damaged. You might be able to determine which ones are dead by finding VCC pins from their outputs and measuring them with a DMM.

    With luck, these relatively cheap power ICs saved the significantly more expensive (and much more difficult to replace) Zynq.

    Regardless, there is likely no "reset" option. You have to replace the components that were damaged.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Cpt.5xtar
    0 Cpt.5xtar over 3 years ago in reply to baldengineer

    thank you sir. lets hope for the best