Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design UltraZedEG, Petalinux 2023.1 BSP
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 357 subscribers
  • Views 2419 views
  • Users 0 members are here
Related

UltraZedEG, Petalinux 2023.1 BSP

e2kcpu
e2kcpu over 2 years ago

Anybody is using it?

I have a problem, as it fail pretty early:

Summary: There were 5 WARNING messages.
[ERROR] mconf/conf command not found
ERROR: Failed to run gen-machineconf
ERROR: Failed to build project. Check the /AD1/PUB/PETA.2023.1/AVNET_UZ3EG_IOCC_BASE/uz3eg_iocc_base_2023_1/build/build.log file for more details...

And another one, is there the updated 2023.1 HW design somewhere too?

Cheers & thanks

  • Sign in to reply
  • Cancel
Parents
  • padudle
    padudle over 2 years ago

    Hello,

    Many board vendors do not maintain Petalinux BSP anymore because they are not really needed.  It is easier and more reliable to create a .xsa file from a compiled Vivado design and reference it in your Petalinux build, like here: https://github.com/hdlguy/zuboard/tree/main/petalinux

    It is this statement that reads in my xsa file.

       petalinux-config --get-hw-description=../../implement/results/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • padudle
    padudle over 2 years ago

    Hello,

    Many board vendors do not maintain Petalinux BSP anymore because they are not really needed.  It is easier and more reliable to create a .xsa file from a compiled Vivado design and reference it in your Petalinux build, like here: https://github.com/hdlguy/zuboard/tree/main/petalinux

    It is this statement that reads in my xsa file.

       petalinux-config --get-hw-description=../../implement/results/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e2kcpu
    e2kcpu over 2 years ago in reply to padudle

    I think, something went wrong, when Ubuntu does updates ... Anyway, after re-installing petalinux, it started again. So I got two of my projects

    compiling again. (uz3eg_iocc & uz3eg_pcie), one actually starts and gets pretty far, the other just prints the first two lines of the Bootloader

    I guess, there is still something wrong in the setup ...

    Thanks for your time !

    P.S. I see, that the hdlguy also has the ACAU15 board, I just got too :)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • padudle
    padudle over 2 years ago in reply to e2kcpu

    Yes, the ACAU15 board looks great. Unfortunately, I have been able to run neither the DDR4 memory nor the PCIe interface.  The example designs from Alinx seem to work but not any of my designs. Oh well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e2kcpu
    e2kcpu over 2 years ago in reply to padudle

    You got me convinced, to just use the compiled Vivado designs ...

    But, where do I find the Vivado projects for those boards?

    Specially, the ones for the working Petalinux examples?

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • minita
    minita over 2 years ago in reply to e2kcpu

    Hello, Follow these steps: https://www.hackster.io/AlbertaBeef/zuboard-building-the-foundational-designs-f114d5, not all of them just the beginning where you download / clone the repos.

    Run the hdl/scripts/make_zub1cg_sbc_base.tcl, this will create thevivado project and the block diagram.  Remember to download the 2023.1 branch

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e2kcpu
    e2kcpu over 2 years ago in reply to minita

    It looks exactly like the blog I was looking for!

    Thanks!

    Few remarks, you could fix/add to your blog:

    paragraph "re-Enabling the Cache"

    I think there is a wrong path in

    project-spec/meta-user/configs/petalinuxbsp.conf

    it should be (at least in 2023.1)

    project-spec/meta-user/conf/petalinuxbsp.conf

    And I think other developers would appreciate the warning, that all this cache setup is important to check twice.

    There is no warning, if the path/files don't exist, it just runs very slow again. If all caching works, the whole compile is done in minutes, without caching it is hours ...

    And, I really appreciate the help here, and REALLY happy, that those boards are still supported somehow.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • minita
    minita over 2 years ago in reply to e2kcpu

    I have to clarify that is not my blog, but I am glad it was useful. I got myself a ZUBoard and I am in the same journey of figuring out things. You are right, that is a good observation. You should add in the commends of the blog that information so it gets recorded and other people can see it.