Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design UltraZed-EV GC LVDS Clock DC Coupling
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 358 subscribers
  • Views 957 views
  • Users 0 members are here
Related

UltraZed-EV GC LVDS Clock DC Coupling

revky
revky over 1 year ago

Hi,

I am using a SI5341 to generate a 400MHz to use as global clock on the UltraZed-EV+.

The SI5341 output buffer supply is +3V3 and the FPGA HP bank is +1V8.

The output buffer common mode voltage for this is 1.1V to 1.3V and swing is 350mV to 510mV. Due to the fact that the FPGA is on the SoM I cannot use ac coupling next to the FPGA.

My question is can I get away with DC coupling if the LVDS voltages are within range of the FPGA or should I use AC-coupling before the SoM Module?

  • Sign in to reply
  • Cancel
Parents
  • padudle
    padudle over 1 year ago

    In theory it does not matter where you put the AC coupling capacitors.  They do not need to be at the load. They can be at the source or anywhere in between. 

    For LVDS you do want the termination resistance at the load though.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • padudle
    padudle over 1 year ago

    In theory it does not matter where you put the AC coupling capacitors.  They do not need to be at the load. They can be at the source or anywhere in between. 

    For LVDS you do want the termination resistance at the load though.