Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design UltraZed-EV GC LVDS Clock DC Coupling
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 358 subscribers
  • Views 955 views
  • Users 0 members are here
Related

UltraZed-EV GC LVDS Clock DC Coupling

revky
revky over 1 year ago

Hi,

I am using a SI5341 to generate a 400MHz to use as global clock on the UltraZed-EV+.

The SI5341 output buffer supply is +3V3 and the FPGA HP bank is +1V8.

The output buffer common mode voltage for this is 1.1V to 1.3V and swing is 350mV to 510mV. Due to the fact that the FPGA is on the SoM I cannot use ac coupling next to the FPGA.

My question is can I get away with DC coupling if the LVDS voltages are within range of the FPGA or should I use AC-coupling before the SoM Module?

  • Sign in to reply
  • Cancel
  • iksevas
    iksevas over 1 year ago

    You may be able to get away with the DC coupled lines if the voltages fall in range of the FPGA I/O. Ultimately you could be playing games with the voltage standard you are using in your Vivado design to make it work if it differs from the LVDS requirements of the FPGA I/O. It would be prudent if you added termination to your design that converts to the proper voltage range. Many times, it's not an ideal solution, but you could add the termination / AC coupling as close as possible to the JX connector of your Carrier Card. Give yourself options to avoid spinning the board later.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • revky
    revky over 1 year ago in reply to iksevas

    Yes, I guess this is what i have decided to go even if it is not ideal.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • padudle
    padudle over 1 year ago

    In theory it does not matter where you put the AC coupling capacitors.  They do not need to be at the load. They can be at the source or anywhere in between. 

    For LVDS you do want the termination resistance at the load though.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bidrohini
    bidrohini over 1 year ago

    AC coupling is generally preferred in cases where there is a mismatch in common-mode voltage requirements or if there is a risk of input overvoltage. AC coupling capacitors (typically 100nF) block the DC component, allowing the FPGA to internally set the appropriate bias level at the LVDS input. Due to the SoM constraints, capacitors cannot be placed directly at the FPGA. However, they can be placed on the Si5341’s side of the connection. This placement is acceptable as long as the capacitors are close enough to maintain signal integrity across the interface, ideally within a few centimetres.