Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design UltraZed-EV GC LVDS Clock DC Coupling
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 358 subscribers
  • Views 956 views
  • Users 0 members are here
Related

UltraZed-EV GC LVDS Clock DC Coupling

revky
revky over 1 year ago

Hi,

I am using a SI5341 to generate a 400MHz to use as global clock on the UltraZed-EV+.

The SI5341 output buffer supply is +3V3 and the FPGA HP bank is +1V8.

The output buffer common mode voltage for this is 1.1V to 1.3V and swing is 350mV to 510mV. Due to the fact that the FPGA is on the SoM I cannot use ac coupling next to the FPGA.

My question is can I get away with DC coupling if the LVDS voltages are within range of the FPGA or should I use AC-coupling before the SoM Module?

  • Sign in to reply
  • Cancel
Parents
  • bidrohini
    bidrohini over 1 year ago

    AC coupling is generally preferred in cases where there is a mismatch in common-mode voltage requirements or if there is a risk of input overvoltage. AC coupling capacitors (typically 100nF) block the DC component, allowing the FPGA to internally set the appropriate bias level at the LVDS input. Due to the SoM constraints, capacitors cannot be placed directly at the FPGA. However, they can be placed on the Si5341’s side of the connection. This placement is acceptable as long as the capacitors are close enough to maintain signal integrity across the interface, ideally within a few centimetres.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • bidrohini
    bidrohini over 1 year ago

    AC coupling is generally preferred in cases where there is a mismatch in common-mode voltage requirements or if there is a risk of input overvoltage. AC coupling capacitors (typically 100nF) block the DC component, allowing the FPGA to internally set the appropriate bias level at the LVDS input. Due to the SoM constraints, capacitors cannot be placed directly at the FPGA. However, they can be placed on the Si5341’s side of the connection. This placement is acceptable as long as the capacitors are close enough to maintain signal integrity across the interface, ideally within a few centimetres.