Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design No USB 3.0 on a Avnet UltraZed-EG-PCIe Board (with AES-ACC-WHIZZ-USB3 adapter)
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 358 subscribers
  • Views 1185 views
  • Users 0 members are here
Related

No USB 3.0 on a Avnet UltraZed-EG-PCIe Board (with AES-ACC-WHIZZ-USB3 adapter)

weidmann
weidmann over 1 year ago

Dear Sir or Madam,

I am trying to get USB 3.0 to work on an Avnet UltraZed-EG-PCIe board.

I am using the Out of the Box Images from uz3eg_pciec_2019_1 bsp.
I have also tried the latest image from uz3eg_pciec_base_2024_1.

When I plug in a USB 3.0 device, it is only recognized as USB 2.0.

Tested devices:

    Samsung USB 3.0 SSD hard drive
    Webcam with USB 3.0
    Transcend USB 3.0 SD card reader

Output in Linux:

Webcam:
root@uz3eg-pciec-2019-1:~# lsusb -t
/:  Bus 02.Port 1: Dev 1, Class=root_hub, Driver=xhci-hcd/1p, 5000M
/:  Bus 01.Port 1: Dev 1, Class=root_hub, Driver=xhci-hcd/1p, 480M
    |__ Port 1: Dev 2, If 0, Class=Video, Driver=uvcvideo, 480M
    |__ Port 1. Dev 2, If 1, Class=Video, Driver=uvcvideo, 480M
    |__ Port 1: Dev 2, If 2, Class=Human Interface Device, Driver=usbhid, 480M

Samsung USB 3.0 SSD:
root@uz3eg-pciec-2019-1:~# lsusb -t
/:  Bus 02.Port 1: Dev 1, Class=root_hub, Driver=xhci-xhd/1p, 5000M
/:  Bus 01.Port 1: Dev 1, Class=Class=root_hub, Driver=xhci-hcd/1p, 480M
    |__ Port 1: Dev 2, If 0, Class=Mass Storage, Driver=uas, 480M

I found the following post:
community.element14.com/.../usb-3-devices-only-detected-with-usb-2-speed

I bought the AES-ACC-WHIZZ-USB3 adapter.
With this adapter, no USB device is recognized. Even USB 2.0 does not work.

Webcam:
root@uz3eg-pciec-2019-1:~# lsusb -t
/:  Bus 02.Port 1: Dev 1, Class=root_hub, Driver=xhci-hcd/1p, 5000M
/:  Bus 01.Port 1: Dev 1, Class=root_hub, Driver=xhci-hcd/1p, 480M

Samsung USB 3.0 SSD:
root@uz3eg-pciec-2019-1:~# lsusb -t
/:  Bus 02.Port 1: Dev 1, Class=root_hub, Driver=xhci-hcd/1p, 5000M
/:  Bus 01.Port 1: Dev 1, Class=root_hub, Driver=xhci-hcd/1p, 480M

If I connect a USB 2.0 extension cable to the AES-ACC-WHIZZ-USB3 adapter,
the devices (camera, HDD) are at least recognized again with USB 2.0.

I am attaching a photo of the setup.
I have not changed anything on the Out of the Box Image.
I cannot get any USB 3.0 device to work.

I am completely at a loss and need help.

With kind regards,
Sebastian

image

  • Sign in to reply
  • Cancel

Top Replies

  • iksevas
    iksevas over 1 year ago in reply to iksevas +2
    Looks like you need to review the jumpers and potentially see if the 52MHz clock for the GTR is not there from the clock synthesizer.
Parents
  • iksevas
    iksevas over 1 year ago

    Here is some info that could help you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • iksevas
    iksevas over 1 year ago in reply to iksevas

    Looks like you need to review the jumpers and potentially see if the 52MHz clock for the GTR is not there from the clock synthesizer.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • iksevas
    iksevas over 1 year ago in reply to iksevas

    Looks like you need to review the jumpers and potentially see if the 52MHz clock for the GTR is not there from the clock synthesizer.