Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Using Xilinx Tools Forum Cannot program the PL
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 363 subscribers
  • Views 276 views
  • Users 0 members are here
Related

Cannot program the PL

Former Member
Former Member over 13 years ago

When trying to download the bitstream to program the PL (following chapter 3 in ZedBoard_CTT_v14.3_121017.pdf) impact (and SDK too) gives me an error.

After having having "Assign a new configuration file" to the zc7z020 part in the JTAG chain (which seems to finish without errors), I try "Program" and get a big red box "Program failed" with the error message "ERROR:Cse - Could not create temporary file: /home/hi/.cse/cse_tempFile.bit".

I think at least some parts of the JTAG communication work, I have successfully run the Hello_world application (chapter 2 in ZedBoard_CTT_v14.3_121017.pdf). And when running "Initialize chain" in impact I get sensible output.

When using Digilent utilities:

$ djtgcfg enum
Found 1 device(s)

Device: Zed
    Product Name:   Digilent Zed
    User Name:      Zed
    Serial Number:  210248450909

$ djtgcfg init -d Zed
Initializing scan chain...
Found Device ID: 03727093
Found Device ID: 4ba00477

Found 2 device(s):
    Device 0: UNKNOWN
    Device 1: UNKNOWN

$ djtgcfg prog -d Zed --index 1 --file ~/fpga/p/q1/q1.sdk/SDK/SDK_Export/system_hw_platform/system.bit
Programming device. Do not touch your board. This may take a few minutes...
ERROR: failed to program device with file /home/hi/fpga/p/q1/q1.sdk/SDK/SDK_Export/system_hw_platform/system.bit

Is this a JTAG/USB communication problem or in which direction should I search for a solution ?

H
I'm using Ubuntu 12.04 64-bit as host.

  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 12 years ago

    Hi, I had this issue as well but just touched the "cse_tempFile.bit" file and changed the permissions for my account so it had full rights to the file.