Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Using Xilinx Tools Forum Execution's problem of a simple verilog program on ZedBoard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 363 subscribers
  • Views 424 views
  • Users 0 members are here
Related

Execution's problem of a simple verilog program on ZedBoard

Former Member
Former Member over 11 years ago

Hello,
I'm a new user of Vivado 2014.2 and I have begun to learn the Verilog language recently. I have tried for 2-3 days to do a simple program that I want to test on my Zedboard. I would like to shift right or left one led (depending on the pushing button choice).

This is the top module file (.v):

`timescale 1ns / 1ps

module pilotage_leds(
    input BTNU,
    input BTND,
    output [7:0] leds
    );
   
    reg [7:0]leds=8'b00010000;
   
    always @(posedge BTNU or posedge BTND)
        begin
       
        if(BTNU==1)
            begin
               if(leds==8'b10000000)
                begin
                    leds=8'b00000001;
                end
              
               else
                begin
                    leds=(leds<<1);
                end
               
            end
           
        else
            begin
                if(BTND==1)
                    begin
                        if(leds==8'b00000001)
                             begin
                                leds=8'b10000000;
                             end
                                  
                        else
                            begin
                                leds=(leds>>1);
                            end
                    end
            end
       
        end
   
endmodule

and here, the XDC file :

set_property PACKAGE_PIN T18 [get_ports BTNU]
set_property PACKAGE_PIN R16 [get_ports BTND]

set_property PACKAGE_PIN T22 [get_ports leds[0]]
set_property PACKAGE_PIN T21 [get_ports leds[1]]
set_property PACKAGE_PIN U22 [get_ports leds[2]]
set_property PACKAGE_PIN U21 [get_ports leds[3]]
set_property PACKAGE_PIN V22 [get_ports leds[4]]
set_property PACKAGE_PIN W22 [get_ports leds[5]]
set_property PACKAGE_PIN U19 [get_ports leds[6]]
set_property PACKAGE_PIN U14 [get_ports leds[7]]

set_property LVCMOS33 [get_ports leds[0]]
set_property LVCMOS33 [get_ports leds[1]]
set_property LVCMOS33 [get_ports leds[2]]
set_property LVCMOS33 [get_ports leds[3]]
set_property LVCMOS33 [get_ports leds[4]]
set_property LVCMOS33 [get_ports leds[5]]
set_property LVCMOS33 [get_ports leds[6]]
set_property LVCMOS33 [get_ports leds[7]]
set_property LVCMOS25 [get_ports BTNU]
set_property LVCMOS25 [get_ports BTND]

set_property SEVERITY {Warning} [get_drc_checks NSTD-1]
set_property SEVERITY {Warning} [get_drc_checks UCIO-1]

set_property CLOCK_DEDICATED_ROUTE FALSE [get_nets BTND_IBUF]
set_property CLOCK_DEDICATED_ROUTE FALSE [get_nets BTNU_IBUF]

When I transfer the program the leds[4] is lightening. The problem is when I push the BTNU button on the ZedBoard, all leds turn off.BTND runs normally.

I have tried to simulate with the vivado simulator. The code is running correctly.

I don't know if it is only a problem of code or if it's a problem of incompatibility of timing/signals regarding my code and the ZedBoard.

Thanks to help me.

Best regards

Thomas C

  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 11 years ago

    Anytime you are reading a mechanical switch pushed in a 'human' time frame you should debounce the signal with either hardware (HDL) or software. Sven gives an example of this in this blog entry: http://svenand.blogdrive.com/archive/207.html#.VBC80PmwI8k

     

    -Gary